cancel
Showing results for 
Search instead for 
Did you mean: 

I went through the homework on Linux, everything is as in the slides except that myProbe_Out says "p2p connected (Unknown MCU)".

przemyslaw2
Associate II

Hello, I've managed to compile, debug and flash the code from homework onto the device (using Cube ver. 1.6) and was able to run the CubeMonitor under linux Manjaro. Everything works just fine and according to the slides, except that myProbe_Out and myProbe_In statuses say: "p2p connected (Unknown MCU)" (rather than give a device name).

I'm getting also [error] messages: myProbe_Out: no probe config, so not sure really if there's just something I'm missing because it's Linux and some additional config is required for the probes in NodeRed?

Thanks!

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0