cancel
Showing results for 
Search instead for 
Did you mean: 

How can I use STM32 uController to voice recognition?

rezaelectronicss
Associate II
Posted on September 07, 2016 at 10:49

Hi

I want to build a voice controlled robot that it should does some actions according to it's command list and the voice it should recognize from user. Is it possible to do it with ST microcontrollers? which one is better for this purpose? is there any simillar open-source project or tutorials to build something as I said?

Thanks in advanced
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Walid FTITI_O
Senior II
Posted on September 07, 2016 at 15:08

Why not pick a project within your current capabilities? Do the project incrementally starting with the robot control and functionality.

Voice processing is hardly STM32 specific, Google for other projects, Open Source ones should be easy to find.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
rezaelectronicss
Associate II
Posted on September 07, 2016 at 15:18

cause I'm looking for a cheap way! I want to build a voice controlled robot/toy and this is a commercial project! So costs are important

rezaelectronicss
Associate II
Posted on September 07, 2016 at 15:21

Thank you hanibal, but is there specific tutorial or open-source project is done with stm32? I watched those files but they are only boards general introductions i think