cancel
Showing results for 
Search instead for 
Did you mean: 

first program of stm3210C

cyril2399
Associate II
Posted on July 11, 2011 at 09:28

Hello,

I have a stm3210C eval board and when I have launched it there was a program with sound, image, a game, web server all with icons.

I have download an example program and now I it is the only thing I have on my eval board.

I would like to found the first program that it had at the beginning.

Where could I find it ?

Thanks
This discussion is locked. Please start a new topic to ask your question.
7 REPLIES 7
rosarium
Associate II
Posted on July 11, 2011 at 09:40

STM3210C-EVAL demonstration firmware  at

http://mcd.rou.st.com/modules.php?name=mcu&file=familiesdocs&FAM=110#Firmware

rosarium
Associate II
cyril2399
Associate II
Posted on July 12, 2011 at 09:19

ok thank you very much, I've found what I need. Thanks

rosarium
Associate II
Posted on July 12, 2011 at 10:21

You are welcome... :)

cyril2399
Associate II
Posted on July 18, 2011 at 09:39

Hello,

Into the firmware, the project ''DEMO'' has an empty main...

the whole program is ''int main() {}''.

I would like to see how it is programmed (icons, image player, system info etc...).

Thank you

cyril2399
Associate II
Posted on August 24, 2011 at 15:04

Is there no way to have these codes?

Posted on August 24, 2011 at 17:42

Is there no way to have these codes?

It is no doubt using commercially licensed libraries, and you'd have to pay for them yourself.

You should probably contact ST, or your FAE, to discuss the availability of source code, or portions thereof. I suspect supporting the application for everyone would tax the engineering resources available.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..