cancel
Showing results for 
Search instead for 
Did you mean: 

EXTI same line different port?

ian239955
Associate II
Posted on October 01, 2013 at 09:52

Hi, I'm experimenting with interrupts from port pins, I can make the basic example work. What I was trying to do is to create and EXTI interrupt from GPIOA bit 0 and also GPIOB bit 0, but I'm starting to think that this is not possible, when I set it up for GPIOB I lose the interrupt from GPIOA. So, is it possible, and if it is, is there a code example somewhere?

Thanks
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on October 01, 2013 at 10:01

[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/NVIC%20interrupts%20on%20two%20ports%20with%20same%20pin%20number&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&currentviews=43]https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2Fcortex_mx_stm32%2FNVIC%20interrupts%20on%20two%20ports%20with%20same%20pin%20number&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=43

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
ian239955
Associate II
Posted on October 01, 2013 at 10:11

Thanks, sorry I didn't find that earlier post. 

Posted on October 01, 2013 at 10:17

Thanks, sorry I didn't find that earlier post.

That's Ok the search facility here is awful, I fished that one back out with Google.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..