2009-05-17 7:37 AM
CAN with internal oscillator
2011-05-17 4:00 AM
Hi,
Is an external crystal required to use CAN (as is the case with USB) or can I use the internal oscillator? The documentation I've read does not mention that a crystal is required. Thanks Trevor2011-05-17 4:00 AM
I had wondered this as well, and found in the BOSCH CAN Bus spec found in a link from wikipedia the following:
''A maximum oscillator tolerance of 1.58% is given and therefore the use of a ceramic resonator at a bus speed of up to 125 Kbits/s as a rule of thumb'' ''For the full bus speed range of the CAN protocol, a quartz oscillator is required. '' Therefore I would run w/ a quartz crystal. Todd2011-05-17 4:00 AM
Thanks Todd. I'll go with a crystal then.
2011-05-17 4:00 AM
The STM32 bxCAN is connected to PCLK1 (APB1 clock ) : 36 MHz max