cancel
Showing results for 
Search instead for 
Did you mean: 

Bootloader command details, SPI timing

brianwilloughby9
Associate II
Posted on September 28, 2015 at 23:07

I have AN4286, but some of the details are vague or confusing. Is there any other source of information on the bootloader? I am working with SPI, and have most commands working, but there are still a few mysteries. Is there example code for communicating with the bootloader over SPI?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on September 29, 2015 at 00:37

Not seen any, and haven't used the SPI connectivity. Used the USART methods a lot, and disassembled the ROMs.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
brianwilloughby9
Associate II
Posted on October 01, 2015 at 20:56

Thanks, clive1. I've had to disassemble the bootloader ROM for the TMS320, but have not done so for the STM32. Do you happen to have any disassembly files around, or notes that you could share? I'm sure I could manage to disassembly the ROM myself, but if I can save time, I'd appreciate it.