cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 HID Host custom device

khetanikrunal
Associate
Posted on November 12, 2014 at 08:42

Hello,

I am interested to make USB HID HOST which can communicate with custom hid device instead of mice or keyboard.

For that I have to send data to that custom hid device.

I have used below fuction for dataout

USBH_InterruptSendData (pdev, (unsigned char *)&HID_Machine.buff, HID_Machine.length, HID_Machine.hc_num_out);

I am only doing out transaction form Host(STM32) to device. Everything is perfect and working fine up to 14th frame but 15th frame get corrupted, I have analyzer showing ''child has an error''. So I am unable to understand the cause of issue, is it memory overflow at host?

If  I continue data transmission with new data then host is sending old data packet onwards

I used dual core example for ST and modified  USBH_HID_Handle() as below (Only two cases are shown here)

case HID_SEND_DATA:

while(USB_OTG_IsEvenFrame(pdev) == FALSE);

USBH_InterruptSendData (pdev, (unsigned char *)&HID_Machine.buff, HID_Machine.length, HID_Machine.hc_num_out);

HID_Machine.state = HID_BUSY;

HID_Machine.timer = HCD_GetCurrentFrame(pdev);

break;

case HID_BUSY:

if(( HCD_GetCurrentFrame(pdev) - HID_Machine.timer) >= HID_Machine.poll)

{

HID_Machine.state = HID_SEND_DATA;

//Retry++; //1

}

else if(HCD_GetURB_State(pdev , HID_Machine.hc_num_out) == URB_DONE) //last transaction was successful or not(USB request Block)

HID_Machine.state = HID_GET_DATA;

BD_Data_Sent_Flag=1;

}

else if(HCD_GetURB_State(pdev, HID_Machine.hc_num_out) == URB_STALL )  

{      

if( (USBH_ClrFeature(pdev,  pphost, HID_Machine.ep_addr, HID_Machine.hc_num_out)) == USBH_OK)

{  

HID_Machine.state = HID_SEND_DATA;        

}      

break;

#hid #host #stm32
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

Sorry, bumping old zombie unanswered threads off my feed

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..