cancel
Showing results for 
Search instead for 
Did you mean: 

STM3210C-EVAL - USB examples

ian239955
Associate II
Posted on April 24, 2013 at 10:30

Hi, I'm getting started, would like to see some USB / PC interfacing. I have the STM3210C-EVAL, I'm using IAR and JLINK and have my own project compiling and running ok.

I downloaded the doc at 

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/CD00158241.pdf

and the code at 

http://www.st.com/web/en/catalog/tools/PF257917

tried the Joystick Mouse demo. In the manual, it says �To select the STMicroelectronics evaluation board used to run the demo, uncomment the corresponding line in the platform_config.h file.�

I have a STM3210C eval, the ones on offer are:

STM3210B

STM3210E

I tried both, but I get �Driver � Fatal error: ST-Link Connection error Session Aboorted�, then

�Failed to load flash loader  ��.FlashSTM32F10xxe.flash� (but the file does exist on my system), then

�A fatal error has occurred�

Is it because there is no demo for the c version of the eval board? That would be annoying! Can I get it running on the c version?

Thanks

#usb
This discussion is locked. Please start a new topic to ask your question.
14 REPLIES 14
ian239955
Associate II
Posted on April 25, 2013 at 09:22

Ok, and clues about communicating over usb with any kind of PC app? This used to be easy with rs232!

Cheers, Ian

frankmeyer9
Associate II
Posted on April 25, 2013 at 10:04

I'm sure the USB access in such high-level environments like .NET, Java or QT is much simpler than on MCU level, with comprehensive and well-documented classes/objects.

A google search will surely bring up some fruitful links.

But this is not the main focus of this forum, so it's less likely for you to find help here.

ian239955
Associate II
Posted on April 25, 2013 at 12:25

Ok, getting there (see below)

But just a couple of problems:

As below, I've modified the example to echo what is sent from the PC. To check reliability, I have the PC also echo, so the same message bounces forever, or should. But it all stops after 649. The message is 20 bytes, 01234567890123456789

  

At this time, I am still receiving messages at the stm, but send stops working (back to the PC).

I think it might be something to do with APP_Rx_ptr_in, which is reset to 0 when it gets to APP_RX_DATA_SIZE, it is always a low value (about 40) when everything stops.

Other problem: If I restart either end, it doesn't seem to work until I unplug and replug the USB cable.

Anyone know enough about the sample program to know what is happening here?

Thanks

Solution so far: It is as easy as rs232 (almost), when you know how.

From this library Clive mentioned earlier http://www.st.com/web/en/catalog/tools/PF257882

Run the VCP (virtual com port) example.At that point, if you have a usb cable plugged in, it will appear in the PC device list in Ports(COM&LPT) as ''STMicroelectronics VirtualCom Port'', and in my case on COM3.

You then just read / write to that from your PC app just like you used to with rs232. 

The top level code is in usbd_cdc_vcp.c. Note that the default line coding is 115200 baud, 1 stop bit, no parity, 8 bit, I set my com port to this but it probably doesn't make any difference as it's not actually going over rs232.

If you put a breakpoint in VCP_DataRx it should trigger when you send something to STM. The project copies it out to a real rs232 port, put if you add a line ''VCP_DataTx(Buf, Len);'' you can get it to echo back to usb.

You also have to change ''VCP_DataTx;'' as it has obviously been hacked to only work with rs232 receive, like this: 

int Count=0;

  while (Count<Len)

  {

    APP_Rx_Buffer[APP_Rx_ptr_in] = *(Buf+Count)+1;

    Count++;

    APP_Rx_ptr_in++;

    if(APP_Rx_ptr_in == APP_RX_DATA_SIZE)

    {

      APP_Rx_ptr_in = 0;

    }  

  }

  

  return USBD_OK;

ian239955
Associate II
Posted on April 25, 2013 at 12:59

Ok, just discovered it's some kind of timing issue - if I display what I receive in my PC app in a list box (which presumably takes an extra few ms) then the messaging continues forever.

But I can't rely on delays for reliable coms.

Is there any explanation for this?

ian239955
Associate II
Posted on April 30, 2013 at 12:24

I did resolve this and answer but for some reason my answer did not show. It was failing above when I was not reading the com port due to the buffers filling up! So it all works great and I hope this might be useful for others.