Skip to main content
Associate III
May 7, 2026
Question

BSP_SD_Init() fails - problem in SDMMC initialization ?

Title updated to better reflect the root problem; was originally 'Riverdi 12.1" + TouchGFX 4.25 + FATFS not working'


Hi everyone,

I am working on a Riverdi 12.1" display board based on STM32H7 with TouchGFX 4.25 generated project.

Environment:

  • TouchGFX 4.25

  • STM32CubeMX generated project

  • STM32CubeIDE

  • Riverdi 12.1" board

  • STM32H7

  • FreeRTOS enabled

  • Debugging with ST-LINK

Problem:
BSP_SD_Init() returns MSD_ERROR_SD_NOT_PRESENT.

In main.c:

uint8_t res;

res = BSP_SD_Init();

risultato = res;

if(res != 2)
{
 Error_Handler();
}

The value stored in risultato is:

MSD_ERROR_SD_NOT_PRESENT

Additional important behavior:

When I start a FreeRTOS task that accesses FATFS/SD, the display becomes completely black and TouchGFX no longer shows images.

This is my task:

void StartDefaultTask(void *argument)
{
 FIL file;
 UINT bw;

 for(;;)
 {
 SCB_CleanDCache();
 SCB_InvalidateDCache();

 if(BSP_SD_Init() == MSD_OK)
 {
 if(f_mount(&SDFatFS, SDPath, 1) == FR_OK)
 {
 if(f_open(&file, "log.txt", FA_OPEN_ALWAYS | FA_WRITE) == FR_OK)
 {
 f_lseek(&file, f_size(&file));

 char msg[] = "log entry\r\n";
 f_write(&file, msg, strlen(msg), &bw);
 f_close(&file);
 }
 }
 }

 osDelay(1000);
 }
}

If I completely comment out this task, TouchGFX works correctly and all images are displayed normally.

So:

  • With SD/FATFS task enabled → display becomes black

  • With SD/FATFS task disabled → GUI works correctly

Other details:

  • SDRAM initialized correctly

  • LTDC working before SD task starts

  • QSPI memory mapped mode enabled

  • FATFS enabled

  • MPU configured with SDRAM framebuffer as non-cacheable

MPU configuration:

MPU_InitStruct.BaseAddress = 0xD0000000;
MPU_InitStruct.Size = MPU_REGION_SIZE_8MB;
MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;

Questions:

  • Could this be a DCache/MPU coherency issue between TouchGFX and FATFS?

  • Is there a known issue with Riverdi BSP + SDMMC + TouchGFX?

  • Should SD buffers be placed in a dedicated MPU region?

  • Is calling SCB_CleanDCache() and SCB_InvalidateDCache() inside the task causing LTDC framebuffer corruption?

  • Is there a recommended STM32H7 cache configuration for TouchGFX + FATFS?

Any suggestion is appreciated.

Thanks.

8 replies

Osman SOYKURT
ST Technical Moderator
May 11, 2026

Hello @Sasa1234 ,

I'm wondering whether the issue is related to TouchGFX at all.
The best way to confirm this is to test SD card initialization in a minimal project without TouchGFX, FreeRTOS, LTDC, or QSPI.
First, verify that BSP_SD_Init() works correctly.
If SD still fails in that setup, the issue is likely in the SDMMC/BSP/card-detect/hardware configuration rather than in the GUI.
Only if it works in the minimal project and fails after adding TouchGFX should cache/MPU/display interaction be investigated.

ST Software Developer | TouchGFX
Sasa1234Author
Associate III
May 21, 2026

Hello everyone, after days of work, I contacted Riverdi technical support and explained the problem. They told me about a bug in version 4.25 of TouchGFX where the detect pin is not configured in the fatfs_platform.c file.

Here is the function:

uint8_t BSP_PlatformIsDetected(void) {
 uint8_t status = SD_PRESENT;
 /* Check SD card detect pin */
 if(HAL_GPIO_ReadPin(SD_DETECT_GPIO_PORT, SD_DETECT_PIN) == GPIO_PIN_RESET)
 {
 status = SD_NOT_PRESENT;
 }
 /* USER CODE BEGIN 1 */
 /* user code can be inserted here */
 /* USER CODE END 1 */
 return status;
}

They told me that in version 4.26.1 everything is resolved. The project works with this modification after implementing it.

However, I have a problem with files that have long names. In CubeMX I enabled the USE_LFN option to 2 or 3, but I get compilation errors saying that these functions are missing:

The linker errors come from FatFs Unicode / Long File Name (LFN) support being enabled, but the required conversion functions are missing.

The missing symbols are:

  • ff_convert

  • ff_wtoupper

My FatFS version is R0.12c.

How can I solve this? Are there any options I need to enable?

Let me know if you'd like a suggested answer to this issue as well.

 
 
 
Associate II
May 21, 2026

Hello I have similar issues with initialization.

What did you change in the code?

uint8_t BSP_PlatformIsDetected(void) {
 uint8_t status = SD_PRESENT;
 /* Check SD card detect pin */
 if(HAL_GPIO_ReadPin(SD_DETECT_GPIO_PORT, SD_DETECT_PIN) == GPIO_PIN_RESET)
 {
 status = SD_NOT_PRESENT;
 }
 /* USER CODE BEGIN 1 */
 /* user code can be inserted here */
 /* USER CODE END 1 */
 return status;
}


I am assuming you added SD_PRESENT in USER CODE 1?

status = SD_PRESENT;

 

Sasa1234Author
Associate III
May 11, 2026

 

Hi @Osman SOYKURT 

The issue does not appear to be related to TouchGFX.

As mentioned previously, BSP_SD_Init() already fails in the current setup, which points to a problem in the SDMMC peripheral initialization rather than anything related to the GUI, FreeRTOS, LTDC, or QSPI.

At this stage, the root cause is most likely related to the SDMMC/BSP configuration, card-detect signal, or underlying hardware setup.

I read this : Solved: STM32H757 SDMMC1 only works with M7 core - STMicroelectronics Community 

But I don't have idea how to do it!!!!

If anyone has experience with BSP_SD_Init() failures and knows how to resolve this kind of issue, any advice would be greatly appreciated.

Osman SOYKURT
ST Technical Moderator
May 12, 2026

Hello @Sasa1234 ,

I will move your message to another ST Community forum board, where you have a better chance to receive an answer.

ST Software Developer | TouchGFX
Peter BENSCH
ST Technical Moderator
May 12, 2026

Moved from forum TouchGFX to  STM32 MCUs Embedded software because the question is not related to TouchGFX.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
mƎALLEm
ST Technical Moderator
May 12, 2026

Hello,


@Sasa1234 wrote:
  • Should SD buffers be placed in a dedicated MPU region?


I don't have idea about how the SDMMC drivers have been implemented but, the data need to be located in region accessible by the SDMMC and that depends on which instance you are using SDMMC1 or SDMMC2. From the RM0399:

mALLEm_0-1778586698252.png

For example if the SD data to transfer are located in DTCM, the transfer won't be performaed as the SDMMCs have no access to that memory. So you need to check from your side.

 


@Sasa1234 wrote:

Is calling SCB_CleanDCache() and SCB_InvalidateDCache() inside the task causing LTDC framebuffer corruption?


I'm wondering why calling these APIs in a loop in that task! If you comment out these lines do you face the same behavior?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.