cancel
Showing results for 
Search instead for 
Did you mean: 

2 strange packets from double-buffered bulk tx endpoint

kubok
Associate
Posted on May 23, 2012 at 09:51

Hello.

Please give me some knowledge about the topic.

Now I use STM32F103, and I found 2 strange packets transfer

after initializing endpoint as double-buffered bulk tx.

I found this problem after trying the following steps, 1,2 and 3.

---

1.

I initialize endpoint as the following,

almost same as ''AudioSpeaker'' Demo in STM USB-FS LIBRARY.

(but this is not Isochronous)

SetEPType(ENDP1, EP_BULK);

SetEPDoubleBuff(ENDP1);

SetEPDblBuffAddr(ENDP1, ENDP1_BUF0Addr, ENDP1_BUF1Addr);

SetEPDblBuffCount(ENDP1, EP_DBUF_IN, 0x40);

ClearDTOG_TX(ENDP1); // for usb peripheral

ClearDTOG_RX(ENDP1); // SW_BUF for application

ToggleDTOG_RX(ENDP1);

SetEPTxStatus(ENDP1, EP_TX_VALID);

SetEPRxStatus(ENDP1, EP_RX_DIS);

Toggle conditions are also cleared equally

when usb request (Set Configuration, Set Interface, etc.) is received.

2.

I connect a Device to PC via USB analyzer.

3.

I found 3 strange packets when a device starts.

All of them are max-packet-size, first one and second one are different,

but first one and third one are same.

---

To improve this strange-packet-transfer, I try to do the following steps, 4 and 5.

---

4.

I delete ''ToggleDTOG_RX(ENDP1);'' at any phase to make toggle bit even.

(No Problem to transfer a packet because SW_BUF can be toggled when it is transferred.)

Then I found 2 strange packets when a device starts.

These 2 packets are max-packet-size, first one and second one are different.

5.

I change a packet size from ''0x40'' to ''0x00'' in initialize phase.

(No Problem to transfer a packet because its size can be changed when it is transferred.)

Then I found 2 strange ''NULL'' packets when a device starts.

---

After all, the packets are NULL but I cannot avoid strange-packets-transfer.

Do I have some mistakes or misunderstanding?

#usb-double-buffer
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0