2019-11-11 11:41 AM
Ps: I saw https://community.st.com/s/question/0D50X0000BWnXe0SQF/st25ru3993-antenna , but it was not enough.
I'm interested in testing the https://www.st.com/en/nfc/st25ru3993.html , but I couldn't find information concerning antenna support. Have anyone used this module to accomplish long distance UHF readings? Can I achieve it with ST25RU3993?
I'm searching for
Which antennas have you used? Everything goes well?
Thanks!
Solved! Go to Solution.
2019-11-19 7:38 AM
Hello,
I am sorry, but for a read range between 2 km and 10 km I would suggest to look into a different kind of technology for sure it should be some kind of active tech.
ST25RU3993 can well support reader for ranges between 2 and 10 meters.
Cheers,
B
2019-11-19 7:38 AM
Hello,
I am sorry, but for a read range between 2 km and 10 km I would suggest to look into a different kind of technology for sure it should be some kind of active tech.
ST25RU3993 can well support reader for ranges between 2 and 10 meters.
Cheers,
B
2019-11-19 10:02 AM
Hello Bart,
Thank you for the answer.
As far as I'm concerned, the module doesn't come with an antenna,
right? I'm search for a good quality yet not expensive antenna which I
can use with ST25RU3993 in order to achieve a reading distance of,
let's say, at least 2 meters.
Could someone point me one (or two)?
Thanks!
2019-11-19 12:38 GMT-03:00, ST Community:
2019-12-05 5:44 AM
Hello jcbrtl,
the kit comes with a near field antenna which allows you to read tags in the centimeter range only.
For a start check:
For sure there a many more providers for good quality antennas!
Cheers,
B
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.