cancel
Showing results for 
Search instead for 
Did you mean: 

Question for Application note AN5734.

shinba
Associate

My company designs circuits and artwork upon request from customers.

We are considering this project based on a customer's request to change the laser power supply to be compatible with worldwide use.

While considering various things, I am also considering a PFC circuit with L4985.

Question for Application note AN5734.

AN5734 : Table 4 on page 27

Is the relationship between Wire type and Wire diameter correct?

----------------------------------------------------------------------------------------------------------------------

Windings   Start pins   End pins    Number of turns        Wire type           Wire diameter

 PRIM              5               2                     70                  Single – G2         Litz 0.2Ø x 30

 AUX                9             11               5 (spaced)            Litz – G2                0.28Ø

----------------------------------------------------------------------------------------------------------------------

Do you have any information on transformers?

Best regards.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Peter BENSCH
ST Employee

Welcome @shinba, to the community!

Why exactly do you think the information on wire diameter and wire type is incorrect?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
shinba
Associate

The wire type on the PRIM side is single Grade 2, but the wire diameter is Litz wire.

Also, the wire type on the AUX side is grade 2 Litz wire, but the wire diameter is 0.28Φ.

Is this correct.

Best regards.