cancel
Showing results for 
Search instead for 
Did you mean: 

Anyone have success with programming the NUCLEO-H723ZGT variant with Arduino IDE?

IBurk.1
Associate

I was wondering if anyone has any experience using the H723ZGT variant within Arduino IDE successfully?

I followed through a tutorial on adding it as a variant to be recognized by the Arduino IDE.

Tutorial Used

I am at the point where I can compile the "blink" example and upload it to the board. I see the RGB LED (LD4) blink red and green after programming and then stay a solid red. I am expecting to see LD2 blink at around 1Hz after programming but I do not see anything. I have tried various other simple test programs without any luck.

Is anyone able to help me out or point me in the right direction?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
ssipa.1
Associate II

open the Arduino IDE

Go to files and click on the preference in the Arduino IDE

Enter the 'https://raw.githubusercontent.com/stm32duino/BoardManagerFiles/master/STM32/package_stm_index.json' into the "Additional Boards Manager URLs"

This is how I figured out that my particular variant does not exist natively so I created my own and am at the point/problem described in my original post.

This does not help me unfortunately, also that link is depreciated and the new updated one is

"https://github.com/stm32duino/BoardManagerFiles/raw/main/package_stmicroelectronics_index.json"