cancel
Showing results for 
Search instead for 
Did you mean: 

STR7 tmer used for PWM

cbeal
Associate
Posted on February 15, 2008 at 09:48

STR7 tmer used for PWM

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
cbeal
Associate
Posted on February 15, 2008 at 09:48

There is a bug in tim.c in the function

TIM_PWMOModeConfig()

The pulse width value is increased if the requested value is less than 5

/* Set the Duty Cycle value */

if (XDutyCycle < 5)

{

XDutyCycle = 4;

}

This shouldn't be there as it means that the minimum value of PWM can never be set.

The next line is:

TIMx->OCAR = XDutyCycle - 4;

This is also wrong, as 5 needs to be subtracted not 4.

I have tested this with timer 3 where the supplied values to the function are 1 for PWM and 0xC0 for frequency giving 125KHz with an on time of about 200nS for an expected on time of 30nS.

The library function puts 0 into OCAR and 0xBF into OCBR.

Correcting the code as outlined puts 0xFFFC into OCAR and 0xbf into OCBR.

This gives 125KHz with 30nS on time as expected.

Charles Beal