cancel
Showing results for 
Search instead for 
Did you mean: 

How to disable LVD? Seems impossible with CAPS, firmware method is suspect

mark9
Associate II
Posted on December 11, 2007 at 16:32

How to disable LVD? Seems impossible with CAPS, firmware method is suspect

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
mark9
Associate II
Posted on May 17, 2011 at 09:48

The flash programming manual documents 3 bits for configuring the LVD, but I only see one checkbutton in CAPS.

The 3 bits are

LVD_WNG_SEL (bit 3) (enable warning interrupt for 3.3 rail)

LVD_RST_SEL (bit 2) (enable reset for 3.3 rail)

LVD_TH (bit 1) (toggle 2.4 or 2.7 v threshold)

at JTAG address 0x520006. CAPS only has an option for LVD_TH. We have an external voltage supervisor, and I am sure that there is a hardware bug with the internal LVD, so I am trying to turn it off.

I'm also trying to disable it with firmware, using the FMI_Config() command in the 91x library, but it does weird things... It appears to be setting

a reserved bit to zero (bit 13), so I am worried that is changing an undocumented feature.

Using the RSIG command to read the flash configuration, I find that it is equal to 0x24CF before I issue this command:

FMI_Config(FMI_READ_WAIT_STATE_1,

FMI_WRITE_WAIT_STATE_1,

FMI_PWD_ENABLE,

FMI_LVD_DISABLE,

FMI_FREQ_LOW);

Afterwards, it is equal to 0x06CF, when I was expecting 0x26CF. I'm worried about the 0x2000 bit mask going to zero. What is this for?