on
2023-04-25
7:00 AM
- edited on
2026-03-11
5:58 AM
by
Laurids_PETERSE
Other sensors than the VL53L4CD and VL53L5CX presented during the webinar can be used (VL53L0X, VL53L3CX), but performances are not as good as VL53L4CD. Example code, API, and drivers have to be adapted. VL53L5CX gives better performances than VL53L4CD due to multizone.
Yes, they are class1.
The wavelength is 940 nm.
Under normal conditions, they should work for years.