cancel
Showing results for 
Search instead for 
Did you mean: 

BlueNRG-MS concurrent role

thomas
Associate
Posted on July 13, 2015 at 16:57

Which concurrent roles does the the BlueNRG-MS support?

For example:

 3 Master - MyDevice

 

 2 Master - MyDevice - 1 Slave

 

 1Master - MyDevice - 2 Slave

 

 MyDevice - 3 Slave

Regards Thomas

#bluenrg-ms
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on July 20, 2015 at 14:51

Dear Customer,

using the stack Mode4 (only for BlueNRG-MS), the device can be configured as:

- Master and Slave (up to 2 masters)

- Simultaneous advertising and scanning

- Up to 4 connections

- 12 KB of RAM retention.

Regards,

GM

Which concurrent roles does the the BlueNRG-MS support?

For example:

 3 Master - MyDevice

 

 2 Master - MyDevice - 1 Slave

 

 1Master - MyDevice - 2 Slave

 

 MyDevice - 3 Slave

Regards Thomas