| Subject | Author | Posted | |
|---|---|---|---|
|
Hello! I am designing a wide input range flyback converter using the altair04-900 for my formula st...
| 2025-11-17 10:11 AM | ||
|
I cannot see the effect of the low speed optimization. I set speed to 1 rpm and watch the phase cu...
| 2025-11-17 5:18 AM | ||
|
The PowerSTEP01's datasheet says on page 34 that MIN_SPEED is 12 bits wide. On page 37, it is desc...
| 2025-11-17 4:25 AM | ||
|
I've been looking at the STEVAL-ISD01KCB, and I saw in an image that it has some capacitors between...
| 2025-11-16 6:45 AM | ||
|
I have a design running on 24V SLA batteries using STEF01 fuses for protection of the lower powered...
| 2025-11-13 11:44 PM | ||
|
Hello, (L6562DTR)I have encountered some problems when using this chip and hope to get some suggest...
| 2025-11-13 5:37 PM | ||
|
Hi,
We have been testing our H-bridge on 2 EVALSTGAP2HDM with IPP026N10NF2S MOSFETs. The gate res...
| 2025-11-12 7:36 AM | ||
|
Hello! I am building a 50-600Vin flyback converter using the altair04-900 to power an LED as a stud...
| 2025-11-07 5:17 AM | ||
|
Last week, I have been testing SRK1000A in EVLSRK1000A-PF, in an application with 250 kHz fixed fre...
| 2025-10-27 6:14 AM | ||
|
I have an application where I am using L99VR02J. for this application I do not need the watchdog so...
| 2025-10-15 8:55 AM | ||
|
I have the EVALSTPM-3PHISO. IT appears that it only measures Volts and amps on a single phase at a ...
| 2025-10-15 6:40 AM | ||
|
Hello, I am creating a board using the STUSB4500QTR and I saw something on a video that ...
| 2025-10-14 10:04 PM | ||
|
Hello ST team and community, I’m currently trying to recreate the AN5287 reference design on my ow...
| 2025-10-13 7:33 PM | ||
|
We are using 2 MASTERGAN1TR to drive current across an inductor. We are seeing damage on the body ...
| 2025-10-13 2:43 PM | ||
|
Is there a way to read the motor position while it's moving, such as with a command like "run," "go...
| 2025-10-12 1:23 AM | ||
|
I have followed the design attached in PDF. It is from ST designsuit. I have used MYRRA 75032 flyb...
| 2025-10-08 1:03 AM | ||
|
Hi everyone,
I’m using the STGIB8CH60TS-E IPM in my motor drive design and trying to configure th...
| 2025-10-06 4:13 AM | ||
|
Which alarm to read if our motor skips steps while moving?
The motor works fine for a period of t...
| 2025-10-06 2:28 AM | ||
|
Hello Team,
We are using VN9E30F High Side Driver, when we try to communicate it through SPI, the...
| 2025-10-05 11:33 PM | ||
|
Hello, I am planning to use the SPV1050 in buck-boost configuration. According to the datasheet, ...
| 2025-10-01 2:21 AM |