| Subject | Author | Posted | |
|---|---|---|---|
|
Hi, I’m working with the LAN9253 and an STM32F446ZCH6, using Quad-SPI for Ether CAT communication....
| 2025-12-01 2:20 AM | ||
|
I'm trying to read the ID of ST7701SN with STM32F469. The read command was sent correctly by the MC...
| 2025-11-25 7:25 PM | ||
|
I am using the starm-clang with cmake. I need to use multithreading lock. I understand that in sta...
| 2025-11-20 4:55 PM | ||
|
Hello everyone, I’m looking for any Wi-Fi connectivity implementation examples for the STEVAL-STWI...
| 2025-11-18 8:35 PM | ||
|
Hi,
We are planning to use PSRAM chip apmemory (APS12808L-3OBM) with STM32U575QII6.
Please che...
| 2025-11-18 4:50 AM | ||
|
Hello everyone, I’m working with the B-L072Z-LRWAN1 Discovery board (STM32L072CZ + Murata CMWX1ZZA...
| 2025-11-12 6:24 AM | ||
|
NUCLEO F411RE, MPU 9250
I'm reading acceleration data via SPI from an MPU 9250 directly to memory...
| 2025-10-10 4:16 AM | ||
|
Hi everyone,
I'm new to the FPV hobby and I've run into a problem that I'm completely stuck on af...
| 2025-10-04 10:12 AM | ||
|
Split from STM32U5G9J DK2 + 4G Module (USB CDC ECM) not detecting USB device - this is a different ...
| 2025-09-26 12:44 AM | ||
|
Hello Community,
I've been trying without success to setup an SPI interface to a LCD panel. It's...
| 2025-09-23 12:51 AM | ||
|
The Raspberry Pi Pico 2W is a dual-core Cortex-M33 processor. It has 16 DMA channels per bus. While...
| 2025-09-22 1:01 AM | ||
|
Hopefully i chose the right thread, right so i have sn stm32h523 chip running a PCISPH fluid simula...
| 2025-08-23 5:05 AM | ||
|
We analyzed the boot and camera initialization time on the STM32N6570-DK using the DCMIPP SnapshotD...
| 2025-08-22 3:34 AM | ||
|
Hello all, I'm currently working on bringing up the CMWX1ZZABZ-078 module from Murata. This module...
| 2025-07-28 11:04 PM | ||
|
Hello, I have a NUCELO_H723ZG and I am trying to set it up to be a master, I am using a MIKROE-3816...
| 2025-07-23 4:11 PM | ||
|
Hello Everybody, I’m developing a Class 0.2 energy metering system for 1-phase, 3-phase (3-wire),...
| 2025-06-28 5:54 PM | ||
|
Hi all, I’d like to share with you a project I recently completed – a digitally-controlled linear ...
| 2025-06-14 10:05 AM | ||
|
I'm working on a DMX communication project using an STM32 microcontroller (e.g., STM32G030K8T6TR). ...
| 2025-05-28 12:47 AM | ||
|
I'm working on a project using STM32U5 and I'm trying to communicate with a TMC2209 stepper driver ...
| 2025-05-23 8:05 AM | ||
|
Hi, I am working on the STM32G431RB and implementing ABI/Z quadrature signal generation. I’m us...
| 2025-05-21 3:41 AM |