2019-12-09 2:06 AM
Dear All ,
SPC5Studio updated components are available (56,57 on 58)
more information on http://download.spc5studio.com/
SPC58xHxx, Advanced GTM and USBTypeC credentials should be requested on credentials@spc5studio.com
New or updated components
RLA 1.11.0
SPC58xHxx : Full support of cut2 Mcan driver without CCCU
SPC584Bxx: PWM ICU test application
SPC560Pxx STEVAL-TTM002V1 board support
RLA 1.11.0 and Benchmark 1.4.0
support of SPC58xH-DISP board with benchmark application
RuntimeIO_1.3.4
Add mode (ASYNC, SYNC, Buffered) for serial configuration
Firmware updater 1.4.1
Inversion of CAN buffer
Flash 1.10.1
Copyrights update
Best Regards
Erwan