2019-05-02 8:29 AM
I have an integrated one of an ultrasonic washing machine.
This when measuring its frequency oscillates in 80kHz, but after a few minutes it begins to decrease the frequency and increase uncontrollably, so I have decided to change it.
the question is that where the model should appear is torn and can not be seen, but below shows this information.
S "Tear" A (only the letter "S" is displayed at the beginning and the letter "A" at the end)
V6 FG675
CHN99614
I will attach an image.
I hope you can help me.
Thank you.
2019-05-02 2:39 PM
schematic ? try the old tracing out by hand of the connections, make some sort of schematic. scientific wild guesses can follow :) info on chip not traceable to the part number