ST-Link Port Detection fails on STM32F765VGT6 & STM32L010RBT6
- 4 replies
- 1026 views
Hello
Please find the attached file for your reference.
I am encountering issues while attempting to flash a hex file onto the STM32F765VGT6 board using STM32 Utility. and I have used ST Link/V2.
Below are the specific issues:
Unable to Flash Hex Files: The hex files are not flashing successfully onto the board.
Target Voltage Detection Failed: The target voltage is detected as 1.2V on my PC, which is not as expected.
Port Not Detected: The utility is unable to detect the port.
Connection Settings in STM32 Utility:
Connection: SWD
Mode: Hot Plug (with Debug enabled in Low Power mode)
it is only detecting in hot plug mode but its not detecting in normal and connect under reset mode.
I have attached the output snippets and settings for your review. Could you kindly verify and guide me on how to resolve these issues at the earliest? Your assistance in troubleshooting this would be greatly appreciated.
Looking forward to your prompt response.
Best regards,
Venkata Narayana Singh