Skip to main content
Associate II
Apr 20, 2026 9:39 PM UTC
Solved

No STM32 target found

I have been programming my STM32H743 custom board for over a year.  Suddenly I'm getting the error message Error: No STM32 target found...

jwtuttle_0-1776721104744.png

I have tried changing the ST-Link itself but get the same error message.

Andrew Neil
Andrew NeilBest answer
Super User
Apr 21, 2026 4:35 PM UTC

@jwtuttle wrote:

what is the sequence the the ST-Link performs to determine that a STM32H743 is present?


It must do the standard SWD connection sequence:

https://developer.arm.com/documentation/ihi0031/a/The-Serial-Wire-Debug-Port--SW-DP-/Protocol-description/Connection-and-line-reset-sequence

It'll also query things like the device ID to find what part it is ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.

6 replies

Peter BENSCH
ST Technical Moderator
Apr 21, 2026 2:50 PM UTC

If it is an ST-LINK/V2, please include photos of the front and back so that it can be ruled out that it is one of the clones being referred to here.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
mƎALLEm
ST Technical Moderator
Apr 21, 2026 3:05 PM UTC

Hello,

Try to connect with "Power Down" mode:

mALLEm_0-1776783657941.png

Otherwise, what happened in between (working to not working)?

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Andrew Neil
Super User
Apr 21, 2026 3:12 PM UTC

@jwtuttle wrote:

Suddenly I'm getting the error 


So what did you change ?

After a year, also check for broken wires, loose connectors, etc

 

How to solve connection errors when connecting and programming the STM32 target board.

How to solve debugger connection issues

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
jwtuttleAuthor
Associate II
Apr 21, 2026 3:52 PM UTC

Hopefully our ST-Links are legit.  We bought them from Digi-key.

What changed: It appears that the interface board that we use to go from the 20 pin 0.1" spacing cable to the 0.05" 10 pin cable has worn out.  So that's the source of my problems.

But for debugging purposes in the future, what is the sequence the the ST-Link performs to determine that a STM32H743 is present?

Obviously, the ST-Link saw the voltage since it displayed the correct value.  But I did not see any of the signal lines change.  As in, NRST didn't go Low, SWDIO and SWCLK didn't toggle.  I assume in a working system these lines should toggle

 

Andrew Neil
Super User
Apr 21, 2026 4:31 PM UTC

@jwtuttle wrote:

Hopefully our ST-Links are legit.  We bought them from Digi-key.


Even DigiKey do sell clones:

AndrewNeil_0-1776788987505.png

Hence the request to see photos of what you're actually using.

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.