Skip to main content
km naxin
Associate
Nov 26, 2019 1:00 PM UTC
Question

How to choose stm32G431 BOOT mode

How to choose stm32G431 BOOT mode

Can you use stm32cubemx to configure BOOT mode? If you cannot use stm32cubemx how to configure.

May I ask if it is configured to boot from user flash memory.

This topic has been closed for replies.

4 replies

DMeie.2
Associate III
May 2, 2024 1:44 PM UTC

@Tilen MAJERLEUnfortunately this document doesn't explain how to configure the bootloader in CubeMX.
How would I change the registers related to that in CubeMX? For example the boot entry setting regsiter bits, "BOOT_LOCK", "nBoot0", "nBoot1", "nBoot0_SW".

If it is not possible to change these in CubeMX, how would I go about doing that in the generated software? As the registers can only be read prior to booting.

Tilen MAJERLE
ST Employee
May 2, 2024 7:29 PM UTC

STM32CubeMX is not a tool for modification of option bytes. Modifying option bytes is similar to modifying BIOS settings on your computer.

Typically you configure the option bytes in 2 possible ways:

  • With STM32CubeProgrammer option bytes command. See STM32CubeProgrammer user manual for this
  • Or as part of your firmware, which then modifies necessary bits. Some changes require power-on-reset after applying the setting.
DMeie.2
Associate III
May 3, 2024 10:37 AM UTC

Thanks a lot, this helped quite a bit.

For anyone else looking this up, these two knowledge base entries are very useful as well:
https://community.st.com/t5/stm32-mcus/what-are-option-bytes-in-stm32-and-how-do-i-use-them/ta-p/49451
https://community.st.com/t5/stm32-mcus/faq-stm32-boot-process/ta-p/49358