Skip to main content
Associate
Jul 15, 2025 3:58 PM UTC
Solved

.ioc file generation

hello everyone , 

When I create a new project in STM32CubeIDE (version: 1.17.0), the .ioc configuration file is not generated in the project directory. Here’s what I’ve tried:

Project Type:

Created via File > New > STM32 Project (using the STM32 Project Wizard).

Selected my MCU/board .

Expected Behavior:

A .ioc file should appear in the project root after setup (enabling peripheral/clock configuration).

Actual Result:

Only standard project files (e.g., Core/, Drivers/, .project) are generated. No .ioc file exists.

I cannot open/configure the project in STM32CubeMX.

This topic has been closed for replies.
sami_bahlousBest answer
Associate
Jul 22, 2025 9:26 AM UTC

Thank you @AScha.3 for sharing this solution — it does help, but it's actually a temporary workaround.

When you delete the following files or folders:

  • .stm32cubemx

  • .stm32cubeide

  • .stm32cufinder

  • .metadata/.plugins/org.eclipse.e4.workbench/workbench.xmi

STM32CubeIDE will:

  • Rebuild its internal caches and indexes

  • Reset corrupted UI/plugin states

  • Stop referencing corrupted paths

This effectively gives you a clean environment, which is why the issue disappears temporarily. However, since the IDE may eventually rebuild the same corrupted state, this doesn't fix the root cause — it just resets the environment.

What actually worked for me:
Upgrading STM32CubeIDE from version 1.17.0 to 1.19.0 solved the issue permanently.

6 replies

AScha.3
Super User
Jul 15, 2025 4:06 PM UTC

Hi,

seems to be "actual" problem, i had also;

Please try to

-Close STM32CubeIDE

-Delete all those files from your PC: .stm32cufinder, .stm32cubemx, .stm32cubeide and .stm32cube 

AScha3_0-1752595552330.png

 

then restart the STM32CubeIDE and retest again.

 

If still strange problems, you could try :


 >>  To fix this, just remove this file inside your workspace:
 >>  .metadata/.plugins/org.eclipse.e4.workbench/workbench.xmi
 >>  Hope this solves the issue.
 >>  (this file is the responsible of saving your workbench layout)

Then start IDE and see...and tell.

 

If you feel a post has answered your question, please click on " Best Answer ".
Associate
Jul 15, 2025 4:08 PM UTC

where can i find those files : .stm32cufinder, .stm32cubemx, .stm32cubeide and .stm32cube

 

AScha.3
Super User
Jul 15, 2025 4:41 PM UTC

oh...

on Linux : in your home directory,

on Win...first set file browser settings , to show "hidden" and system files, = all files;

also in your home directory,

 

 

 

on what system you are ?

If you feel a post has answered your question, please click on " Best Answer ".
Andrew Neil
Super User
Jul 15, 2025 4:43 PM UTC
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
Jul 22, 2025 9:34 AM UTC

See the pinned post on this known issue:

STM32CubeIDE STM32Cube project creation issue

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.