Skip to main content
Associate II
Aug 12, 2023 10:53 AM UTC
Solved

CubeIDE forcing you to login to ST is complete [...]

I don't care if the title of this post breaks some sort of forum usage rule, I just need to make it absolutely plain that I am sick and tired of every last company on Earth insisting I have an account with them and use it whenever I so much as breathe, drink a glass of water or, Chtuluh forbid ! update a HAL library for a microcontroller.

I believe there are more than enough bugs in CubeIDE, let alone actual necessary features that are missing, to keep your developers occupied forever. You did not need to waste everyone's time forcing people to login to ST. This feature brings nothing, helps no one but yourselves, and was asked by absolutely nobody, ever. So please, may I suggest you rethink this stupid, bordering on evil new addition to CubeIDE, and remove it with the next version ?

FYI, some of us work in companies where our computers are not, must not and cannot be, connected to the internet. It's already tough enough installing some of your HAL libraries (the patches) while being offline, we do not need the additional hassle of a login system that does nothing useful anyway.

A tool has to be convenient. If my screwdriver required an internet connection so as to snitch on how many turns I do in each direction depending on my GPS location, I'd start considering switching to fingernails or rocks.

You are welcome to try and make a case as to why you need me to log in to download updates to stuff you provide free of charge. I do need a good laugh.

Oh and I haven't checked on my last CubeIDE ticket... did you finally fix the bug where CubeIDE is confused when launching firmware on a target with Flash banks swapped ? Because that would sure be of actual use to the legions of programmers doing FOTA.

This topic has been closed for replies.
Amel NASRI
Amel NASRIBest answer
ST Technical Moderator
May 21, 2024 8:46 AM UTC

Hello,

For our Community members who faced login issue with STM32CubeIDE or STM32CubeMX, please refer to this post where explanation is provided and there the confirmation that problem is resolved.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.

53 replies

Tobe
Senior III
Dec 4, 2023 8:06 AM UTC

Maybe some have other ideas as just tracking? Today it is a login, but tomorrow it could be a login with a monthly payment... Just like the boiling frog: heat the water slowly.

Associate II
Dec 8, 2023 7:22 AM UTC

I don't think the ST tools will ever be sold or within a renewable subscriptions process like MS do with their products. The force of this ST SW ecosystem is to be free and largely used by customers to test-and-try examples, make their choice for an MCU, then buy an eval board and develop a more or less complex application for it.

When SW tools are free, they have to make their users buy the HW for the business model to stay profitable.

In return, these tools need to be qualitative enough not to make the users feel they have been fooled by this model.

Harvey White
Senior III
Dec 11, 2023 4:46 PM UTC

This has several subjects to address:

On the topic of drivers.  Look at the drivers for an AVR or simpler processor.  The hardware is simple enough that writing low level drivers for I2C are reasonable to do (and I've done some). 
On the other hand, the hardware for the I2C interface (for an example) has a lot of modes, and drivers provided by the manufacturer are highly recommended.  A purist would say "go write your own".  I am not a purist.  If the manufacturer cannot write decent drivers for their own hardware, then what?

The LL drivers are just enough to load registers.  You need to figure out what the registers do.  OK...  HAL drivers?  They need to document them, not so much how to use them, but what their assumptions are.  Are their effective mutexes to keep the hardware safe from multiple uses?  There needs to be in an operating system environment.  Are they provided by HAL?  I'm not sure.

I have drivers which encapsulate the HAL drivers.  They are operating system dependent (FreeRTOS), C++ classes that enable programmed NSS, address lines, R/W lines, mutex protection, and changing clockrate for different chips, etc. Changing for a different operating system simply requires changing mutex access.

Should ST have provided them?  Nope. Should it tell me how the HAL drivers were designed?  Yep.

As far as monitoring goes, it seems to split into two different subjects:

  1. Monitoring logins and requiring logins to access data:  enough has been said here to indicate that most people seem to be bothered enough to complain, but not enough to quit using the product.  In the case of some environments, internet access is not possible for either security reasons or the simple "it's not here".  Since the content of GitHub and the manufacturer's download seems to be different, GitHub is not really sufficient if you want what ST has.
  2. Constant update to refresh ST tools:  Now I think that's a bit much at times.  The CubeMX application gets shut down at times to do some file structure changes on the project software.  Start it back up and it wants to make sure everything is up to date.  Annoying.  I know there are settings, but still....   

What would be nice to see is a plan from ST that acknowledges some of these issues, and whether or not they will be addressed, and how.  Note that this is NOT a product development state secret, since it is unrelated to how the product hardware (processors) will be designed, what's next, etc.

Making your customers feel better is a good business goal.

 

 

 

 

 

Graduate
Dec 20, 2023 8:26 AM UTC

Login required for every single small thing is so annoying. Want datasheet for our processor? Oh, you need to login.

You need some utility right now when you are on site? Ok, just login. You forgot which email/password you use? Nevermind, just reset your password or create new account. We will answer in few hours.

Oh, You want to download library? You know the drill...

If they are afraid of bots, they should use some captcha alternative.
What will be next? Like and subscribe?

Associate II
Dec 20, 2023 12:13 PM UTC

As far as I know, login is not *yet* required to download datasheets, programming manuals or any technical document from Docs & Resources menu. It means that as of today ST is not interested in doing analytics of these downloads. But one day could come where they could have this great idea. You never know, downloading a specific application note would say a lot about your usage of the MCU ! Tracking only a version of a FW pack or peripheral used in a project is not very talkative finally.

Never tested the "Forgot your password ?" thing, so I can't tell...

What's next ? Receiving newletters ? Fill-in a survey at each session ?

Agree with you about other ways to register a user. Maybe they just don't know but the anonymous login is commonly used around.

Piranha
Principal III
Dec 21, 2023 1:20 AM UTC

The analytics on documentation and other downloads can and already are gathered without a login.

@Oskar_H , a silent opt-in on newsletters are already executed in some cases:

https://community.st.com/t5/feedback-forum/st-marketing-abuse/td-p/596281

@Harvey White , what you are describing with your higher layer drivers is the platform/OS layer depicted as the "Driver" (yellow) layer in this picture:

https://microchip.wdfiles.com/local--files/harmony:overview/harmony.jpg

The HAL belongs to the hardware "PLIB" (red) layer and should provide the interrupt safety, but not the access control. Instead the famous broken "HAL lock" tries to do both, but doesn't actually provide any of those, while simultaneously adding an unjustified way of failure under a basic and completely normal usage. A spectacular failure, which just shows that the developers do not understand what they are doing...

Harvey White
Senior III
Dec 21, 2023 1:56 AM UTC

Which now (not that it had an explanation before) explains the "HAL_lock".  Apparently a good thing that I managed to wrap the function in my own operating system choice of semaphores. 

Now if we only had a decent explanation of how the rest of it worked, and what they thought they were doing.

I'll agree that task interlocking with semaphores is another level up.  Wonder why we had to go to a rival manufacturer to find that out?

Wonder if a decent explanation of HAL (and LL) drivers might mention some sort of layer model?

It's beyond expectations to teach people how to design software for a manufacturer of chips.  Not their job.  However, a small document that describes software levels and what part their software plays, and where it is, well.......

For a company that espouses Azure as a wonderful solution (and second lines FreeRTOS), if we're doing operating systems.  Somewhere I managed to find some supporting documentation.

Why am I not surprised?

Eventually, documentation will make or kill your product.  Wonderful to have advanced features and "golly gee whiz" hardware.  Now to figure out how to use it (and the application notes are not all that good in places).

 

 

Harvey White
Senior III
Dec 21, 2023 2:11 AM UTC

As a further clarification, I should mention that things are often more complicated than this.  Let's take the example of an INA-219 current monitor chip interfaced with I2C.  The following levels are available:

  1. Hardware: connected to chip
  2. I2C driver provided by ST.
  3. HAL_I2C for each interface used.  Has Semaphores and encapsulates some higher composite functions.  Those functions vary per chip and interface.
  4. CHIP driver, using the HAL_I2C composite driver.  Talks to the chip and provides register level interface, functional interface, and chip specific functions
  5. SYSTEM_CHIP driver.  Uses CHIP driver.  This allows multiple local chips on multiple I2C interfaces, and depending on the system architecture for the project, allows packet communications over local, NRF, WIFI, serial, or I2C_networking to another processor which contains the interface to the desired chip on another board.
  6. APPLICATION PROGRAM, interacts with the SYSTEM_CHIP driver only.  Only needs to talk to a particular chip at a particular node address, the operating system and driver take care of all the rest.

This works for me, structure wise. It's designed for multiple board, multiple processor use in a distributed system

 

 

Tobe
Senior III
Dec 21, 2023 1:42 PM UTC

I think you posted in the wrong thread...

Graduate II
Mar 5, 2024 9:57 AM UTC

The log-in function in my IDE isn't even working.  It just does nothing.

So now I'm stuck.

ST...  we really don't need this log-in nonsense.

If you really must force it on us, you need to make sure it is 100% reliable - and it ain't.

This is wasting my valuable time.

Slh
Senior
Apr 22, 2024 7:48 AM UTC

After a while, a project with STM32. I forced to log-in... I just want to know where is this feature really useful and why we must be log-in?

CBerg
Senior II
Apr 22, 2024 7:54 AM UTC

@Slh as far as I am concerned: nope, this BS is not usefull at all - at least for the users. It's just annoying.

 

Associate III
May 15, 2024 5:42 AM UTC

I cannot login in the STM32CubeIDE, it keeps faling, I can login in the browser, but I cannot download the software for reinstall, everytime it keeps promting me for loggin into stm again, even that I already is logged in. I have a plain private internet connection without any additional firewall than the one there is on my computer. I do not use vpn.

i have also tried to disable my firewall, still no luck, Have also tried hotspot on my phone.
I have tried all three network settings under the preferences.

i you want us to login it would be great if it worked

 

AScha.3
Super User
May 15, 2024 5:55 AM UTC

You have to login in the IDE, not in a browser.

In IDE in it's menu.

Did you try that?

ed

Ok, i see now ... login in IDE not working... perfect !

If you feel a post has answered your question, please click on " Best Answer ".
Visitor II
May 15, 2024 9:14 AM UTC

I've got the same issue. There is no logging (IDE) possible.

Got a window "User Authentication Dialog", then, after some time "Connection lost".

I'm working in a "private enviroment", every other application, app, straming,.... which uses internet is working fine.

So please . remove this bug!

Thanks Winfried