Skip to main content
NikolaiB
Associate II
Jan 4, 2026 8:18 PM UTC
Solved

Can not start debug session STM32CubeIDE (ST-Link, Nucleo-F767ZI)

Hello all,

I get an error starting a debug session from STM32CubeIDE (1.18.1) (STM32 Nucleo-F767ZI):

STMicroelectronics ST-LINK GDB server. Version 7.10.0

Copyright (c) 2025, STMicroelectronics. All rights reserved.

Starting server with the following options:

Persistent Mode : Disabled

Logging Level : 1

Listen Port Number : 61234

Status Refresh Delay : 15s

Verbose Mode : Disabled

SWD Debug : Enabled

InitWhile : Enabled

Target USB comms error

Error in initializing ST-LINK device.

Reason: USB communication error. Please reconnect the ST-LINK USB cable and try again.

 

NikolaiB_1-1767557351681.png

If I switch to SEGGER J-Link everythink works fine.

Is my debug configuration:

NikolaiB_2-1767557469777.png

What I tried:
- Restart PC
- Reinstall the USB-Driver (https://www.st.com/en/development-tools/stsw-link009.html)
- Erased the flash with STM32CubeProgrammer
- Changes USB cable
- Googled for solutions

Please help

Best regards

Nikolai

 

 

 

NikolaiB
NikolaiBBest answer
Associate II
Jan 7, 2026 5:29 PM UTC

Hello all! Here comes the solution!

After reflashing the ST-Link debug probe with ST-Link firmware using STLinkReflash, an update by meens of STLinkUpgrade has to be conducted. STLinkUpgrade is a tool inside the CudeIDE (Help->STLinkUpgrade)(screenshot).

NikolaiB_0-1767806616410.png

I suppose, the STLinkReflash (Segger Tool) ist outdated. Is has version 190812 (2019.08.12). But it is the latest version currently.

After the "uprade" debugging from the CudeIDE works fine. So switching between SEGGER J-Link und ST ST-Link is now possible.

Best regards

Nikolai

 

13 replies

NikolaiB
NikolaiBAuthor
Associate II
Jan 4, 2026 9:33 PM UTC

I switch between ST-Link and J-Link with the STLinkReflash-Tool. That works fine. If J-Link is flashed I can start a debug session from the STM32CubeIDE and from the SEGGER-Tools (Ozone, SystemView). But if I change to ST-Link, I get the error. 

NikolaiB_0-1767562396620.png

 

NikolaiB
NikolaiBAuthor
Associate II
Jan 5, 2026 12:07 PM UTC

I tried it with version 2.0.0 of the STM32CobeIDE, but it didn't help. Same problem.

NikolaiB
NikolaiBAuthor
Associate II
Jan 5, 2026 12:10 PM UTC

All jumpers are default. I haven't changed anything.

NikolaiB_0-1767615020516.jpeg

 

 

Andrew Neil
Super User
Jan 5, 2026 12:20 PM UTC

Does CubeProgrammer connect OK?

Has this board ever worked for you?

More things to try here.

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
NikolaiB
NikolaiBAuthor
Associate II
Jan 5, 2026 12:35 PM UTC

I can flash the ST-Link debug probe withe J-Link or ST-Link. If the J-Link firmware is running I can connect via the CubeProgrammer. Then erase or flash the MCU. If the ST-Link firmware is running on the debug probe, I have the described problem. But the CudeIDE detects the MCU!!!

NikolaiB_0-1767616427719.png

 

ST Technical Moderator
Jan 5, 2026 12:23 PM UTC

Hello @NikolaiB and welcome to the Community

Did you try reinstalling ST-LINK server software ?

Ensure debug pins (SWDIO, SWCLK) are not assigned to other signals.

Check also the option bytes for correct configuration.

Try to connect under reset mode.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
NikolaiB
NikolaiBAuthor
Associate II
Jan 5, 2026 12:44 PM UTC

I have installed the ST-Link server. I see in the task manger that it is a 32Bit application. I have a 64 bit OS. Could that be a problem?

NikolaiB_0-1767617073983.png

 

NikolaiB
NikolaiBAuthor
Associate II
Jan 5, 2026 1:18 PM UTC

I just ordered a new Nuceo-Dev-Board to exclude any hardware issues. Will take a week to arrive.

NikolaiB
NikolaiBAuthorBest answer
Associate II
Jan 7, 2026 5:29 PM UTC

Hello all! Here comes the solution!

After reflashing the ST-Link debug probe with ST-Link firmware using STLinkReflash, an update by meens of STLinkUpgrade has to be conducted. STLinkUpgrade is a tool inside the CudeIDE (Help->STLinkUpgrade)(screenshot).

NikolaiB_0-1767806616410.png

I suppose, the STLinkReflash (Segger Tool) ist outdated. Is has version 190812 (2019.08.12). But it is the latest version currently.

After the "uprade" debugging from the CudeIDE works fine. So switching between SEGGER J-Link und ST ST-Link is now possible.

Best regards

Nikolai

 

Andrew Neil
Super User
Jan 7, 2026 6:05 PM UTC

@NikolaiB wrote:

Here comes the solution!


Thanks for that - please mark it as the solution.

 


@NikolaiB wrote:

I suppose, the STLinkReflash (Segger Tool) ist outdated.


Please raise that with Segger:

https://forum.segger.com/board/4-j-link-flasher-related/

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.