WATCH ON-DEMAND | STM32 Summit 2026
Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.
Most recent activity
There is official errata named "2.5.6 Indirect write mode limited to 256 Mbytes" where indirect OSPI write requests for addr >256MB are written to invalid target address. I tested the behavior and it seems address is effectively truncated to 28bits. Contrary to what errata says, I can see the same truncated address also for indirect reads.From what I see the problem is affecting NORs only because NAND uses page addressing in 0x13/0x10 cmds and these are always smaller than 24bits.Is the assumption correct ?Martin
Product:MCU/SoC: STM32MP2Description:In our ST Linux environment, the hantro-vpu driver registers:/dev/video5 -> VDEC (H.264/VP8 Decoder)/dev/video6 -> VENC (H.264/VP8 Encoder) We want to implement direct V4L2 API usage for H.264/VP8 encoding and decoding, without using GStreamer.Specific Questions: Are there official minimal examples or demos using pure V4L2 API for H.264 / VP8 encoding/decoding?DMA Usage: Is it possible to use DMA for input/output buffers in V4L2 mem2mem mode on STM32MP2 Hantro VPU? If yes, what is the recommended configuration and constraints?
Hi,I have a OTP provisioning script that wrote OTP 1 with value 0x000000ff, executing a partial close of security state B. The board now passes ROM/FSBL/OP-TEE/U-Boot but resets when the Linux kernel probes the first RIF-protected peripheral (HPDMA3). Disabling HPDMA3 in DT causes the same reset on HPDMA2, indicating closed-state RIF policy is being enforced globally regardless of the device tree configuration applied by OP-TEECan the board be returned to a open state using an rma procedure? Kind Regards,Jack Redpath
I am trying to collect images from a MIPI camera that is not supported by default on the STM32MP257F-DK, but for which I have a driver. With that driver, it's seeing the camera as an attached device, and I can see it in the dmesg output and also as /dev/media2 in v4l2-ctl --list-devices. I have followed the steps at this link (modified to use the imx664 instead of imx335), and also steps I have found elsewhere (below). Is there anything I need to look for or change in order to actually see image frames from the camera, now that I can see the camera itself?media-ctl -d /dev/media2 -rmedia-ctl -d /dev/media2 -l "'48020000.csi':1 -> 'dcmipp_input':0 [1]"media-ctl -d /dev/media2 -l "'dcmipp_input':2 -> 'dcmipp_main_isp':0 [1]"media-ctl -d /dev/media2 -V "'imx664 0-0010':0 [fmt:SRGGB12_1X12/2704x1540]"media-ctl -d /dev/media2 -V "'48020000.csi':1 [fmt:SRGGB12_1X12/2704x1540]"media-ctl -d /dev/media2 -V "'dcmipp_input':2 [fmt:SRGGB12_1X12/2704x1540]"media-ctl -d /dev/media2 -
The STM32MP135 is powered by PMIC1A. After initial power-up, the voltage at BUCK4 is normal at 3.3V, but during U-Boot flashing, the output voltage at VOUT4 drops to only 2.4V, causing the flashing to fail. The VDD and VDDQ pins of the eMMC are powered by the same power rail, VOUT4.
Hi, I tried exporting the IBIS model from ST website. On importing model to SI tool I can see that there is no model assigned to DSI lines. It is showing NC. Can you share the IBIS model with MIPI drivers in it. or share some IBIS model which I can use for my simulation of MIPI line interface
Hi everyone,I am working on an STM32MP2 platform and facing a persistent issue with LPUART1 in interrupt mode.SetupMCU: STM32MP2UART used: LPUART1 (RS485 communication via MAX485)Debug UART: UART5 (polling mode, printf works fine)Using:HAL_UARTEx_ReceiveToIdle_IT() for RXHAL_UART_Transmit() for TXBaudrate: 115200ProblemWhen using interrupt mode, the system gets stuck in: HAL_UART_IRQHandler()The interrupt keeps triggering continuously and the system appears stuck (infinite IRQ loop).ObservationsPolling mode (HAL_UART_Receive) works perfectlySensor communication works fine in pollingIssue only happens in interrupt modeWhat I already checked NVIC enabled correctly:HAL_NVIC_SetPriority(LPUART1_IRQn, 5, 0);HAL_NVIC_EnableIRQ(LPUART1_IRQn); IRQ handler is correct:void LPUART1_IRQHandler(void){HAL_UART_IRQHandler(&hlpuart1);}No wrong handle (huart1) is used anywhereFIFO configuration added:HAL_UARTEx_SetTxFifoThreshold(&hlpuart1, UART_TXFIFO_THRESHOLD_1_8);HAL_UA
Hello,I don't have so much experience with the boards of STM32 and I'm struggling a bit (actually a lot) with a quite simple task.I want to run a blinking test with the board STM32MP257F-EV1.I installed the STM32CubeMX, STM32CubeIDE and STM32CubeProgrammer.First I generated the code with CubeMX and added the code for blinking in the CubeIDE. Then I clicked on Run -> Debug and there was this error:Error message from debugger back end:Remote communication error. Target disconnected: (undocumented errno 10061).I changed the BOOT switches to 0 1 0 0, and then did Run -> Debug again. This time there was this error:Open On-Chip Debugger 0.12.0+dev-00608-gd8ed48fef (2025-02-06-11:17) [https://github.com/STMicroelectronics/OpenOCD]Licensed under GNU GPL v2For bug reports, readhttp://openocd.org/doc/doxygen/bugs.htmlsrst_only srst_pulls_trst srst_gates_jtag srst_open_drain connect_deassert_srstInfo : Listening on port 6666 for tcl connectionsInfo : Listening on port 4444 for telnet connec
Hi,I'm working on to get the multiple SAI to Codec to work synchronized as the connection below,1x MCLK1x BCLK1x FSYNC4x DIN4x DOUTWhere the three Clocks 1x lines (MCLK, BCLK & LRCLK) from one SAI master (actual pinout clock) & other SAI (pinout DIN & DOUT) sync clock internally (not sure possible b/w the SAI).SAI1 (clock master) -> MCLK, BCLK, FSYNC, DIN/DOUT -> codec1SAI2 (clock slave) -> (SAI1 MCLK, BCLK, FSYNC), DIN/DOUT -> codec2SAI3 (clock slave) -> (SAI1 MCLK, BCLK, FSYNC), DIN/DOUT -> codec3SAI4 (clock slave) -> (SAI1 MCLK, BCLK, FSYNC), DIN/DOUT -> codec4According to the TRM RM0436 Rev 7 55.4.4 External synchronization should be used between the SAI.does this need external pin connection between two SAI (all three clocks)? I'm facing error when arecord on SAI1 in the background and trying to start playback on SAI2, attached dts overlay filearecord -D hw:0,0 -f S16_LE -r 48000 -c 2 -d 0 /dev/null &sleep 1aplay -D hw:0,2 -f
Hi everyone,I'm currently validating a custom board featuring the STM32MP257 interfacing a single 16-bit DDR4 at 2133MT/s (Point-to-Point topology). I am using the ST-provided Excel tool ("Examples of DDR memory routing on STM32MP2 MPUs") to extract the Die-to-Ball Package Trace Lengths (mm).I’ve run into a few specific SI conflicts regarding the hardware guidelines, primarily driven by my PCB stackup. Due to routing density, my Address/Command (A/C) signals are split across two different layers:L6 (Bottom Layer): Microstrip. Outer solder mask is 0.6mil (Dk 4.85) over a 3.91mil 3313 Prepreg (Dk 4.4). Effective Dk is much lower due to air exposure.L3 (Inner Layer): Stripline. Sandwiched between a Core (Dk 4.6) and Prepreg (Dk 4.5). Effective Dk is approx 4.5.This leads to the following questions:1. Balancing Physical Length (mm) vs. Electrical Delay (ps): The ST guideline dictates an A/C to CLK_P/N equalization of +/- 140 mils (3.55 mm). However, if I strictly match the physical length
Hi,I recently just finished the Yocto Bringup of a custom STM32MP15FAA1. Everything seems to be working in my application. I am now looking to begin development of the M4 in which I need access to either SWD or JTAG to do lower-level development. Unfortunately, I am having trouble connecting to either interfaces through both CubeIDE and also manually inputting OpenOCD in an IDF Powershell instance.I presume the easiest way to get to my goal is to setup SWD which on the MP15 maps to TMS (SWDIO) and TCLK (SWCLK) and I connected GND and VCC. My STLinkV3-MIME detects 3.3V on the reference line but can never connect to target. This is my first time working with a SOM as most of my development is on base Cortex M microcontrollers so I have a few questions.1. Is there anything in the M4 device tree that can be preventing JTAG from operating like the STPMIC? I do have M4 RPROC enabled in my device tree and the file descriptor is available for me to access.2. Does the boot mode matter? My end a
Hi,I'm designing a board with STM32MP153FAD and have a question about DDR layout reference.Which reference should I follow for the DRAM section?Eval kit MB1272C_03 layoutST's published reference DDR layout.Questions:Which is the recommended reference for custom board design?Is there a design guide specifically for STM32MP153 DDR layout and routing guidelines?Is there a document listing pin delays for the FAD series SoCs? This would be helpful for length matching calculations.Best regards,Batuhan
Hello,I'm stalling with an issue with Optee on a custom board with 256 MB of ram and an STM32MP135D.The environment was working with the DK (MP135F and 512M ram).I followed the guide for the configuration with 256 MB of ram (https://wiki.st.com/stm32mpu/wiki/How_to_configure_a_256MB_DDR_mapping_from_STM32_MPU_Distribution_Package), however it panics as soon as optee starts.Am I missing something or do you have some hints?Thank you NOTICE: CPU: STM32MP135D Rev.Y NOTICE: Model: STMicroelectronics custom STM32CubeMX board - openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06 ERROR: nvmem node board_id not found INFO: PMIC version = 0x21 WARNING: VDD unknown WARNING: stm32_rng_init: No RNG found in device tree. NOTICE: Reset reason (0x35): INFO: Power-on Reset (rst_por) INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe0000 INFO: FCONF: Reading firmware configuration information for: stm32mp_fuse INFO: FCONF: Reading firmware configuration information for: stm32mp_io INFO:
Hello,There seems to be an issue with the I2C addresses listed in the MB1854 (B-CAMS-IMX) documentation and schematics (B01/B02).The documents show:IMU: 0xD4 / 0xD5ToF: 0x52However, these appear to be 8-bit addresses. The correct 7-bit I2C addresses should be:ToF (VL53L5CX): 0x29IMU (ISM330DLC): 0x6A / 0x6BThis can cause confusion when using standard I2C tools or drivers.Could you please clarify or update the documentation to specify the address format (7-bit vs 8-bit)?Thanks.
Section 2 of this page shows how to setup python for building firmware. It seems the rest of the tutorials assume you are building on a modern Ubuntu, so I would suggest changing the following lines:pip install pyelftoolspip install pycryptodomexto:sudo apt install python3-pyelftoolssudo apt install python3-pycryptodomeI would also suggest adding:sudo apt install python-is-python3 My reasons are that you can not/should not install the above packages to the global python environment with pip. Also, the makefiles for M33 firmware call 'python' which does not exist on a new ubuntu install (well, it didn't on mine). Installing python-is-python3 is the recommended way to resolve this. Alternately use a virtual environment, but the firmware build system seems to assume use of the global python.
Are there STM32CubeMX files for the example projects in STM32Cube_FW_MP2? It would really help understand peripheral configuration. Specifically the .ioc file for the OpenAMP example project used in this tutorial.I am trying to better understand STM32CubeMX peripheral setup, especially in regard to how each peripheral can be selected for each core in secure or non secure mode. And how that interacts with the Linux device tree.
I flash the image from FlashLayout_sdcard_stm32mp257f-ev1-ca35tdcid-ostl-m33-examples-optee.tsv pi@inspiron:~/yocto/build-openstlinuxweston-stm32mp2/tmp-glibc/deploy/images/stm32mp2$ STM32_Programmer_CLI -c port=usb1 -w flashlayout_st-image-weston/optee/FlashLayout_sdcard_stm32mp257f-ev1-ca35tdcid-ostl-m33-examples-optee.tsv I copy stm32mp257f-ev1-ca35tdcid-ostl-m33-examples.dts from the following directory. pi@inspiron:~/yocto/build-openstlinuxweston-stm32mp2/tmp-glibc/work-shared/stm32mp2/external-dt/linux$ ls Makefile stm32mp257f-dk-ca35tdcid-ostl-resmem.dtsi stm32mp135f-dk-rt.dts stm32mp257f-ev1-ca35tdcid-ostl.dts stm32mp157f-dk2-rt.dts stm32mp257f-ev1-ca35tdcid-ostl-m33-examples.dts stm32mp157f-ev1-rt.dts stm32mp257f-ev1-ca35tdcid-ostl-m33-examples-resmem.dtsi stm32mp257f-dk-ca35tdcid-ostl.dts stm32mp257f-ev1-ca35tdcid-ostl-resmem.dtsi stm32mp257f-dk-ca35tdcid-ostl-m33-examples.dts stm32mp257f-ev1-rt.dts stm32mp257f-dk-ca35tdcid-ostl-m33-e
Dear all,We have a design where the VCCQ of eMMC is currently 3.3V. We need to move to 1.8V to be able to use a new referenceIs there any risk to break somthing if I use the below DTS on board where eMMC is 3.3V VCCQ. We have pull up to VCCQ on D0 and CMDvqmmc-supply = <&v1v8>; mmc-ddr-1_8v;According to my tests, system is up and running, but I fear this should have an impact on MPU padsIf no risk, this could avoid me to add a DTS overlay according to my hardware board version in case of 3.3V VCCQI add my layout for eMMC for better understanding, see R353 and R356 to switch VCCQThanks in advance for answers and hintsRegardsLaurent
Hi!I have a STM32MP257F processor. The clock for SDMMC1 is constant at 3.3V. Therefore the U-boot cannot read the SD-card.My question is: What clock need to be active/chosed in the device tree so it u-boot can read the SD-card sdmmc1? Hit any key to stop autoboot: 0 Boot over mmc0! Saving Environment to MMC... stm32_sdmmc2 mmc@48220000: stm32_sdmmc2_getcd called stm32_sdmmc2 mmc@48220000: bus_with = 1, clock = 0 stm32mp25_reset clock-controller@44200000: reset id=69 offset=0x830 bit=0 status=1 stm32mp25_reset clock-controller@44200000: reset id=69 offset=0x830 bit=0 status=0 D/TC:? 0 tee_ta_init_session_with_context:562 Re-open trusted service a8cfe406-d4f5-4a2e-9f8d-a25dc754c099 F/TC:? 0 pta_scmi_invoke_command:404 SCMI command 0x3 ptypes 0x3 F/TC:? 0 pta_scmi_invoke_command:404 SCMI command 0x4 ptypes 0x651 F/TC:? 0 regulator_disable:142 v3v3 D/TC:? 0 tee_ta_close_session:465 csess 0x8212f890 id 1 D/TC:? 0 tee_ta_close_session:484 Destroy session D/TC:? 0 tee_ta_init_session_wi
The project requirement is to use optical ethernet with STM32MP257F. I want to try this interfacing first at STM32MP257F EV1 with some copper to optical Ethernet converter module, but in STM32MP257F EV1, Ethernet pins are not available for interfacing. Kindly suggest some solution for using optical ethernet with STM32MP257F. Kindly send the solution as early as possible. Thank you With Best Regards, Dr. Amruta S. Dixit
Hello,I am following AN4803 to simulate my board with an STM32MP151 with DDR3L memory, but there seems to be a problem with the IBIS model. These IBIS models have missing receiver voltage thresholds, which may affect analysis:IBIS File: C:\Users\...\IBIS\stm32mp151_153xaa_lfbga448_sm.ibsIBIS Model: MSD_D3RP3L_48Model does not have a [Receiver Thresholds] section.Only Vinh and Vinl thresholds are specified in the [Model Spec] section, and will be used for both AC and DC thresholds.Net: $9I75\DDR_DQ0Controller pin: U1.E21 (DDR_DQ0)Net: $9I75\DDR_DQ1Controller pin: U1.F21 (DDR_DQ1)Net: $9I75\DDR_DQ2Controller pin: U1.H21 (DDR_DQ2)Net: $9I75\DDR_DQ3Controller pin: U1.E20 (DDR_DQ3)Net: $9I75\DDR_DQ4Controller pin: U1.J21 (DDR_DQ4)Net: $9I75\DDR_DQ5Controller pin: U1.H20 (DDR_DQ5)Net: $9I75\DDR_DQ6Controller pin: U1.H22 (DDR_DQ6)Net: $9I75\DDR_DQ7Controller pin: U1.G19 (DDR_DQ7)Net: $9I75\DDR_DQ8Controller pin: U1.N22 (DDR_DQ8)Net: $9I75\DDR_DQ9Controller pin: U1.R21 (DDR_DQ9)Net: $9I75
I am using the STM32MP131 in a baremetal environment. Since there is no internal flash, I am planning to use external flash and DDR.I have confirmed that writing to and reading from the flash works, but I don't know how to start from FLASH instead of SYSRAM when powering on.I saved the FW's bin data at address 0 of the Flash and tried changing the boot mode to QUADSPI Flash, but it did not work.I think QUADSPI needs to be activated before reading and executing from Flash. Where should I activate this?Do I also need to modify the linker script for the firmware that runs from Flash? Please let me know if you have any solutions to this problemThank you very much in advance.
Hi,I’m working with a MYIR MYD-YA157C (STM32MP157AAC) board and I’m trying to restore a board using STM32CubeProgrammer (USB / DFU mode) with a FlashLayout TSV.The board is custom made , but the HW should not be a problemBut i am running into erorr: 16:47:55 : Download in Progress:16:47:56 : Error: failed to download Sector[0]16:47:56 : Error: failed to download the File16:47:56 : Error: Download partition 0x21 failed16:47:56 : Error: TSV flashing service failed16:47:56 : Disconnected from device. Little bit of a backgroundThe chip comes with preloaded yocto , and after trying to flash our distro we get this erorr I tried the following thingsRemove everything from the EMMC - Nothing helpsChaning offsets - Did not helpUse UDF tool - Did not helpTried on different computer - Did not helpTried different cable - Did not help It is very strange I attached logs from Cube programmer @Aimen1 Could somebody help us with some suggestions
I am working with the STM32MP257F-DK using the official Starter Package. Suddenly, the board entered a state where several power rails are disabled. The ST-LINK LED (LD5) is blinking red slowly, and there is no HDMI output (0V on the rail) I have SSH access via USB OTG (usb0), but the system is in a "degraded" state.The ST-LINK is not recognized by the PC.HDMI monitor detects no signal. Diagnostic Data (Output of grep "" /sys/class/regulator/*/state): I have attached a screenshot, but here are the critical regulators currently in disabled state:regulator.11 (vdd3v3_usb) -> disabledregulator.12 (v5v_hdmi) -> disabledregulator.3 (vddio3) & regulator.4 (vddio4) -> disabledregulator.7 (vddcore) -> disabled (Surprisingly, since the CPU is running).Attempts to fix: Tried to enable them via sysfs: echo enabled > /sys/class/regulator/regulator.12/state -> Result: Permission denied.Tried to force it via I2C: i2cset -f -y 0 0x33 0x93 0x01 -> Result: Write
For the STM32MP135 series, specifically the STPMIC1A I'm using, can VDD_CORE and VDD_CPU share the same power rail (buck1)?
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.