Skip to main content
Associate
Apr 30, 2026 1:16 AM UTC
Solved

PMIC-related issues

The STM32MP135 is powered by PMIC1A. After initial power-up, the voltage at BUCK4 is normal at 3.3V, but during U-Boot flashing, the output voltage at VOUT4 drops to only 2.4V, causing the flashing to fail. The VDD and VDDQ pins of the eMMC are powered by the same power rail, VOUT4.

PatrickF
PatrickFBest answer
ST Employee
Apr 30, 2026 9:37 AM UTC

Hi @LH1 

have you excluded some SW going to change buck4 voltage thru I2C ?
Is eMMC IO supply on STM32MP135 at 3.3V too (check VDDSD1/VDDSD2 if relevant) ?


Could you share the board model you are using. Is it a custom board where HW is not yet trustable ?

Buck component choice and layout could be tricky.

Is the 2.4V clean and stable or oscillating ?

Please look into 
AN5474Getting started with STM32MP13x lines hardware development
DS12792 Highly integrated power management IC for micro processor units
AN5431 The STPMIC1 PCB layout guidlines

and maybe

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent

1 reply

PatrickF
PatrickFBest answer
ST Employee
Apr 30, 2026 9:37 AM UTC

Hi @LH1 

have you excluded some SW going to change buck4 voltage thru I2C ?
Is eMMC IO supply on STM32MP135 at 3.3V too (check VDDSD1/VDDSD2 if relevant) ?


Could you share the board model you are using. Is it a custom board where HW is not yet trustable ?

Buck component choice and layout could be tricky.

Is the 2.4V clean and stable or oscillating ?

Please look into 
AN5474Getting started with STM32MP13x lines hardware development
DS12792 Highly integrated power management IC for micro processor units
AN5431 The STPMIC1 PCB layout guidlines

and maybe

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent