STM32MP157 + MYD-YA157C: TSV flashing fails with “failed to download Sector[0]”
- 1 reply
- 217 views
Hi,
I’m working with a MYIR MYD-YA157C (STM32MP157AAC) board and I’m trying to restore a board using STM32CubeProgrammer (USB / DFU mode) with a FlashLayout TSV.
The board is custom made , but the HW should not be a problem
But i am running into erorr:
16:47:55 : Download in Progress:
16:47:56 : Error: failed to download Sector[0]
16:47:56 : Error: failed to download the File
16:47:56 : Error: Download partition 0x21 failed
16:47:56 : Error: TSV flashing service failed
16:47:56 : Disconnected from device.
Little bit of a background
The chip comes with preloaded yocto , and after trying to flash our distro we get this erorr
I tried the following things
Remove everything from the EMMC - Nothing helps
Chaning offsets - Did not help
Use UDF tool - Did not help
Tried on different computer - Did not help
Tried different cable - Did not help
It is very strange
I attached logs from Cube programmer
Could somebody help us with some suggestions