WATCH ON-DEMAND | STM32 Summit 2026
Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.
Most recent activity
Hi everyone,The stm32mp1 use SDMMC2 as default emmc controller. Now, I need use SDMMC1 to connect emmc flash. And I saw the OTP need changed. Bud I am confuse about IOs of SDMMC1. Does it also need setting some OTP bits to pinmux CK, CMD, D0?This picture show need change bit to chose SDMMC1.This picture is confused me. When I use SDMMC1, is it need configure CMD, CK,D0 to default pinmux on SDMMC1? If it is needed, where to configure those?
Hi Guys,Please I facing problem to have a QT application fitting the DSI screen,it sounds like it is 400x240 and not 800x480. I`m probably missing something on QTor on the STM32MP157C-DK2.Can someone please help-me to correct the resolution and how to use it landscape ?Thanks [ ]
I am trying stm32mp157f-dk2 for learning linux based on starter packageI just got succeed with load example 1 dtb and echo uart operating Anyway so I got checked the extlinux.conf file can control which dtb would be called But I dont know what's happening let me show what i wonder 1. Why stm32mp157c-dk2-extlinux.conf is called?2. Why load stm32mp157c-dk2.dtb? there's not FDT setting in default LABEL I can do with just change conf file in 157c-dk2 for nowBut i want to know how to select conf file Thank you
HelloI tried everything but I cannot get STM32CubeIDE to get the editor to work.I just keep on getting this message: There is no active editor that provides an outline.I spent hours re-installing but nothing workedAll help will be appreciated
Hello, my aim is to achieve a reliable receiving UDP speed with stm32mp13 while sending a payload of 150 mbit/s.I did performance tests of 1 gigabit Ethernet using a MYD-YF13X development board and iperf3. Here are some of my results:19% packet drop rate at 150 mbit/s is, for my purpose, unacceptable. I think the problem is related to either the MPU or the YT8521SH Ethernet PHY.But I doubt it is the second one, so I would focus on the MPU itself. It seems to me that the MPU is not fast enough to achieve a sensible >100 mbit/s receiving speed.The architecture is arm 32bit, which has 32KB cache memory inclusive.The amount of cache is decisive for receiving huge payloads. Could it be the reason for such a performance? What was the reason to put 100 mbit PHYs and not 1 gbit into the STM32MP135F-DK? Best,J. Schneider
Hi,I have STM32MP157f-DK2 . I built openstlinux-5.15-yocto-kirkstone-mp1-v22.07.27 , distro=openstlinux-eglfs , and I try flash image to sd card.When I am flashing "FlashLayout_sdcard_stm32mp157f-dk2-trusted.tsv" I have different errors related with partitioning ..., but when I am flashing "FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv", the board works....What can be wrong ?
Hello,I am trying the open-st-linux-eglfs distribution with my QT application.When QT load my QML I am facing with this error : module "QtQuick.Controls" is not installedHow can I verify the installation of qtquick control in my distribution ?
hi st experts:I am porting stm32mp2 software to my own robot board(stm32mp257D), after i finished my yocto build, i tried to download image to my board, there was a problem, it seems reconnect devices failed, STM32Cubeprogrammer log: 12:53:51 : STM32CubeProgrammer API v2.18.0 | Linux-64Bits 12:54:00 : UR connection mode is defined with the HWrst reset mode 12:54:00 : USB speed : High Speed (480MBit/s) 12:54:00 : Manuf. ID : STMicroelectronics 12:54:00 : Product ID : DFU in HS Mode @Device ID /0x505, @Revision ID /0x2000 12:54:00 : SN : 002B00254136501800353059 12:54:00 : DFU protocol: 1.1 12:54:00 : Board : -- 12:54:00 : Device ID : 0x0505 12:54:06 : Read TSV File: /mnt/ext_disk/code/myb_github/build-openstlinuxweston-zero-robot/tmp-glibc/deploy/images/zero-robot/flashlayout_zero-robot-image-core/optee/FlashLayout_emmc_zero-robot-stm32mp257x-2GB-optee.tsv 12:54:06 : Number of partitions: 14 12:54:14 : Start Embedded Flashing service 12:54:14 : Opening and
Hello, I am looking for a MPU as CAN FD master but couldn't find the type with explicit CAN FD support. I would inquire here to make sure I haven't missed any details, and also ask for more information about the availability of the high performance chip with CAN FD interface. Thank you!
I try to build a rpmsg sample app by following this instruction : https://docs.zephyrproject.org/latest/samples/subsys/ipc/rpmsg_service/README.htmlThe example repository here: https://github.com/zephyrproject-rtos/zephyr/tree/main/samples/subsys/ipc/rpmsg_serviceIt seems that the device tree overlay is missing for STM32MP157F-DK2, so I create one/ { chosen { /* * shared memory reserved for the inter-processor communication */ zephyr,ipc_shm = &mcuram2; zephyr,ipc = &mailbox; }; mcuram2: mcuram2@10000000 { compatible = "mmio-sram"; reg = <0x10000000 0x40000>; };It is not working, please advice if the device tree is correct or not? and Is there any relation with Linux device tree? thanks
Hi,When testing the stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v24.12.05 image, the LVDS screen doesn't work and blocks the board's startup (in u-boot) and I can't reset the board unless I disconnect the LVDS port.On the other hand, the HDMI is functional, and the screen works without any problem on my STM32MP257F-EV1 board.Note that the board is powered via a USB port capable of delivering up to 1.5A.Thank you
Hello,I am encountering an issue while building a Yocto-based image for the STM32MP157F-DK2. The problem arises when attempting to fetch the gcnano-userland-multi-binary-stm32mp package. Below are the details of the issue: Project DetailsYocto Version: Dunfell (OpenSTLinux 5.10-dunfell-mp1-23-11-01)Target Machine: STM32MP157F-DK2Recipe Name: gcnano-userland-multi-binary-stm32mpSoftware Version: gcnano 6.4.3Issue DescriptionThe fetch operation fails due to a missing source file. Specifically:http://downloads.yoctoproject.org/mirror/sources/git2_github.com.STMicroelectronics.gcnano-binaries.tar.gzHowever, this file is unavailable, and the fetch results in a 404 error.Here is an excerpt from the build logs:http://downloads.yoctoproject.org/mirror/sources/git2_github.com.STMicroelectronics.gcnano-binaries.tar.gzResolving downloads.yoctoproject.org (downloads.yoctoproject.org)... 2a01:4f9:3070:3985::2, 37.27.135.249Connecting to downloads.yoctoproject.org (downloads.yoctoproject.org)|2
I try to study embedded linux with stm32mp157f-dk2 boardI got download my image on my board and make dts from stm32cubeide's default board settingAnd i compile that in my source's dts folder modified Make file and checked dtb output with decompileIt works with added pwm from cubemx but not working touchSo CONFIG_TOUCHSCREEN_EDT_FT5X06 is being yes in my .configAnd it works in default starter pacakge's dtb but I changed just dtb with my pwm addedso if i echo 0-0038 bind to edt-ft5x06 with my pwm dtb, it works butI wonder why this builtin module not work with rebootThanks
Dear Sir/Madam,Thank you for reading my message. I have a newly bought STM32MP157F-DK2 but it doesn't boot the Bootlin's pre-build Linux kernel image. Its screen showed nothing (no boot messages, cursor, etc, as shown in the attached picture). I received the kernel image from bootlin's "buildroot-external-st" repo on github. Has anyone faced the same issue like mine above?Thank you. Regards,ZS Lee
Here's the translation of your request:"I was following the instructions on '6. Building the OpenSTLinux distribution' from the ST wiki (https://wiki.st.com/stm32mpu/wiki/STM32MPU_Distribution_Package), but encountered an error, so I couldn't proceed. Could anyone advise on how to resolve this issue?"If you provide more details about the error you're encountering, I can help you troubleshoot more specifically.
The STM32MP151 Reference manual says "For more information refer to Boot ROMapplication note.". But I can't find any application note that talks about Boot ROM. Please help to find this information.Thanks.
Hello everyone,I am planning to build an embedded project using a System on Module (SoM), and I am looking for a SoM board that supports bare-metal programming. Could you please help me find the best SoM board suitable for this purpose?
I've been following the STM32MP15 Discovery kits - Starter Package tutorial to set up my STM32MP157D-DK1 board and am having trouble flashing the SD card via the CubeProgrammer CLI. It successfully loads partitions 0x01, 0x03, then the board disconnects and the flash fails. Here's screenshots of the CLI output as well as a picture of the board:Additional info:My PC is running Windows 10LD6 (red LED between USER1 and USER2 buttons) flashes rapidly after disconnectLD8 (blue LED left of micro-USB port) is lit after disconnectHere's the troubleshooting I've done so far:Resetting the board before it times out results in the flash operation restarting from the beginning and failing in the same wayUsing device manager to scan for hardware changes after disconnect does nothingUSB driver switched to libusbK via ZadigFormatted the SD card to wipe previous partitionsUsed different cords and USB portsAttempted to flash from other .tsv files (tutorial calls for FlashLayout_sdcard_stm32mp1
Hi STM Community !!We use the STM32MP1 on our board.We use the gpio feature for an IRQ in our system.We use it in a kernel module.With the Ecosystem v5, it worked perfectly, but we used#define PIN_FPGA_INTA (16 + 10)static struct gpio gpio_irq_pps = {PIN_FPGA_INTA, GPIOF_IN, "IRQ PPS FPGA"};...if (gpio_request_one(gpio_irq_pps.gpio, gpio_irq_pps.flags, gpio_irq_pps.label)) {printk("Fail of gpio_request for PPS_INT(B10 pin) :( \n");}irq_num_pps = gpio_to_irq(gpio_irq_pps.gpio);if (irq_num_pps < 0) {printk("Fail to use GPIO B10 as PPS Interrupt :( \n");gpio_free(PIN_FPGA_INTA);}// set interrupt for PPSret = request_irq(irq_num_pps, pps_irq_handler, IRQF_TRIGGER_FALLING, "pnt_fpga_int_a", NULL);if (ret != 0) {printk("Interrupt Request Failed for INT_PPS: %d\n", ret);gpio_free(PIN_FPGA_INTA);} elseprintk("Interrupt PPS OK\n");...Now, in the Ecosystem v6, we need to move to new gpiod kernel functions, because gpio_* functions are deprecated.So, in the DTS In the DTS we have :/ {...my_gpi
The Static IP settings of my computer are as follows As follows, My computer can ping itself Then the Static IP (/lib/systemd/network/52-static.network) of my STM32MP135F-DK is set as follows As follows, My STM32MP135F-DK also can ping itself Why can't my computer ping STM32MP135F-DK? This is my comouter ip route, Why can’t I see the ip route of STM32MP135F-DK? Is there any mistake in setting the Static IP above? Or am I missing some settings? How can I solve this problem?
please suggest me some displays for STM32MP157D-dk1 and if possible provide me some links for purchase,i want 4 inch display
I'm wondering if anyone has any advice re. microcontroller (#MCU) support for #CSI-2?ST application note AN5478 "STM32MP135 line interfacing with a MIPI® CSI-2 camera" written in 2023 seems to be the best reference that I can find on this and uses the STMIPID02 MIPI CSI-2 deserializer.https://www.st.com/resource/en/application_note/DM00697325.pdfSD do provide an internal peripheral for CSI-2:https://wiki.st.com/stm32mpu/wiki/CSI_internal_peripheralST application note AN5470 on #STM32MP15x "STM32MP15x Series interfacing with a MIPI® CSI-2 camera" written in 2020 and updated in 2023 uses the same deserializer and says that:"it is possible to extend the range of addressable camera sensors for instance MIPI® CSI-2 cameras (camera serial interface), thanks to the STMIPID02 MIPI CSI-2 deserializer discrete component"https://www.st.com/resource/en/application_note/dm00693021-stm32mp15x-series-interfacing-with-a-mipi-csi2-camera-stmicroelectronics.pdfThe "D3 DesignCore camera mezzanine board O
hellowI have a project about kinematic of a drone.Is good solution the :https://www.st.com/en/evaluation-tools/steval-fcu001v2.html to collect real time data from the imu sensors ?There is access on data threw bluetoothor something ?
Trying to boot from a SD card, Boot loader configuration is working but then my configuration is not, any reason why ?
I am trying to get started on Linux kernel development on STM32MP157F-DK2 board. Thus far I have been able to,1. Flash the started package and get Linux booting successfully2. Download the developer package, add extra logs and update the linux kernel on the boardI am trying to get started on kernel drivers and was not able to find linux headers in the sdk include path. I am getting linux/init.h as not found.I tried to update the include path by adding the headers from the linux source code from the developer package but am facing a lot of include errors. I tried looking for a way to download the linux headers for the openst linux image online but wasn't able to find any so far.I have the following queries,1. Can someone provide a way to download the linux headers for cross compilation?2. If possible can someone share a simple wiki/example of a custom kernel module/driver on the openstlinux.Thanks in advance.
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.