Skip to main content
Associate
Nov 2, 2024 4:02 AM UTC
Question

Why my computer can't ping STM32MP135F-DK?

The Static IP settings of my computer are as follows

syuan_0-1730519185369.png

As follows, My computer can ping itself

syuan_1-1730519342431.png

Then the Static IP (/lib/systemd/network/52-static.network) of my STM32MP135F-DK is set as follows

syuan_2-1730519678133.png

As follows, My STM32MP135F-DK also can ping itself

syuan_3-1730519730430.png

Why can't my computer ping STM32MP135F-DK?

syuan_4-1730519889381.png

This is my comouter ip route, Why can’t I see the ip route of STM32MP135F-DK?

syuan_5-1730520016881.png

Is there any mistake in setting the Static IP above?

Or am I missing some settings?

How can I solve this problem?

 

 

 

 

 

 

 

 

 

 

This topic has been closed for replies.

2 replies

ST Employee
Nov 4, 2024 10:36 AM UTC

Hello @syuan ,

are you connecting the PC and Board via a switch or directly?

can you PC and Host ping 192.168.11.1 default gateway?
can you monitor the traffic via Wireshark and see if there are any ARP announcement in the network from either you PC or board?

Regards

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ST Employee
Dec 30, 2024 3:06 PM UTC

Hello @syuan ,

did you manage to get it working ?

Regards

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.