Skip to main content
Associate II
Dec 28, 2024 2:00 PM UTC
Question

LVDS not working with STM32MP257F-DK board

Hi,

When testing the stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v24.12.05 image, the LVDS screen doesn't work and blocks the board's startup (in u-boot) and I can't reset the board unless I disconnect the LVDS port.

On the other hand, the HDMI is functional, and the screen works without any problem on my STM32MP257F-EV1 board.

Note that the board is powered via a USB port capable of delivering up to 1.5A.

Thank you

This topic has been closed for replies.

1 reply

Pwxn
ST Employee
Jan 8, 2025 10:05 AM UTC

Hello @zakariazh ,

 

I've just tested the FlashLayout_sdcard_stm32mp257f-dk-ca35tdcid-ostl-m33-examples-optee.tsv on my board and the LVDS screen work fine. 

 

Could you provide more information about your setup ? Do you have any trace to share ?

 

Best regard,