Get ready for the STM32 Summit 2026 | Online, November 3
Join conversations with your peers and ST experts. Explore the full potential of STM32 microprocessors for your embedded design.
Most recent activity
Hi everybody,I've just installed STM32CubeIDE 1.2.0 on Ubuntu 18.04.It seems that breakpoints on Cortex-M4 don't work. When I debug via ST-Link on stm32mp157c-dk2 everything is fine but breakpoints, they are simply ignored.Any suggestion?With previous installation (STM32CubeIDE 1.1.0) breakpoints on Cortex-M4 worked well, allowing to stop execution wherever I wanted.In the "Progress" tab in Eclipse it seems that Configuring GDB hangs on (at 93%), even if the execution really starts.
We designed our own board and use RTL8211E instead of RTL8211EG-VB-CG. We are unable to get the PHY device to respond although we copy the same circuit from the MB1262. The MAC is working but the communication to Realtek PHY seems to be a problem. Does the current kernel build support RTL8211E?
I guess, it has something to do with the secure monitor inited by TF-A, since GPIOZ is protected. Maybe there is something wrong with the default device tree using the GPIOZ? What can I do?
According to the documentation of the EV1 eval board:"The STM32MP157xAA3 also drives a sub system reset, SUB_NRST signal on PD10 IO, to the peripherals: USB Host Hub, MFX, Ethernet, and RGB_LTDC connector."Is this signal generated automatically by the STM32MP157? Is it software controlled? If the latter, is this implemented in OpenSTLinux images by default?Thanks,Guillermo
Hi,I am building openstlinux-weston/st-image-weston image for stm32mp157c-dk2 board, and I have developed 2 application to be displayed at the same time. I configured DSI and HDMI with Buildroot, for the last one I followed this wiki: https://wiki.st.com/stm32mpu/wiki/How_to_display_on_HDMI, but I would like to know if there is a way to display 2 different application on the 2 interfaces at the same time.Regards.Aitor.
Hello all,I am trying to use the SPEAKER_OUT connector in the STM32MP157C-EV1 board to play sound using a set of regular 8 Ohm (non-amplified / passive) loudspeakers.I am configuring the wm8994 to enable the SPKOUTL/RP path as described here: https://wiki.st.com/stm32mpu/wiki/Soundcard_configuration#Wolfson_wm8994_output_configurationWhen I play a sound file via ALSA (using aplay), the sound signal is very weak. I can hear the sound if I connect a headphone set to the SPEAKER_OUT connector, but not if I connect the regular loudspeakers.If I am reading the wm8994 datasheet correctly, the SPKOUT path includes a 2W amplifier. Do I have to do anything else in order to enable it?BR,Guillermo
Hey all,I have a STM32MP157C-DK2 developer board with screen and i am trying to get node.js running on it. Has anyone done this before? I know the board is pretty new, released in Oktober. But worth a shot.ThanksRinke
..
I'm trying to find a solution to a problem using vision, I discovered the 'MPU' line with the STM32MP157C-DK2 but while investigating I cannot find CSI input or even a camera input. While I enjoy playing with USB based cameras it is 2019 and everyone has moved on to CSI based cameras, using parallel cameras is so 2013... It also appears everything is disconnected, what use is a AI based system for CNN networks if you cannot hook up a camera? Talking with Amazon?Does STM have a vision based STMxx product?
I've run a simple graphical program with Mono and OpenTK. It contains a simple fragment shader (demo). One frame renders about 7 seconds and CPU usage is 100%. Is it normal?vec2 p = ( gl_FragCoord.xy / resolution.xy ) - 0.5; float sx = (amp)*1.9 * sin( 4.0 * (freq) * (p.x-phase) - 6.0 * (speed)*time); float dy = 43./ ( 60. * abs(4.9*p.y - sx - 1.2)); dy += 1./ (60. * length(p - vec2(p.x, 0.))); gl_FragColor = vec4( (p.x + 0.05) * dy, 0.2 * dy, dy, 2.0 );
Is it possible to use opengl without wayland?the /vendor/lib libraries have dependency to libwaylandand as far as i am aware these libraries are binary only.are there other versions of the libraries that can work with fb, without x or wayland?otherwise this is a pretty significant limitation, if opengl is wayland only
hi,I can start the weston demo program by burning the same system to sdcard, but cannot start it by burning to emmc.And I found that the vendorfs and userfs partitions were not mounted
Hello, I'd like to install Python dependencies to run a RTL-SDR python program on the discovery kit and I failed to execute the following command line below : apt-get install python-numpy (or python3-numpy). Do you know how to install numpy on the DK2 ?BR
Hello,we would like to boot from a eMMC memory on our board connected to SDMMC2. As the camera interface is in conflic with SDMMC2 8bit mode, we must configure it as a SDMMC 4 bit width. The question is will we still me able to boot from our eMMC memory in 4 bit mode as we do in 8 bit ? The memory we use is the following MTFC4GACAJCN-1M from MicronTanks for your support.
My STM32MP157CAA3 Board Not Boot By SDCARDI already check SDCARD Clock Pin .. ...reset MCU and i check SDCARD Clock Pin ... but not signal ....);I already check Boot MODE -> SDCARDHELP ME...
Hi everyone. I have a STM32MP157A-DK1 with a developer package. My goal is to install iperf. But I'm not familiar with OpenSTLinux and Yocto. Apt-get and dpkg do not allow to install iperf. What is the simplest way to install 3rd party util (iperf in my case) on the STM32MP157A kit?Thanks in advance.
Hello,After power on my EV1 board, I get the following error message:NOTICE: CPU: STM32MP157AAA Rev.B NOTICE: Model: STMicroelectronics STM32MP157C eval daughter on eval mother NOTICE: Board: MB1263 Var1 Rev.C-01 INFO: Reset reason (0x15): INFO: Power-on Reset (rst_por) INFO: Using NOR INFO: Instance 1 INFO: Boot used partition fsbl1 INFO: NOR: Memory mapped mode NOTICE: BL2: v2.0-r1.5(debug): NOTICE: BL2: Built : 13:13:37, Oct 2 2018 INFO: BL2: Doing platform setup INFO: PMIC version = 0x10 INFO: RAM: DDR3-1066/888 bin G 2x4Gb 533MHz v1.45 INFO: Memory size = 0x40000000 (1024 MB) INFO: BL2 runs SP_MIN setup INFO: BL2: Loading image id 4 INFO: Loading image id=4 at address 0x2fff0000 INFO: Image id=4 loaded: 0x2fff0000 - 0x30000000 INFO: BL2: Loading image id 5 INFO: Loading image id=5 at address 0xc0100000 INFO: STM32 Image size : 806658 WARNING: Skip signature check (header option) INFO: Image id=5 loaded: 0xc0100000 - 0xc01c4f02 INFO: read version 0 current version 0 NOTICE: BL2: Bo
I have evaluated the VisualGDB IDE and I am quite excited about the hassle less user experience.Setup of a project for the Cortex M4 core is almost as easy as setup a Windows project.Debugging of the Cortex M4 application is possible over ST-Link. The application is uploaded into the Linux file system an started by the Debugger. Using the debugger is almost as easy as using the Visual Studio debugger. User experience is far better than with the SW4STM32 IDE I tried before. Everything is done in the Windows environment and the ARM cross compiler for Windows will be automatically downloaded and installed.Developing a Linux application with VisualGDB is also possible. This is the next thing I will try.https://visualgdb.com/w/tutorials/tag/stm32mp1/
Dear STM32 MPU Community,This is November MPU Community news digest ! Some useful information we would like to share with you this month.New MP1 Ecosystem V1.1.0 ! ST is pleased to announce the MP1 Ecosystem V1.1.0 complete delivery done begin of October : https://wiki.st.com/stm32mpu/index.php/STM32MP15_ecosystem_release_note2 main items to highlight :- V1.0.0 Distribution for Android 9- CubeIDE V1.1.0 to support M4 Co-processorSTM32CubeIDE tool is now the Eclipse IDE ST reference.The STM32CubeIDE V1.1.0 release supports same features set than SW4STM32 IDE V2.9.0Customers can continue to use SW4STM32 IDE but the ST Eclipse reference is STM32CubeIDE. In case of support, ST will focus and recommend STM32CubeIDE tool. SW4STM32 projects can be imported in STM32CubeIDE V1.1.0. Please refer to document : AN5360 Getting started with projects based on the STM32MP1 S
Do we have a road map ?looking for a controller STM32H with 480Mbps USB portwhat about the STM32MP series roadmap ?when is the MP2 coming out ?can we get some Flash and Ram in the MP2 ?just need 1MB Flash and 1MB RAM or 4/8MBytes RAM to satisfy a 1366 x 768 image
SPI
We used nandflash of MT29F4g08ABADAWP and found that there was an error in startup. May I ask how to solve it?Boot over nand0!ubi0: attaching mtd4ubi0: scanning is finishedubi0: volume 3 ("userfs") re-sized from 521 to 587 LEBsubi0: attached mtd4 (name "UBI", size 506 MiB)ubi0: PEB size: 131072 bytes (128 KiB), LEB size: 126976 bytesubi0: min./max. I/O unit sizes: 2048/2048, sub-page size 2048ubi0: VID header offset: 2048 (aligned 2048), data offset: 4096ubi0: good PEBs: 4044, bad PEBs: 4, corrupted PEBs: 0ubi0: user volume: 4, internal volumes: 1, max. volumes count: 128ubi0: max/mean erase counter: 1/0, WL threshold: 4096, image sequence number: 826760955ubi0: available PEBs: 0, total reserved PEBs: 4044, PEBs reserved for bad PEB handling: 76UBIFS error (ubi0:0 pid 0): ubifs_recover_master_node: failed to recover master nodeError reading superblock on volume 'ubi0:boot' errno=-22!ubifsmount - mount UBIFS volumeUsage:ubifsmount <volume-name> - mount 'volume-na
hi:I have a requirement that I need to update my nand flash or emmc system with an sd card.Currently, burning image with STM32CubeProgrammer is not suitable for batch updating.I hope you can support me
I use jtag debugging m4 program, the following error, how should be resolvedOpen On-Chip Debugger 0.10.0+dev-01124-gbfb41e6 (2018-11-16-15:23)Licensed under GNU GPL v2For bug reports, read http://openocd.org/doc/doxygen/bugs.htmldebug_level: 1cortex_a interrupt mask oncortex_a interrupt mask oncortex_a domain access control fixup oncortex_a domain access control fixup on3333none separateadapter speed: 5000 kHzadapter_nsrst_assert_width: 200adapter_nsrst_delay: 200none srst_pulls_trstsrst_only srst_pulls_trst srst_gates_jtag srst_open_drain connect_deassert_srstError: Could not find MEM-AP to control the coreap 0 selected, csw 0x10006000Error: Target not examined yetundefined debug reason 7 - target needs resetError: Target not examined yetError: Could not find MEM-AP to control the coreError: Target not examined yetembedded:startup.tcl:24: Error: in procedure 'stm32mp15x.cpu2' called at file "embedded:startup.tcl", line 283in procedure 'ocd_bouncer' at file "embedded:startup.
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.