Get ready for the STM32 Summit 2026 | Online, November 3
Join conversations with your peers and ST experts. Explore the full potential of STM32 microprocessors for your embedded design.
Most recent activity
Hello everyone,I received my STM32MP157C-DK2 device and I built a Buildroot-image and flashed it successfully.I am new to STM32 and to the IoT field so perhaps you can orient me and tell me which Programs I need to do so. I want to write a "hello_world" program that sends hello_world every x-seconds to an Endpoint-rest through Wifi.Is it possible to only use Linux Bash/Shell interface to execute my Program? (I am familiar to these) and like I said I am only testing some features here like the ability of the DK2 to interact with Endpoint-rests.Thank you all and have a nice day.
Hi,How can I connect to STM32MPU via SSH from inside STM32CUBEIDE.?? Is there a way we can do that?This really helps in live debug of things.Alternatively is there a way I can live debug an application running on A7?
Hi,I would like to know for the board how to enter low power mode. I am using a version, openstlinux-5.10-dunfell-mp1-21-03-31. Please let me know how to address it.Best Regards,Sun
I have two codes running (on stm32mp157f-Dk2) successfully one is running on M4+freeRTOS another on A7+Linux, they are intercommunicating via RPMSGx. The problem is that after power-loss or reboot, I want both of my programs starting automatically and not the default UI (GNU desktop screen with icons of examples). Is there a chance to get either step-by-step guide or even better a video executing all the steps to change the kernel and launch customer's code?4 Build the Linux® kernel source code for the first time:https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2/Develop_on_Arm%C2%AE_Cortex%C2%AE-A7/Modify,_rebuild_and_reload_the_Linux%C2%AE_kernel#Build_the_Linux-C2-AE_kernel_source_code_for_the_first_time (4.1.2 Remote processor 'auto' boot (not recommended by STMicroelectronics)↑:(https://wiki.st.com/stm32mpu/wiki/Linux_remoteproc_framework_overview3.3 Modifying the Linux kernel device tree↑:https://wiki.st.com/stm32m
Good evening,I am using stm32mp157F-DK-2 board. And I want to update the kernel from old 5.4.31 to 5.10.10.I was following step-by-step "Modify, rebuild and reload the Linux® kernel" on the "https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2/Develop_on_Arm%C2%AE_Cortex%C2%AE-A7/Modify,_rebuild_and_reload_the_Linux%C2%AE_kernel#Build_the_Linux-C2-AE_kernel_source_code_for_the_first_time". Only strange thing the command: >> /sbin/depmod -a - does not return any success/failure info. No errors appeared so I used >> sync and >>reboot.After reboot I see that both old and new kernel modules are present:>> ls /lib/modules 5.10.10 5.4.31When i try to check current kernel version :>> uname -aLinux stm32mp1 5.4.31 #1 SMP PREEMPT Wed Apr 8 07:08:47 UTC 2020 armv7l armv7l armv7l GNU/LinuxHave I missed something? Does the old kernel module should be removed entirely?I have tried re-flashing the board and repeating procedure multiple
Hi.. thereHope all are doing well We have designed our own custom board by taking the reference of the DK2 board, in which we're using the LBEE5KL1DX-883 WiFi/BT module from Murata at SDMMC3 somehow, the module is unable to detect!after dmesg of the MMC log, I got to know that the SDMMC 3 is not initializedhere is the mmc dmesg logs [ 0.000000] Kernel command line: console=ttySTM0,115200n8 quiet hw_dispid=6 hw_code=143 fastboot=n board_name=ns02_ek435 touch_type= root=/dev/mmcblk0p2 rootfstype=ext4 rootwait [ 0.678302] mmci-pl18x: probe of 48004000.sdmmc failed with error -22 [ 0.679283] mmci-pl18x 58005000.sdmmc: Linked as a consumer to regulator.3 [ 0.679417] mmci-pl18x 58005000.sdmmc: mmc0: PL180 manf 53 rev2 at 0x58005000 irq 63,0 (pio) [ 0.708451] mmci-pl18x 58007000.sdmmc: Linked as a consumer to regulator.2 [ 0.708585] mmci-pl18x 58007000.sdmmc: mmc1: PL180 manf 53 rev2 at 0x58007000 irq 64,0 (pio) [ 0.743212] mmc0: host does not support reading read-only switch, assuming write-
Hi All,i am using stm32mp1 cpu,, recently i m facing floating rx issue on debug uart, with physical debug cable , i could default state of RX lines were pull up, and when i remove the cable, the RX lines is floating and its voltage fluctuates between 0.9-1.4 Volts,when i power up unit, with out cable, the u-boot code waiting for receive events, i see the u-boot cancel the normal boot because (USART_ISR) lot of error were seen like noise, eob, cmf, Fe, bits , so most of error bit were set along with RDR data to read flag,i am using FIFO enabled, with 16 byte rx buffer, tried with disabled fifo, still same problemThere is pull up is required, but can this be fixable in software u boot and kernel ? some thing like soft reset/ or any clear pending interrupts ?Any suggestion would be helpfull
Hi,I would like to compile a user space c++ application on the STM32MP157C-DK2. Is it possible to install GCC or G++ on the board?I tried installing them via apt-get but seems like there is not any package with name gcc or g++.How can i install it and how do i make sure it is up and running ? I know we can use Yocto SDK to compile and transfer the code on to the board via SCP. But here i specifically want to compile it on board itself.Any leads will be highly appreciated.
HI ,How can i display simple image on to the screen ?Currently we have weston demo running. I am aware of how to stop it , but post that what command can i use to simply just display an image on to screen?
MDK compiles, and the program loads the following results: IDE compiles, and the program loads the following results: The MDK program is exported from the IDE, and the two programs are the sameI want to use openamp in MDK, how can I modify it
Hi!I am trying to have full secure booting on the stm32mp platform, using FIP and fitImage on a custom distribution built using Yocto with the meta-st-stm32mp layer.I currently have a FIP containing u-boot booting on the board, that can then load and boot an unsigned fitImage.I now want to enable fitImage signing. The signature verification in u-boot is enabled in u-boot's configuration, and u-boot devicetree has been extended to include a signature section, so that mkimage can insert the signing key for u-boot's to verify my fitImage.The fitImage is signed with the key by setting the following variable in my machine configuration:UBOOT_SIGN_ENABLE = "1"I checked that the image is indeed signed, and that a u-boot devicetree containing the key is in my deploy directory (I disabled the use of the "u-boot" subfolder with a bbappend on u-boot-stm32mp recipe).The issue comes from the final dtb included in u-boot´s binary, before the FIP generation by fiptool. By the end of the kernel s
Hello,We are using the LBEE5KL1DX-883 WLAN+BT chip with a STM32MP157C on a custom board. The SDIO interface is routed to the SDMMC3 interface (different from the DK-2 board). However when we are probing the brcmfmac module, it cannot find the mmc0 interface it seems. It writes the following to the dmesg logs:[ 21.319324] brcmfmac: No platform data available.Is there anything extra which needs to be configured when using SDMMC3 as opposed to SDMMC2? Posting relevant configuration below. Thanksmmc related dmesg logs during boot:root@stm32mp1:~# dmesg | grep mmc [ 0.000000] Kernel command line: root=/dev/mmcblk1p5 rootwait rw console=ttySTM0,115200 [ 1.799815] mmci-pl18x 48004000.sdmmc: allocated mmc-pwrseq [ 1.804262] mmci-pl18x 48004000.sdmmc: Linked as a consumer to regulator.7 [ 1.810928] mmci-pl18x 48004000.sdmmc: mmc0: PL180 manf 53 rev1 at 0x48004000 irq 41,0 (pio) [ 1.848186] mmci-pl18x 58005000.sdmmc: Linked as a consumer to regulator.7 [ 1.853931] mmci-pl18x 58005000.sdmmc: mmc1
Hi,How can i install and develop around amazon AWS SDK for an custom IoT solution?
Hi,I have done certain changes to support the display in the dts files.I have modified dts files under kernel and u-boot.I had also added certain changes in panel-simple.c file as well. I gave a build and forgot to make some changes. So i changed those locally and gave :bitbake st-image-westonBut this time around upon checking i found out that latest changes i made were not compiled and a new .o was not generated. How can i make sure , that local changes are compiled by yocto build system??
hi, we are using stm32MP157A ,in this we enabled timer2 APB1 and APB2 clock for timers . When we trying to write timer 2 the processor gets hanged . For this what may be the issue. In the similar way i did it for the UART4 its working fine . Where as coming to the writing to timer registers its hanging .
I want to use open source utilities to load U-boot into SRAM in "Serial mode". Is it possible?P.S. As I can see, there is an article about it on ST Wiki, but an access to it is restricted for regular users: https://wiki.st.com/stm32mpu/wiki/How_to_load_U-Boot_with_dfu-utilHow to gain access to this article for an ordinary user?
Is there also an ARM version of the SDK to develop the Modules.because here I only found a X86 versionhttps://wiki.st.com/stm32mpu/wiki/STM32MP1_Developer_Package#Installing_the_SDK
We are using a STM32MP157 chip on a custom low-power design and don't need the Cortex M4 core. We would like to disable it properly to reduce power consumption and also remove dedicated support in linux kernel.Is there any recommended way to do this ? Is disabling clock enough ?Thanks in advance for your help
After DDR3 (16 bit) training complete, registers are:DX0DQSTR=0x3DB03001, DX1DQSTR=0x3DB03001Should I redesign CPU board or these values are suitable?
HI ,How can i install mongodb , mariadb and postgresql on stm32mp1?Is there support for databases provided for stm32mp1?
We are seeing some strange behavior on our stm32mp157 system exiting suspend mode.This is not a 'weston' build, so we enter (deep) suspend mode by executing "echo mem > /sys/power/state" and the system powers down and enters low power.root@stm32mp157:~ # echo deep > /sys/power/mem_sleeproot@stm32mp157:~ # echo mem > /sys/power/state[ 30.426284] PM: suspend entry (deep)[ 30.428793] PM: Syncing filesystems ... done.[ 30.477793] Freezing user space processes ... (elapsed 0.001 seconds) done.[ 30.484664] OOM killer disabled.[ 30.487814] Freezing remaining freezable tasks ... (elapsed 0.001 seconds) done.[ 30.495358] Suspending console(s) (use no_console_suspend to debug)When a wake up happens the processor wakes up and the TF-A detects that the processor exited STANDBY and is running from eMMC, however the system never executes the Linux system, it hangs after "Preparing exit to normal world"NOTICE: CPU: STM32M
Hi all,I am trying to bring a LVDS display up. Display: BOE EV121WXM-N10-1850. Datasheet: LinkDriving MPU : STM32MP1. I am using VisionSoM STM32MP1 based evaluation Kit. LinkThe firmware changes required to make the device up are part of git: LinkI have made following changes in the dts files to support display:kernel/stm32mp157a-visionsom-rgb-emmc-mx.dts and u-boot/stm32mp157a-visionsom-rgb-emmc-mx.dts has following changes : panel { compatible = "boe,ev121wxmn10", "simple-panel"; backlight = <&backlight>; port { panel_in: endpoint { remote-endpoint = <&ltdc_out_rgb>; }; }; };In case u-boot/stm32mp157a-visionsom-rgb-emmc-mx-u-boot.dtsi panel { display-timings { timing0: timing0 { clock-frequency = <74250000>; hactive = <1280>; vactive = <800>; hfront-porch = <48>; hback-porch = <80>;
Hello all,I'm getting following error on our custom board while initializing sdmmc3 as wifi module with SDIO:~# dmesg | grep -i sdio -B 1 [ 3.410271] mmci-pl18x 48004000.sdmmc: no support for card's volts [ 3.415001] mmc0: error -22 whilst initialising SDIO card -- [ 5.298030] mmci-pl18x 48004000.sdmmc: no support for card's volts [ 5.302938] mmc0: error -22 whilst initialising SDIO card -- [ 7.140215] mmci-pl18x 48004000.sdmmc: no support for card's volts [ 7.144982] mmc0: error -22 whilst initialising SDIO card -- [ 8.930932] mmci-pl18x 48004000.sdmmc: no support for card's volts [ 8.935676] mmc0: error -22 whilst initialising SDIO cardWifi module is a ST60-2230C (https://www.lairdconnect.com/documentation/datasheet-st60-2230c) with I/O signalling voltage 1V8.Between STM32MP and ST60 module there are three voltage translators which translate 3V3 (STM32MP) to 1V8 (ST-60). See attached schematics snippet.This is device tree configuration:&sdmmc3{ arm,primecell-periphid = <0x101
In our project we are currently trying to decrease boot time and energy consumption of an embedded linux running on an STM32MP153.To improve energy consumption we are trying to activate hibernation, in order to test suspend-to-disk as well as the hybrid-sleep mechanism.I have activated hibernation in the kernel and have also created a swap disk (which does not mount properly after reboot) by hand.But still "/sys/power/state" gives me nothing more but "mem", indicating we can only do a suspend-to-ram and returns "not supported" for anything else i'll try to echo into it.Is there a possibility to enable hibernation, even if the documentation does not list it explicitly?Thanks in advance!
Can anybody say meaning of four values in ACSR field of DDRPHYC_ACIOCR register?May ill ddr3-equipped board work more stable (i think) if I add no-zero values here...
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.