Skip to main content
dungeonlords789
Associate III
July 16, 2021
Solved

Is boards not recommended for new design? STM32MP157C-DK1 STM32MP157C-DK2

I am looking for STM32MP157A-DK1 and STM32MP157A-DK2 Why thouse boards is not recommended for new design? Which developer board you can recommend?

@PatrickF​ @Community member​ @SEam72​ 

This topic has been closed for replies.
PatrickF
PatrickFBest answer
ST Employee
July 16, 2021

Hi,

These boards has been replaced by new boards using faster 800MHz processor. They are 100% backward compatible with previous one (same HW, same SW).

STM32MP157A-DK1 and STM32MP157C-DK2 has been replaced respectively by STM32MP157D-DK1 and STM32MP157F-DK2

Note that all the 650MHz devices versions still exist with the 10-year longevity program (as well the 800MHz versions), just the 650MHz boards has been discontinued (800MHz boards cover as well the 650MHz evaluation purposes)

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent

3 replies

PatrickF
PatrickFBest answer
ST Employee
July 16, 2021

Hi,

These boards has been replaced by new boards using faster 800MHz processor. They are 100% backward compatible with previous one (same HW, same SW).

STM32MP157A-DK1 and STM32MP157C-DK2 has been replaced respectively by STM32MP157D-DK1 and STM32MP157F-DK2

Note that all the 650MHz devices versions still exist with the 10-year longevity program (as well the 800MHz versions), just the 650MHz boards has been discontinued (800MHz boards cover as well the 650MHz evaluation purposes)

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
Peter BENSCH
ST Technical Moderator
July 16, 2021

You can use the successor boards STM32MP157D-DK1 and STM32MP157F-DK2.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
PatrickF
ST Employee
July 16, 2021

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent