Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Most recent activity
Hi,I want to build a simple point-to-point communication (2 devices for now) system between two NUCLEO-55WLJC1 dev kit.I would like to use the LoRa modulation for this purpose but do not want to use the complete LoRaWAN protocol (and its stack).Is this something that is supported by ST's software and example codes ?Has anyone tried using LoRa on the STM32WL without the LoRaWAN stack ?It was relatively easy to do that with STM32L0 + SX126x using example codes. I am not sure how complex it can be, especially with the dual core version of the STM32WL.Regards.
..
Dear communityI'm working on a project using STM32WLE5J microcontroller. I would like to collect time from some external source and then keep it on the device. My problem is that the device loses its internal time after waking up from standby (e.g in the first cycle it counts from 0 to 30 seconds, then the device goes to sleep, it wakes up and again it begins to count from 0). I noticed that when reading from SSR register (by LL_RTC_TIME_GetSubSecond()) it gets cleared indeed.Is there anything to set that I forget about? I wonder if the fact that device wakes up after Standby and makes all the initializations over and over again clears some data, and also RTC values.Regards
Hi,How can i find the Pin voltage of different Pin of Board P-NUCLEO-WB55-Nucleo(stm32WB55RGVx), Especially the Pins used for UART communication? (Tx and Rx Pin)I didn' find a clear information in the Datasheet of this board:https://www.st.com/resource/en/user_manual/dm00517423-bluetooth-low-energy-and-802154-nucleo-pack-based-on-stm32wb-series-microcontrollers-stmicroelectronics.pdfThans in advance.
Helle Evryone , I juste wante to modifiy my file no-ota to file ota, i following the video in youtube https://www.youtube.com/watch?v=mRzZOa3jmuM but the problem whene I want to change start adress my application don't work
Hello,I'm using STM32Wb CubeMX HAL FW 1.10.1 and a PNUCLEO-WB55I'd like to get the wireless coprocessor stack version at runtime. I didn't find a HAL API to do this, so I went about it manually using AN5185 as a guide. According to AN5185, the device information table contains (among other things) the wireless stack version. This table is in SRAM2a and should be accessible by both cores. Using the flowchart on page 16, I'm trying to read the magic number stored at the top of this table, but I'm always getting back 0x00000000. Here's my code:void print_device_info(void) { // Get IPCCDBA FLASH_OBProgramInitTypeDef pOBInit; HAL_FLASHEx_OBGetConfig(&pOBInit); volatile uint32_t *ipccdba = (uint32_t *)(pOBInit.IPCCdataBufAddr); // Get offset of device info table uint8_t device_info_table_offset = (uint8_t)*ipccdba; printf("Device info table magic number = %08lX\r\n", *(ipccdba + device_info_table_offset)); __BKPT(0); }If I point the debugger at that memory address, it in
I am going through the Hands-on2 and Hands-on3 in STM32WB55 MOOC. In the both examples sequencer or simple scheduler is used for the BLE. Inside the while loop I found only the Seq_run() function. I want to learn how the sequencer works. Can anyone provide me resources for this ?
Hello,I have a custom PCB using a STM32WB35CCU6A that I'm trying to get Bluetooth up and running. I'm using the latest firmware available at this time: "STM32Cube_FW_WB_V1.10.1".I've been unable to get CPU2 to initialize from my STM32CubeIDE project. When I set breakpoints in `APPE_SysStatusNot`and `APPE_SysUserEvtRx` from `app_entry.c` the former is the only one that is called. Looking in STM32CubeProgrammer it appeared my wireless stack was not running.I followed UM2550 section 5: when I get to "Download new wireless stack" I get the following error:The Copro Binaries do not list this 256K chip in the binary tables; I'm assuming the FUS address is 0x0803A00, and BLE_Stack_full_fw 0x800B000, it's possible I'm not using the correct address for the BLE stack.
I am building a device that has to register data that is send in BLE beacons. I want to filter this data out of received Advertisement messages. Are there any implementations of this capability that I can learn from? I started from the P2P Client example, but when I change the gap role from GAP_CENTRAL_ROLE to GAP_OBSERVER_ROLE, I do not get any advertisement reports anymore.
Hello,I want to implement my own temperature & humidity Zigbee sensor using STM32WB.I can now send and report temperature using zcl.temp.meas.h.In the documentation AN5506, I can read that 47 clusters - and among them Relative humidity measurement cluster - are supposed to be available in the STM32WB stack. Unfortunately, in the library that I have, I cannot find Relative humidity measurement cluster.Is it available somewhere?Thank you for your support,Best regards,Leo
I watched the stm32WB workshop and studied the ble example on the stm32wb55 nucleo board and it worked well.Now I'm trying to test the ble on my custom board, stm32wb35cc, but I didn't do anything.The stm32wb manual found that the stm32wb35 contained cpu1 cortex-M4 and cpu2 cortex-M0.Does it work if you put the binary related to the ble stack in Cortex-M0?According to the "stm32wb getting started" document, there are binary (stm32wb3x_BLE_Stack_full_fw.bin) files, does it work by putting them in cpu2 cortex-m0?If I buy a stm32wb35cc chip, is there no basic binary?
I am using STM32WB55RG nucleo board. I want to use low power modes only for the CPU2 ? Is it possible to do that ? If so how ?
And I can't find the description and API of the modules and Libraries. I need the FLASH drivers and LOG module.
Hi, I recently designed my own pcb board for STM32WB55CEUx MCU.Then, during working with my board I got some problem at APP_BLE_Init() functionand the symptoms are exactly same with thisSTM32WB55 BLE Stack trouble on new hardware: https://community.st.com/s/question/0D50X0000B5IOp2SQG/stm32wb55-ble-stack-trouble-on-new-hardwareand thisSTM32WB : Bug in FW_WB_V1.0.0: aci_gap_set_discoverable > hci_send_req > hci_cmd_resp_wait - wait infinitely for hci_cmd_resp_release after few connection/disconnectionhttps://community.st.com/s/question/0D50X0000AYqZ6mSQF/stm32wb-bug-in-fwwbv100-acigapsetdiscoverable-hcisendreq-hcicmdrespwait-wait-infinitely-for-hcicmdresprelease-after-few-connectiondisconnectionSo, I think I should update the ble stack inside my mcu.But, I can only find the examples for the nucleoboard, which has USB bootloader mode.I only have ST-link interface in my custom board.How can I update ble stack with only stlink? or is it impossible?Every pins of STM32WB55CEUx is avail
hello I want to update any firmware with app ST BLHello evryone, I want to create my own application BLE and update firmware via OTA, without using BLE examples existing like heartrate, and p2pserver.
Hi,I have a STM32WB55-Nucleo running the BLE_HeartRateFreeRTOS sample application. All works well for a while - I can scan and connect to it (from LightBlue on iOS) and read, write and subscribe to notifications. However, after approximately 40 mins, the application crashes.My environment is:STM32CubeIDE 1.5.1 on Mac OS 10.14.6STM32CubeWB-master (downloaded directly from github - v1.9??)STM32Cube_FW_WB_v1.10.0 (patch downloaded from STM.com)BLE_HeartRateFreeRTOS sample (I am not generating any code from the MX view in STM32CubeIDE)stm32wb5x_BLE_Stack_full_fw.bin from downloaded patch uploaded to Nucleo board using CLI to address 0x080CB000The application crashes because it exits from the Idle Task in port.c as shown here (can't upload screenshot for some reason...):/* Start the first task. */ prvPortStartFirstTask(); /* Should never get here as the tasks will now be executing! Call the task exit error function to prevent compiler warnings about a static function not being ca
Hi everyone,I am developping an application on the SPBTLE-1S module (BLE 4.2).When the connection quality is low, a disconnection will sometimes occur with error code 0x28 (Reason: Instant Passed) before the connection timeout is reached.Current connection settings are: Conn_Interval_Min: 10Conn_Interval_Max: 20Slave_latency: 5Timeout_Multiplier: 3200Reading more on this type of error, it seems to happen when "an LMP PDU or LL PDU that includes an instant cannot be performed because the instant when this would have occurred has passed." These paquets are typically used for frequency hopping or for connection updates. In my case, they must be frequency hoping paquets. Any idea on how to prevent these disconnections caused by "Instant Passed" errors?Cheers,Xavier
I am trying to build a Lora-End-Node application for STM32L476RGT6 + a separate Semtech SX1272 chipt attached to it. The only exampüles are for Nucleo boards. In addition the code is stringly nested, so that it is difficult to understand. ST sure did not want to make Lora implementation easy.Where can I find an understandable Lora-End-Node example for this combination of chips?
Hi,I am trying to develop a ble application with the stm32wb55 and stm32cubemx. The MCU is on st nucleo board.I have create a new cubemx project, add middleware BLE STM32_WPAN, add scheduler on while() cycle in main.c, add IPCC interrupt handlers in stm32wbxx_it.c.It's peripheral custom template, I have 1 service with 3 characteristics with all UUIDs filled and without read/write permission need.Advertising start but when I try to connect the device disconnect immediately after connection. I see that through breakpoints in debug mode. First eventi is EVT_LE_CONN_COMPLETE and immediately after EVT_DISCONN_COMPLETE. I see in hci_disconnection_complete_event_rp0 the reason value and it is 0x3e alias ERR_CONN_FAILED_TO_ESTABLISH.So I don't understand what is the problem, why the connection drop soon after connection.Can someone help me? Thanks
A new version 2.7.0 is released.New features :802.15.4 RF sniffer : it is now possible to use a STM32WB Nucleo boards to spy the 802.15.4 packets and display the traces in Wireshark. Wireshark can be started directly from STM32CubeMonitor-RF. The procedure to use the sniffer is described in chapter 6 of User Manual (UM2288)Update some OpenThread commands to be properly aligned with O.T. firmware Fixed issues : Fixes the OTA updater panel address bytes inverted, and improve reliabilityOpenThread network explore button label management has been fixed,Fixes the naming of some BLE commands to match with AN5270 specification, Fixes ACI client characteristic partial discovery after reconnectionThe complete list is provided in the release note. Enjoy !
Dear ST-Community,I've checked your latest Ressources on STM32WLE:https://www.st.com/en/microcontrollers-microprocessors/stm32wlex.html#cad-resourcesAnd opened the file in Altium to export it to P-CAD ASCIIhttps://forums.autodesk.com/t5/eagle-forum/importing-files-from-altium-designer-to-eagle/td-p/6827258I could import it in Autodesk EAGLE but the design is broken at many pads:EAGLE ImportALTIUM originalCould you maybe also provide EAGLE files or provide recommendations how to get the files to EAGLE?Thank you!
WATCH ON-DEMAND | STM32 Summit 2026
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.