Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Most recent activity
..
I followed this[1] URL to update FUS and wireless stack, it failed and now i can't get wireless to work. All the examples are hard faulting. My FUS is still in version 0.5.3Reading 32-bit memory content Size : 4 Bytes Address: : 0x20030030 0x20030030 : 00050300But i can't upgrade to the latest one.USB speed : Full Speed (12MBit/s) Manuf. ID : STMicroelectronics Product ID : DFU in FS Mode SN : 206F3169554D FW version : 0x011a Device ID : 0x0495 Device name : STM32WBxx Flash size : 1 MBytes Device type : MCU Device CPU : Cortex-M4 Current FUS Version : 0x00050300==================] 100% Uploaded FUS Version : 0x01000200 FUS state is FUS_IDLE FUS status is FUS_NO_ERROR Old wireless stack delete ... Deleting firmware ... Firmware delete finished FUS state is FUS_SERVICE_ONGOING FUS status is FUS_IMAGE_NOT_FOUND FUS state is FUS_IDLE FUS status is FUS_NO_ERROR Download firmware image at address 0x80ec000 ... Memory Programming ... Opening and parsing file: st
In our previous design we were using DFSDM to read the microphone data, but with the STM32WB family there is only SAI PDM port. I read that the SAI consume more power than the DFSDM because it is processing PDM to PCM. I found also that the DFSDM is more light than the SAI with the acoustic beamforming https://community.st.com/s/question/0D53W00000W674p/is-there-a-way-to-use-st-acousticbf-from-xcubememsmic1-lib-in-pdm-mode-to-use-together-with-dfsdm-peripheral-we-can-also-use-sai-peripheral-for-46-microphones-so-what-is-better-sai-or-dfsdm I am looking for a clear information about the main difference between these two protocol of communication in matter of CPU resources, computing, performance and power consumption.
I notice that there is an API, aci_gap_set_limited_discoverable(), which is designed to time out the STM32WB55 if no connection is made within a certain period. However, this option does not show up within the Cube (v6.2, just released) when setting up a custom template. This should be found under the BLE Advertising tab, Advertising Configuration, Advertising type. That is where you are supposed to select the advertising option, which dictates the api call made from from within Adv_Request(), the advertising request setup call generated by the Cube. I see no way to invoke the limited discovery api using the Cube. Does anybody know how or if the limited discovery option can be be done?
I am attempting to load an image onto the wireless coprocessor of the STM32WB55CGU6. I am using STM32CubeProgrammer through its wireless image tab to accomplish this, and I am following the instructions in the release notes provided with the binary image. When I do this, however, I get a pop up with the error FUS_STATE_ERR_UNKNOWN.I have seen previous posters have errors with having no secured section on their board, but the ESE option byte is enabled, as shown here:I have attempted to load the board with firmware to configure the USB for DFU and connect through the STMCubeProgrammer that way, but I get an error regarding the address for programming.Any advice on how to get this operational would be greatly appreciated!
Please, Help me.Attach log:PS C:\> STM32_Programmer_CLI.exe -c port=usb1 -fwdelete ------------------------------------------------------------------- STM32CubeProgrammer v2.6.0 -------------------------------------------------------------------USB speed : Full Speed (12MBit/s)Manuf. ID : STMicroelectronicsProduct ID : DFU in FS ModeSN : 20583172544EFW version : 0x011aDevice ID : 0x0495Device name : STM32WBxxFlash size : 1 MBytesDevice type : MCUDevice CPU : Cortex-M4FUS state is FUS_ERRORFUS status is FUS_NOT_RUNNINGFUS state is FUS_IDLEFUS status is FUS_NO_ERRORDeleting firmware ...Firmware delete finished
Hello,I'm booked in / confirmed for the STM32WL workshop on the 19th of March. Could anyone provide me with information about when the hardware pack (P-Nucleo-LRWAN2 and NUCLEO-WL55JC) is likely to be delivered? Should I expect to get an email confirming that is is on the way, or a parcel tracking number?Thanks,Chris
Hi, I've been trying to figure out how to get the above-mentioned LoRaWAN examples working on a STM32WL5 devkit.I'm at the point where I can join with OTAA on a Multitech gateway on the Things network, but I can't seem to get the devkit to then send any more packets.. Could someone please assist?Regards
Hi!My project consists of a bootloader and a main program that uses BLE functionality. If, after turning on the device, the main program was not started, then after switching the bootloader to STANDBY, I get a current consumption of 5 µA, taking into account the additional components on the board-OK. If the main program was started (respectively, CPU2->RUN), after the software reset, the bootloader puts the system in standbay, but the current consumption floats in the range of 30-70 µA. After that, the situation can only be changed by switching the power. I took code samples for switching to standby in STM32Cube_FW_WB_V1. 10. 1 PWR_EnterStandbyMode//in start main() after HAL init: if((LL_PWR_IsActiveFlag_C1SB() != 0) && (LL_PWR_IsActiveFlag_C2SB() != 0)){ LL_PWR_ClearFlag_C1STOP_C1STB(); LL_PWR_ClearFlag_C1STOP_C1STB(); } // SLEEP device: HAL_RTCEx_DeactivateWakeUpTimer(&hrtc); HAL_SuspendTick(); if((LL_PWR_IsActiveFlag_C1SB() == 0)|| (LL_PWR_IsActiveFlag_C2S
Its easy to fulfill requirements for startup ( I turn 3.6V LDO enable with 1.8V voltage), but when powerdown, the 3.6V decay is much longer and if 1.8V is already decayed, there is still 2V on 3.6V power line. Will this physically damage MCU or will it mess with brownout detectors ? Help ! :)
HiI did not got the second E-Mail you send me. Please invite me onec again. Hope it works
Hey all,I am trying to use the STM32WB55RG Nucleo board and for the application, I would have to use the board with the coin battery power supply (There is a coin battery slot for CR2032 battery). However, I could not see much information on how to change the configurations on the board to use battery power. It can be seen in the datasheet it is said that the SB29 should be closed to use the battery but I am not sure how to do it. Any help would be appreciated. Thank you.
Are additional external circuit components needed to reliably connect USB voltage to an ADC input, besides a voltage divider that brings 5V down to 3.3V?
Hello,I've confirmed my registration on feb 25th, but today i got an email stating my registration can't be confirmed. Is this an error?
Hello,I just received an email from ST; I registered for the 30 March workshop but due to reached capacity my registration was not confirmed. I would like to ask if there is the possibility to join the workshop on another day.Thank youAlessandro
I try to create end_node project for stm32wl5cc uC, but for unkonw reason to me it is impossible "End_Node" option is inaccessible (grey).In LoRaWAN_End_Node example it is available.Ho to do this in Cube Ide.When I try to import project from NUCLEO-WL55JC I can't change uC type to stm32wle5cc Mcu and Board It's also grey.
It is possible to use the ISE 1.6.0 instead of 1.5.1?
When a P2P server is advertising I am able to see the raw data values of the advertisement as well as the explained details using mobile app.(nRQ connect) Here I need to find exact same things using STM32WB as a client. I am struggling to find a way to extract those things. Also I need to extract the server's address from client side using raw data. Is that possible?
Hello,Recently I started working with Nucleo board with STM32WB55 and I would appreciate if somebody could help me with this issue about BLE. I never worked with the BLE stack before and I am quite lost and confused.I am working in a project where I only need to detect the SCAN REQUEST. In the learning process of STM32WB, I found the very useful MOOCs and more specifically “STM32WB Workshop – 3 How to add BLE funcionality�?. It Works with the project “HandsOn2�? supplied by ST.https://www.youtube.com/watch?v=zNfIGh30kSs&list=PLnMKNibPkDnGRfqUO1Q_-1nW-tOKfDQbc&index=4Among other things, it explains how to blink a LED every time a radio RF activity finishes, using Radio Activity Event. I thought following the steps of this event would be a good way to get a SCAN REQUEST event, but unfortunately so far I have not achieved anything. Please find below the pseudo code of app_ble.c file, where the radio RF activity is mentioned. - &n
Is it possible?
Hi, I am using the STM32WB55 Nucleo board for development (latest STM32Cube V1.2.0 FW). I need to obtain the RSSI value from iBeacon advertisements. I am doing a scan using ACI_GAP_START_GENERAL_DISCOVERY_PROC. The RSSI value returned in the HCI_LE_ADVERTISING_REPORT_EVENT seems to be garbage. I then started calling ACI_HAL_READ_RAW_RSSI, which does return data, but I can't seem to find any information on how to interpret the 3 byte array returned. Neither the application note (AN5270 rev3 June 2019) or the header file ble_hal_aci.h provide any details. Any information on how to interpret the raw RSSI data or alternate advice on how to get the RSSI from the received advertisement would be greatly appreciated. ble_hal_aci.h/** * @brief This command returns the raw value of the RSSI * @param[out] Value RAW RSSI value * @retval Value indicating success or error code.*/tBleStatus aci_hal_read_raw_rssi(uint8_t Value[3]);
WATCH ON-DEMAND | STM32 Summit 2026
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.