Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Most recent activity
Hi,I am new to the STM32WB range. I need to use the 1MB flash version in a project, But I am struggling a bit to understand the flash layout.I read that the first 6 Sectors are to be used my the OTA application. It seems like settings should go directly after that (say one sector). Then you can place your code.It is stated that the CPU2 application is at the end of flash. I cant seem to find any actual specifications on the exact location (or how big it is).And does the code for CPU2 actually live on the same flash space? I need to work out my boundaries. But it feels like i am missing some info that I dont seem to be getting from the docs.
Hello to everyone,I have two B-L072Z-LRWAN1 kit. Trying for measure best distance i can reach. I am using Ping-Pong example and change some variables such as LORA_SPREADING_FACTOR, LORA_BANDWIDTH, LORA_CODINGRATE, LORA_PREAMBLE_LENGTH etc. Until now, modules could not connect when spreading factor above 9. So i didnt achieve long distances. Anyone tried or know what is the best configuration for long distances.Thanks.
Sorry ST guys but the UART HAL and LL_HAL ist a total fail!I developing over 15 years all kind of serial communication with linux and different microcontrollers. Now I regret my desistion to use the STM32WB MCU. I'm trying over two weeks the get a stable UART communication running with different data length (5 to 50 bytes). All tries with DMA or Interrupt are failed. All this ST HAL examples are not realy usefull and if I search for some input I can read a lot and I mean a loooot of similar problem at the forums....Now I have to think about to went awai from this MCU or I have to write my own working HAL from scratch.It seams the marketing did a good job but the rest ???? I dont know....A unhappy user....
HI.In description of aci_gap_init() function writed:Initialize the GAP layer. Register the GAP service with the GATT.All the standard GAP characteristics will also be added:- Device Name- Appearance- Peripheral Preferred Connection Parameters (peripheral role only)but this function does not return ppcp handle.In AN5270 writed the same.Question: how to set ppcp characteristic (min-max interval, conn_sup_timeout, slave latency) ?Thanks.
I am developing a Beacon model application with ST bluetile. Bluenrg2 low power current consumption differs between SensorDemo (200uA) and Beacon application (1.8mA). I made sure that the bluetile goes into SLEEP_NO_TIMER mode and wakes up only when triggered. What is the contributing factor to the low power current consumption. Other than calling BlueNRG_Sleep(SLEEP_NO_TIMER,0,0). what else has to be checked to reduce the current consumption.
ST Micro store says it has 200 in stock, but the order won't go through. Tried AVNET, Digikey, etc. No luck.
Is the nucleo-wl55jc available in the market?And I wanna know what's the difference between the wl55jc1 and wl55jc2, which one of them should I buy for my region (North Africa)?
Hi,I'm using the example FLASH_WriteProtection with P-NUCLEO-WB55 with success but if I change the define FLASH_USER_START_ADDR in order to write only two (so I change the define FLASH_USER_END_ADDR in 'ADDR_FLASH_PAGE_250 + FLASH_PAGE_SIZE - 1') page from the PAGE_230 (adddress: 0x080E6000) I've a hard fault after I call HAL_FLASHEx_Erase.I want to delete and after write on this location because in my application I need to store at the end of flash some application data. What's the problem? regards,Giampietro
Dear sir/madam,I am interesting in using STM32WL55CC . Does its stack available for mesh or point to point ?does any 3rd party party require for mesh or point to pont?
With the throughput example if i use 2 WB55 boards, the maximum throughput that i get is 2KBpsDT = 2160 bytes/s lost = 0If i use my phone with PHY1, i get 90KBps+ and with PHY2 sometimes its 150KBps and sometimes 15KBps, on download. With upload its only 42KBps and 75KBps with PHY1 and PHY2 respectively. Also if i open upload tab first and then click on download, thp PHY1 speed is reduced to 40KBps. Why is that the transfer rate is all over the place? Why is upload slower than download? Which of these values is the correct one?
It seems I am having the same problem here: https://community.st.com/s/question/0D50X0000Az4HdhSQE/cant-get-the-advertising-state?t=1613668936202. Except the solution for that question was to make sure the memory buffer was mapped properly to SRAM2 and to be sure I have the missing IPCC interrupt handlers. However, I have the memory mapped correctly to SRAM2 and I have the IPCC interrupt handlers.So I'm wondering what I'm missing. Most of my code is very similar to the BLE_Datathroughput Nucleo example except I'm using FreeRTOS. I was looking at Figure 65 in this application note: https://www.st.com/content/ccc/resource/technical/document/application_note/group1/43/ea/2f/dc/10/a3/46/e6/DM00598033/files/DM00598033.pdf/jcr:content/translations/en.DM00598033.pdf. And I am able to send TL_Enable() but then I never get a signal back from CPU2.Any advice is much appreciated!
1. STM32WB55 unable to modify option bytes.2. It is not even allowing to do full chip erase. 3. M4 is running but M0 is not running hence it is struck at IPCC Initilization.
Hello, I'm using STM32WB55 for my application.My application is installed in 20 devices more or less.I set the RTC with RTC_HOURFORMAT_24.The RTC calendar is updated every 24 hours by cloud, usually.Only two of those devices, expose a problem with RTC: when reading the calendar the hours keep counting after 24 reaching more than 70 in some case.The day does not increase, passing 24 hours.The same issue (I think) also give me one differtent behaviour, after 12:59:59 the hours become 01:00:00 like the RTC was set to RTC_HOURFORMAT_12, but it is not!I use the set function in one part of the code, using these instructions:HAL_PWR_EnableBkUpAccess();HAL_RTC_SetTime(&hrtc, &RTC_TimeStruct, RTC_FORMAT_BIN);HAL_RTC_SetDate(&hrtc, &RTC_DateStruct, RTC_FORMAT_BIN);HAL_PWR_DisableBkUpAccess();Could some wrong operation overwrite the RTC register and change the settings in this way?Could someone suggest me a fix or a test to do?
I have a B-L072Z-LRWAN1 development board and am using it to send a PWM (0-100%) value to TTI and receive a PWM value to control a fan. The LoRa settings at the moment are:Class C deviceADR off (using DR_3)Confirmed uplinksNo periodic uplinksThe problem is when not using periodic uplinks, and only sending an uplink when a confirmed downlink is received there comes a time the confirmed downlink from TTI is not received on the board so, there is also no uplink, this triggers the 5 minute timeout for waiting for a reaction, but it will never come in those 5 minutes because the board doesn't receive anything and is listening for a message, so the communication is stopped for 5 minutes. At the moment we can set the timeout to 10 seconds or something using the command line interface (CLI), but it is not preferred because we want an uplink with every downlink. Has anyone experienced this problem before or does someone have something I can try.
Please forgive me for not attending the workshop, but I couldn't force Teams to cooperate.I had to go through at least 10 email and passwords resets and best i got to wasAADSTS50020: User account '--@---------.---' from identity provider 'live.com' does not exist in tenant 'STMicroelectronics' and cannot access the application '5e3ce6c0-2b1f-4285-8d4b-75ee78787346'(Microsoft Teams Web Client) in that tenant. The account needs to be added as an external user in the tenant first. Sign out and sign in again with a different Azure Active Directory user account.Yours sincerelyTomas Jakubik
I am trying to get quick-started with the following:STM32WB55 - Nucleo PackX-Nucleo-IKS01A3 (MEMS Inertial and Environmental Expansion Board)Stm32CubeIDE v 1.6.0STBLESensor (Phone app)FP-SNS-MOTENVWB1 v.1.0.0To start, I've flashed the provided binary from the function pack (STM32CubeFunctionPack_MOTENVWB1_V1.0.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\MOTENV1\Binary\MOTENV1_IKS01A3_WB55RG.bin ) onto my nucleo board, and that works as expected. I can pair with the board via BLE and view the output on my phone app.However, when I build and flash the project from CubeIDE, I don't get the same results. I created a new project from the Cube MX configuration file provided in the Function pack at \STM32CubeFunctionPack_MOTENVWB1_V1.0.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\MOTENV1\MOTENV1_IKS01A3_WB55RG.iocI get a warning that the project was set-up using Cube firmware version 1.2.0 and gives me the option to either migrate or continue. I have tried both options at this point. I build
Hey...Hi...HelloHope all are doing wellI'm dealing with TSM32WB with one of my project I'm using FreeRTOS with few peripherals like ADC (DMA), UART, USB, I2C etc I've create the few custom BLE services, out of them when i switch to accelerometer services (Code flow is almost similar with the SenorTile) then i'll cause the thread stuck at "b Infinite_Loop" at startup file I'm using the Cube IDE as a development environment When i open-up the stack analyzer then i found that the ADC1_IRQ_Handler the following message When i click on it then it's redirecting me on the startup file at "Infinite_loop"I've attached the screenshot of the stack analyzer Any suggestions please ?Thanks
I need a good STM32WL module. Can anyone advise me to choosing this?
Hello everyone,I'm trying to build a server application with the STM32WB55 but I can't get the advertising state. I took example on the server example in the STM32Cube_FW_WB_V1.0.0 and I think it is pretty similar but it doen't work as intended. I made some researches and I find someone with the same problem here : https://community.st.com/s/question/0D50X0000AhPJcCSQW/trying-to-get-the-advertising-state . However the proposed solution didn't work for me and I still can't get the advertising state. The programm doesn't run APPE_SysUserEvtRx() because I don't receive VS_HCI_C2_Ready I think.Would anyone has any idea on why it behaves this way and how to solve this problem ?Thank you.
Hi all,How can I launch a request to synchronize the date/time at the application level using the LoRa's Stack that the STM32WL uses?I have seen that there is a function to launch that request, but it is not accessible at the application level since it is defined in the .c but not in the .hLmHandler.c <<LmHandlerDeviceTimeReq()>>Is there any way to call this function without modifying the codeBest Regards, Sergio
Do the new products offer coded PHY for long distance BLE?
How may I obtain the P-Nucleo-LRWAN2 pack, my special interrest is the Gateway.
The documentation for STM32WB55 Nucleo states that a 5.2 stack is available ("comes with") but the BT stack provided in STM32Cube_FW_WB_V1.11.0 is a 5.0 stack...Regards,AC
Hi,I received my kit and saw that the package was damaged in some place. After powering on NUCLEO-L073RZ, no obvious problem (LED are OK).On NUCLEO-F746ZG, everything seems OK too (LED OK)On LRWAN_GS_HF1, no LED turns ON. If I understand well, at least a PWR LED is supposed to turn on when powered.I tried both Power connector (on the LRWAN_GS_HF1 and on the NUCLEO-F746ZG, with the same result. I suspect that the board is DOA.Can you help please?Thanks.
Hello,We are finalizing the low power modes of our project and can't manage to solve this issue.We are going correctly into Low Power Mode via the UTIL_SEQ_Idle and related functions...But it looks the CPU2 (BLE) doesn't wake up the CPU1.Our application launches a aci_gap_start_general_discovery_proc and then sends the CPU1 to sleep....I'm waiting for the completed scan event ( EVT_BLUE_GAP_PROCEDURE_COMPLETE ) but we don't receive it, sometimes it works because in the main code we have timers that wakeup regularly CPU1 so if the completed event occurs when CPU1 is running everyrhing works.What are we doing wrong?ThanksMassimo
WATCH ON-DEMAND | STM32 Summit 2026
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.