Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Most recent activity
I read some contradictory information and I am not sure what is true. According to the document https://www.google.com/url?sa=t&rct=j&q=&esrc=s&source=web&cd=&ved=2ahUKEwjX3NCZvoDwAhVIY8AKHe2zCrkQFjAAegQICBAD&url=https%3A%2F%2Fwww.st.com%2Fcontent%2Fccc%2Fresource%2Ftraining%2Ftechnical%2Fproduct_training%2Fgroup1%2Ffe%2F40%2Fb3%2F78%2F6f%2F98%2F46%2F84%2FSTM32WL-System-Power_control_PWR%2Ffiles%2FSTM32WL-System-Power_control_PWR.pdf%2F_jcr_content%2Ftranslations%2Fen.STM32WL-System-Power_control_PWR.pdf&usg=AOvVaw0jeJwKlPWB-quea87ZodxM"The main power supply VDD ensures full-featured operationin all power modes from 1.71 up to 3.6 V, allowing supply byan external 1.8 V (+-5%) regulator. Device functionality isguaranteed down to 1.61 V, the minimum voltage after whicha brown-out reset is generated.sub-GHz radio operation is allowed down to 1.95 V."I don't see any mention of this in DS13105 Rev 8 or RM0453Reference manual. Does Everything operate down to a
..
I bought NUCLEO-WL5JC2 Low Band (As NUCLEO-WL5JC1 were not in stock)Is it possible to turn them into High Band by changing some passive components ? So I can use them in 868Mhz instead of 433Mhz Thanks
I am trying to do the example "HandsOn_2" from STM32WB_workshop. Executes commands as described. The only difference is I use STM32Cube_FW_WB_V1.3.0 instead of STM32Cube_FW_WB_V1.0.0.STM32Cubex does not copy the scheduler.c, scheduler.h files to the directory ...\Middlewares\ST\STM32_WPAN\utilities\ . Why in STM32Cube_FW_WB_V1.3.0 files scheduler.c, scheduler.h don't exist?
I want to reset and reinitialize only CPU2 (M0 +) of STM32WB I used to ask a question in "Data reception stops at Mac_802_15_4_FFD in the sample code."Even now, this matter has not been resolved.At the end, it was said that RFD was used, but since I want to communicate with FFD, I have not confirmed it with RFD.I would like to resolve this phenomenon, but if I can confirm this phenomenon with F/W, I would like to reset and reinitialize only CPU2.Is such a thing possible? How can I do it?
Environment:MacOS 10.14.6STM32CubeIDE 1.6.1STM32WB SDK 1.11.0Starting with a clean install of Cube, SDK, empty workspace. Importing p2p_Server project (from the initial splash screen->Import STM32 sample app), the build fails with (among other):/Users/skajam66/Developer/stm/workspace/BLE_p2pServer/STM32_WPAN/App/app_ble.c:517:11: error: 'handleNotification' undeclared (first use in this function); did you mean 'HRS_Notification'? 517 | handleNotification.P2P_Evt_Opcode = PEER_CONN_HANDLE_EVT; | ^~~~~~~~~~~~~~~~~~ | HRS_Notification /Users/skajam66/Developer/stm/workspace/BLE_p2pServer/STM32_WPAN/App/app_ble.c:517:11: note: each undeclared identifier is reported only once for each function it appears in /Users/skajam66/Developer/stm/workspace/BLE_p2pServer/STM32_WPAN/App/app_ble.c:517:47: error: 'PEER_CONN_HANDLE_EVT' undeclared (first use in this function); did you mean 'HIDS_CONN_HANDLE_EVT'? 517 | handleNotification.P2P_Evt_Opcode = PEER_CONN_HANDLE_EVT;Adding an include state
In the pack FP-AUD-BVLINKWB1, BLE audio streaming example provided with Opus codec, will you be also providing similar example using new LE audio standard with LC3 codec?
Namaste from India.I am working on STM32WB Nucleo board for BLE functionality as per the tutorial available: https://www.youtube.com/watch?v=zNfIGh30kSsI have copied the codes from workshop snippets provided by ST. When I press the LED on the ST BLE sensor App, the LED of the Nucleo board toggles its state. When I press the button switch 1, the notification is not received in the BLE app. The LED stops blinking and debugger shows this message: SIGTRAP:Trace/breakpoint trap) HardFault_Handler() When I use the p2pServer project provided by the ST, it works flawlessly. If I build the project from scratch by following the tutorial, I am facing this issue.Cube IDE Version: 1.6.1CubeMX version: 6.1.1STM32Cube_FW_WB_V1.10.0Anyone here should help me.RegardsRaghavendra
Hello,function "aci_gap_delete_ad_type" returns value "0x1F". This value is not defined in file "ble_defs.h" at lines 192ff like other return values ("BLE_STATUS_SUCCESS" etc.)Do you confirm that the meaning of "0x1F" is "AD_TYPE not found" ?Can you add a "#define" with comment for this value to "ble_defs.h"?Best regardsPaul
I need to program the chip use JTAG or SWD, But now i could just read the jtag id. i could not access the flash. so is there special document for how to access the flash using JTAG or SWD interface.
I am going to download the ble stack to stm32wb55 using the program. On P-NUCLEO-WB-55, it was downloaded properly, but I tried the same thing on my custom board, but it failed.This is the log we did on NUCLEO-WB55 below.Deleting previous wireless stack... C:\Users\cupid\AppData\Local\Temp\STM32WBUpdater\STM32CubeProgrammer\STM32_Programmer_CLI.exe -c port=usb1 -fwdelete ------------------------------------------------------------------- STM32CubeProgrammer v2.1.0 ------------------------------------------------------------------- C:\Users\cupid\AppData\Local\Temp\STM32WBUpdater\STM32CubeProgrammer\STM32_Programmer_CLI.exe exited with code 0 USB speed : Full Speed (12MBit/s) Manuf. ID : STMicroelectronics Product ID : DFU in FS Mode SN : 206B389E3036 FW version : 0x011a Device ID : 0x0495 Error: Device not supported RSS state is RSS_ERROR RSS status is RSS_NOT_RUNNING RSS state is RSS_IDLE RSS status is RSS_NO_ERROR Deleting firmware
Hi when trying to get some of the examples for the STM32WL devkit (Nucleo-WL55JC1) working for LL LPUART serial with the external 32kHz crystal, I've noticed that LL_RCC_LSE_EnablePropagation() is never called in SystemClock_Config. It looks like this is needed for LPUART to use the crystal as its clock?I also can't seem to find an option in CubeMX to enable LSE as a system clock for LPUARTThe examples I've tried from STM32Cube_FW_WL_V1.0.0: Examples_LL -> LPUART -> LPUART_WakeUpFromStop_InitExamples_LL -> USART -> USART_Communication_TxRx_DMA_Init
I want to continuously send bytes from one device to another, both of the device using BlueNRG-2 microcontroller, I can send next packet when TX_BUFFER_FULL was not set. when the tx power level was set to 4 using aci_hal_set_tx_power_level(0x04), everything worked well,however, if the tx level was set to 0x07, the first 1.8k bytes (200bytes per packet) can sent successfully within a short period of time (same as TX=4). however, i cannot send the 10th packet within a short time. the TX_BUFFER_FULL was set for a much much much longer period of time. i also tested my code using two evaluation board, i did not have this problem. for both tx level(4 and 7), the code worked well.anyone knows why?
Dear,My goal is to erase some flash sectors after the receipt of a specific BLE notification ( ChardId = OTAS_STM_BASE_ADDR_ID / Command = OTAS_STM_APPLICATION_UPLOAD) (line 17 in the first code sample). Once the operation done, I should notify the initiator via BLE using the method OTAS_STM_UpdateChar().The issue is that the notification is correctly read by the initiator if I do not perform the erase operation, and is NOT read by the initiator if I perform the erase operation. Therefore, I suspect this flash erase operation to disturb the BLE protocol. Here the code dealing with the received notification from the initiator :switch(p_notification->ChardId) { case OTAS_STM_BASE_ADDR_ID: { switch( ((OTA_STM_Base_Addr_Event_Format_t*)(p_notification->pPayload))->Command ) { case OTAS_STM_STOP_ALL_UPLOAD: break; case OTAS_STM_WIRELESS_FW_UPLOAD: OTAS_APP_Context.file_type = Wireless_Fw; OTAS_APP_Context.base_address = FLASH_B
My application only needs to send data once every few minutes during which time i can save power by turning off the radio. I don't see any examples that do it, they don't even have a deinit function.
Hello,I tried to open and test a LoRaWAN example for the STM32WL, Nucleo-6344 board but it returned an error message shown in the attachment.Can you advise, please?Thanks,Mohammed
Hello.I have a STM32 Nucleo board and a USB dongle. What Stack and FW should be programmed to use STM32CubeMonitor-RF 802.15.4 RF test mode described in chapter 5 of the UM2288?Thanks.
Hello,I have created mesh by embedded provisioner. Mesh contains, let's say, 5 more nodes. I know where are saved node addresses, number of elements and device keys for all nodes (embedded provisioner has them saved in NVM memory). Is there any function or place in NVM memory, which contains more information about each node? Let's say, type of model (generic on/off, sensor server,...), property ID of sensor server model, publish/subscribe address etc.I am using Nucleo board with STM32WB55RG and SDK version 1.10.0. Vit
Hi there!I added 3 characteristics to the p2p server example, with lengths of 2, 2 and 64 bytes. Event processing occurs directly in the p2p_stm_app_notification (p2p_server_app.c) function. The Client performs 16 iterations a La:{ char1.write(2 byte); char2.write(2 byte); delay(100 ms); char1.read(64 byte); }It takes about 12 seconds, it's too slow. The client application was implemented on flutter(android) and on the script for BLEConsole(Win 10), running on different devices, the execution time is unchanged, so I think that the problem is in my implementation of the application on STM32WB. The first thing I tried to change was Slave_Conn_Interval_Min and Slave_Can_Interval_Max in the aci_gap_set_discoverable function at 6, and 80 (accordingly 7.5 ms min and 100 ms max). In the EVT_LE_COQ_COMPLETE handler, the value connection_complete_event - >Count_Interval = 39 ( accordingly 50 ms). But it didn't increase the speed. Tell me please, what can be the
and I cannot change and even read option bits via stm32cubeprogrammer. hjow can i save and restore my board? Yasser
I would like to turn on the LED on the board with an external switch instead of using the one provided on the board. Which pins do I use and how do I approach this?
As soon as I add a task to the scheduler and schedule it to run once every 5 seconds, when the timer fires and the sequencer tries to run the task the STM32 goes to the hard fault handler.I'm using the latest example BLE_p2pServer from STM32CubeWB 1.5.0, the example is as-is, except for adding "deviceModes.c":#include "deviceModes.h" void StandbyMode(); void QueueStandbyMode(); const int SCH_PRIORITY_STANDBY_MODE = CFG_SCH_PRIO_20; uint8_t standbyTimerId; #define FIVE_S (5 * 1000 * 1000 / CFG_TS_TICK_VAL) void RegisterDeviceModes() { UTIL_SEQ_RegTask(CFG_TASK_STANDBY_MODE, UTIL_SEQ_RFU,StandbyMode); HW_TS_Create(CFG_TIM_PROC_ID_ISR, &standbyTimerId, hw_ts_Repeated, QueueStandbyMode); HW_TS_Start(standbyTimerId, FIVE_S); } void QueueStandbyMode() { UTIL_SEQ_SetTask(1 << CFG_TASK_STANDBY_MODE, SCH_PRIORITY_STANDBY_MODE); } void StandbyMode() { BSP_LED_Toggle(LED_RED); HAL_Delay(5); BSP_LED_Toggl
Hi all,I cannot detect MCU STM32WLE5CC by ST-Link V2.My schematic:Could you show me my mistake? Thank you very much.
WATCH ON-DEMAND | STM32 Summit 2026
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.