Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Most recent activity
Hi guys. When I program the device with LoRaWAN and DAC with pin extern (PA10), I saw in oscilloscope that DAC stay high every when has uplink. Like the image: Does anyone have any idea why this happens? Thanks!
Hi,I am looking for a dual core controller and options I have been able to find out are:Stm32Wb seriesStm32H seriesBeing, H series quite expensive, Is it possible to use WB series M0+ for running another application in parallel?Or we can only use it for Radio implementation.Regards,Anurag
I set the OB bit to 0xe4, but it shifts left 1 on flash with IDE. MAPPING_TABLE 0x00000000200000e4 0x13c load address 0x0000000008003744 MAPPING_TABLE 0x00000000200000e4 0x13c MbMux/mbmuxif_sys.o 0x0000000020000220 . = ALIGN (0x4)0x00000000200000e4 become 0x0000000020000e40
There is something missing upon receiving junk .How do we keep the count of how much response will be received in advance ? should any flags be set to check whether the response received is correct and clear upon not receiving proper response , bit confused . please helpThanks in advance.
In STM32WL55JC2, there are LORAWAN, SubGHZ ,SigfoxI just want to connect physical lora TX RX .
Hello.I run BLE_HeartRate_ota example on STM32WB55 (nucleo MB1355C). After connecting to ST BLE Sensor App I have corresponded HeartBit application GUI.In the settings there is option "Set node time", but it is inactive.What should I add to STM32WB55 SW to activate this feature on my smartphone? Could somebody advise an example or an article, please?
We are trying to work out how much flash is used in total for a given project, and how much more is actually available for development. For example, when compiling the BLE_BloodPressure example project (in Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE\BLE_HeartRateFreeRTOS\STM32CubeIDE), the Build Analyser output of the BLE_BloodPressure.map file is as below- Does this really mean that there is 449.25KB free, or is some of this used by the coprocessor binary?
I have a single channel lora GATEWAY (DRAGINO LGO2) since it can only transmit packets in 1 channel like 868400000, I couldnt activate my stm32-wl55Jc1 with that gateway via ABP mode. Would you please guide me to config the stm32-wl55Jc1 to transmit packets in just 1 frequency is there any solution?
I used STM32CubeIDE 1.6.1 and STM32_WL V1.0.0 to create the LoRaWAN_End_Node example project. When I edit the IOC file to simply add support for CRC and regenerate sources, I can no longer build the example.I get a huge number of duplicate symbol errors - example:C:/Users/danam/STM32CubeIDE/workspace_1.6.1/LoRaWAN_End_Node/Middlewares/Third_Party/LoRaWAN/Utilities/utilities.c:73: multiple definition of `memcpyr'; Middlewares/LoRaWAN/utilities.o:C:/Users/danam/STM32CubeIDE/workspace_1.6.1/LoRaWAN_End_Node/Middlewares/Third_Party/LoRaWAN/Utilities/utilities.c:73: first defined here c:\st\stm32cubeide_1.5.1\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_1.5.0.202011040924\tools\arm-none-eabi\bin\ld.exe: Middlewares/LoRaWAN/Utilities/utilities.o: in function `memset1': C:/Users/danam/STM32CubeIDE/workspace_1.6.1/LoRaWAN_End_Node/Middlewares/Third_Party/LoRaWAN/Utilities/utilities.c:82: multiple definition of `memset1'; Middlewares/LoR
if (OptionsBytesStruct.IPCCdataBufAddr != (uint32_t) pMb_RefTable) { /* USER CODE BEGIN MBMUXIF_SystemInit_Prevent_OB_Programming */ /* WARNING: If there is a difference between the MAPPING_TABLE placement in memory */ /* and the address calculated according to the IPCCDBA option byte, */ /* To avoid writing the IPCCDBA OB by mistake, the execution enters now in a while(1){} */The IPCC addr and MBMUX_ComTable_t value are compared: My results are IPCCdataBufAddr = 536871136 MBMUX_ComTable_t *pMb_RefTable = 536871140Where do I change this offset value?
I accidently put the FUS and BLE firmware in the wrong starting address. The chip has 1M flash. When I loaded the firmware, I was following the 512K flash memory location. Now I cannot perform full memory erase as some areas (from index 243 - 245, total of 255) are locked. Is there a way to erase these areas?Thanks,Charles
Hello!I'm using stm32wb nucleo board as a central device to connect multiple peripherals. An input data stream from one device is about 40 kb/s, there can be up to three devices. After successful connection the client board starts to get notifications. But at some point the central device stops processing events - such as ACI_GATT_NOTIFICATION_VSEVT_CODE, HCI_DISCONNECTION_COMPLETE_EVT_CODE etc (it could be 10 minutes, half hour or several hours). I know for sure that peripherals continue to transmit data. After this I can't disconnect peripherals, start discover or other ble actions. But as I can see in debugger peripheral stay connected. I have not found a reason why this happens and solution for this problem.Maybe someone had the same issue?Best regards,Den
..
Hello,I was wondering what the maximum transfer speed is of the single wired (Half-Duplex) LPUART connection of the STM32WB55CGU. The clock configuration shows a clock frequency of 64Mhz, the baud rate is by default 209700 Bit/s. Is it possible to transfer at 1Mbit/s, or more?Thank you!
Hi All, wondering if there are any Android/iOS libraries that allow integrating the OTA DFU update process for the STM32WB55 to our App?Thanks!
The example non-dual core runs perfect. The dual core doesn't run out of box. Is there some presentation or walkthrough I'm missing?
The board stays in join request mode. Single Core setup runs perfect.
I am using I-CUBE-LRWAN to create a LORA end-node device. But the documentation does not say anything about how to create your own device using this extension. I have two questions:1) Can this extension be integrated into CubeMX?2) Are there instructions on how to use this extension to create your own device?
hi,I need to run a freertos ble project on stm32wb5mm-dk board like "BLE_HeartRateFreeRTOS" example project avaiable for p-nucleo-wb55 board, but there isn't any avaiable and if I try to replicate it from new project it don't work, "APP_BLE_Init()" is never callde, like cpu2 is not started, how can I achieve this?
On debug, the LoRa device gets stuck in a busy-signal loop. What is the part of the chain I'm missing, in config?
Hi,I am using STVM32WB5MMG-DK for my project development activities.When I referred the user manual "UM2825", I came to know that the STM32WB5MMG USART1 interface is connected to the UART2 port of the STM32F103 ST-LINK/ V2-1 MCU.Is there anyway that USART1 of STM32WB5MMG can be used for normal serial application related thing and LPUART1 to be used as Virtual COM Port?At present am using LPUART1 to send/receive data packets and USART1 as Virtual COM Port for debug printing(USART1 console)Thanks.
I am new to this area and I just bought two P-nucleo-wb55 boards. When I used the p2p server example, it can work properly and I am able to use my phone to control the on/off of the led. However, when I tried with another sample 'BLE_HeartRate', it can build properly but after I click debug, LED6 become red forever and I can no longer connect to the device anymore. I have also tried to look at it with st-link unity and stm32 targe information becomes always "Detection Failed" after the program 'BLE_HeartRate' is input.I have tried with both boards and they have the exact same problem after clicking debug with 'BLE_HeartRate', so I guess it must be something wrong with this example.But the main problem lays in how can I recover my boards to their original state or if the mcu are already damaged and unrecoverable. I had tried to connect the boot 0 to 3V but nothing seems to happen. Any help would be appreciated. Thank you.
STM32WL55 family devices need unique credentials on a chip-by-chip basis. These include DevEUI, AppKey and AppEUI, as well as Region etc.What strategies are there to permit this provisioning during the manufacturing process?I am thinking of this process, but I would like to hear of others: initially all devices have the same DevEUI, AppKey and AppEUI. They connect to a LoRaWAN application which then sends them new values for DevEUI, AppKey and AppEUI. The device stores these in a sector of its flash memory, set aside as NVM. On subsequent boots, these new DevEUI, AppKey and AppEUI values are used in place of the defaults.What other strategises? Any software available?
The module that was used on this PCB was the STM32WB5MMGI/O was connected according to the datasheet attached for STM32WB55MMGShort found on 3V3 on 6 out of 6 sample prototypes. When module was desoldered from the PCB, the short went away on both PCB and module. Solder bridging was suspected. Post-mfg x-rays showed 3 possible solder bridges, with one of them on 3V3 pin. However, this one was bridged to an unconnected pin.SWDIO and SWCLK were already identified as incorrect connections. There are two schematic attachments, one for before and after this was changed the ECAD. The layout attachments are after the changes.
WATCH ON-DEMAND | STM32 Summit 2026
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.