Associate II
Jun 30, 2021 7:17 PM UTC
Question
Assuming the manufacturing was done correctly, are there any I/O connections that would cause a 3V3 short?
- 3 replies
- 5734 views
- The module that was used on this PCB was the STM32WB5MMG
- I/O was connected according to the datasheet attached for STM32WB55MMG
- Short found on 3V3 on 6 out of 6 sample prototypes. When module was desoldered from the PCB, the short went away on both PCB and module.
- Solder bridging was suspected. Post-mfg x-rays showed 3 possible solder bridges, with one of them on 3V3 pin. However, this one was bridged to an unconnected pin.
- SWDIO and SWCLK were already identified as incorrect connections. There are two schematic attachments, one for before and after this was changed the ECAD. The layout attachments are after the changes.