Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Most recent activity
..
For evaluating the WB55 i would like to have software on a PC that can accept data from the Nucleo board over BLE. Since my PC doesn't have the latest Bluetooth version i want to use a WB55 as the radio. Zephyr RTOS has an example that would make the board enumerate as a Bluetooth dongle after which i can use the Bluetooth stack in Linux for writing my software. However this firmware only compiles for the nordicsemi boards, the required code is not implemented for WB55. Does ST have something similar?
Hello,I am searching online for a BLE P2P example or tutorial but am having a very hard time finding anything that is relevant and not outdated. I am very new to BLE, this is my first application and could really use some assistance getting up and running.Does ST have anything like this available?Thanks for any help.
Is it possible to output the debug info on a STM32WB30 through usart?The option stays off in cubeMX and when I turn it on manually ZbInit() returns NULL.Is there a working example for the STM32WB30?Thanks!
Hello. I'm currently working on an IoT-related project using B-L072Z-LRWAN1 Discovery kit with STML072CZ microcontroller. In order to estimate when the battery will run out, I'd like to create some C++ program on Mbed OS 6.15.0 that monitors the battery voltage. However, I have no clue how to achieve this. I began using B-L072Z-LRWAN1 and also Mbed OS 6 pretty recently. Any help would be much appreciated. Thank you.
Example given on STM32WB55 github page is not working on my Nucleo board. Are there any new updates? Is someone having the same problem? Also, I would like to know are there any examples except this one? (Only HeartRate is given as a possibility on CubeMX)
Hello! I have configured the RTC in cube with a frequency of 1Hz in the board STM32WB55, and I want so as to each second the RTC interruption set a task. I found out that I should use RTC_IRQHandler, but in my project I can't found this function, I don't know how to enable RTC interruption, in cube V1.5 I only see the alarm's interruptions. How should I proceed?
Hello, Selecting the NUCLEO WL55JC2 board, then initialized with the peripherals.Enabled both SUBGHZ and SUBGHZ_PHY mode.(in older SUBGHZ_Phy_PingPong stm32cubewl software there was predefined RF SW CTRL pins and other board resources)How can i define RF SW CTRL in SUBGHZ_PHY Platform settings in new template without depending on SUBGHZ_Phy_PingPong ioc template file?
Hi,I’m trying to implement OTA using the example software and hardware below. But it seems very unreliable.STM32Cube_FW_WB_V1.7.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\BLEBLE_OtaBLE_p2pServer_otaCompiled with IAR for ARM 8.50STM32CubeProgrammer API v2.4.0STM32CubeMonitor-RF Version 2.5.0STM32WB55 Nucleo PackNucleo board PNWB55$CU3USB DongleI programmed BLE_Ota.out and BLE_p2pServer_ota.out into the P-NUCLEO-WB55 using the STM32CubeProgrammer and verified the green LED is flashing indicating RF messages.I then used the STM32CubeMonitor-RF with the USB dongle and Nucleo board about 5 cm apart.And then I tried to perform an OTA update. I found mostly it worked, but sometimes it failed. When it failed, the flash memory at 0x08007000 was all FFs (which is where the new application should be located). I added a break point to BLE_Ota and verified this was due to an invalid magic number (0x94448A29).When you create a build the address of the last word in your image is stored a
I am trying to set up a bootloader where I can transition CPU2 to FUS, then back to the wireless stack. I followed the examples of sending 2 FUS_GET_STATE commands to enter FUS. Then I send the FUS_START_WS with the SHCI_C2_FUS_StartWs call. Nothing happens. No reset (like the docs say) and the next time I call SHCI_C2_FUS_GetState I get a FUS_STATE_ERROR_AUTH_TAG_ST_NOTFOUND response. I can start the stack using the Cube programmer, so I know the image is good. How do I do this from code? I am using v1.12.1 of stack and v1.2 of FUS.thanks.
Hello!We are developing the BLE application on STM32WB55 along with the mobile app companion. The microcontroller is in a Peripheral role, mobile app - in Central.After BLE connection is established, MCU firmware sends a security request and master initiates the pairing procedure. We chose Passkey entry pairing method and after the first successful pairing, the mobile device is added to bonded devices, so that we can skip entering pin code for the next connections.In most cases, everything works flawlessly, however, we faced a problem with bonded devices information loss after MCU firmware update. It repeats every time we update the core2 firmware and sometimes after updating core1 firmware. Could you specify where exactly the bonded devices information is stored? The AN5289 mentions that "When devices are bonded, the keys are stored in the non-volatile memory area." How can we avoid erasing this FLASH area while updating firmware on both cores?
Is it possible to run a custom radio stack on M4 core of STM32WB processor without using M0 core ? If yes, where can I find the manual to read about accessing radio peripherals from CPU1
Hello geeks..Hope all are doing well I'm using multi channel ADC with STM32WB having DMA activated My issue is, every time when i perform the power ON reset, at the same time the channel sequence getting change! It means, the conversion buffer in HAL_ADC_ConvCpltCallback function sequence is getting changeI have verified the same thing manually by connecting the 3.3V & GND at the particular channelsFor example, when i connect the 3.3v at PC4 then the allocated buffer variable shows 4096 samples. However when i do the power on reset then some different buffer shows the value 4096I have activated the 6 channels here with DMA I have shared ADC initialization code snippet here Can any one help me here ?All suggestions & comments welcome Thanks /** * @brief ADC1 Initialization Function * @param None * @retval None */ int32_t BSP_ADC1_Init(void) { /* USER CODE BEGIN ADC1_Init 0 */ /* USER CODE END ADC1_Init 0 */ ADC_ChannelConfTypeDef sConfig = { 0 }
hey there! I'm planning to design my own PCB based on the STM32WL55 (900MHz range) and I have the NUCLEO reference design to look at, but find that here's a lot of RF paths in there, and I just want to know if there's any discussion anywhere on how much of all this is actually needed. ideally I would like to get rid of those RF switches and multiple paths, but I'd like to understand a bit more about what would happen if I did. And I'd also like to do that as fast as possible with as few PCB iterations as possible. :)1) does the Rx path really need to be isolated from the TX paths with an RF switch rather than just linked up? (with impedance matching of course!) if so, what are we achieving with the switch?2) What would the penalty be (assuming LoRaWAN!) if I was to just go with one PA output? I'm guessing that depending on what one I picked, either I'm transmit power limited or I'm limited in how much I can reduce battery draw during good quality link conditions... but I also need to u
Hello,I have two NUCLEO_WL55JC2 boards. I am starting with SubGhz_Phy_Per example. One of board is Tx and other is Rx as mentioned readme.txt in project files.Rx board's red led is blinking that means the board does not receive any signal. My jumpers are at initial settings. I suspected power and I tried with external 5v. It did not work. I was waiting ready to use demo.Do you have any suggestions? Should I do any change in configuration files?
Hello, I am currently working on two projects and the firmware is tested and verified on two mcus ( STM32L476RG and STM32WB55CG). I would like to consider different MCUs where the code can run without changing the code. I know if I consider the ICs from the same family I could do this if there are no changes in the flash interpretations. Could you please suggest some ICs and if I am considering ICs from other families what all changes need to be done to the code. Do I have to change the libraries? Is it a time-consuming process? What is the easiest approach to convert the code? I am using Keil IDE for coding.
I am using Serial Wire Debug (SWD) to trace some debug information while using the STM32WB55CGU6U MCU. Based on UM2609, the default maximum size of the SWV trace buffer on a PC = 2,000,000 packets. This buffer is stored in the heap of the STM32CubeIDE. Both parameters can be increased and I have no problem with that. However, in UM2609, I have not found the definition for the SWV packet. What is the size of this packet? What is the maximum size of the user data that can be fit into one packet?
I'm working on a mobile project based on the STM32WB5MMG.First, we bought a P-NUCLEO-WB55 and had a look at some of the example projects.After a good experience with the Nucleo board, we decided to build HW around the controller.Now the HW is working and the BLE_Stack has been flashed to the device.Even some examples are working on our platform.Now I want to implement two specified services "Battery Level" and "Automation I/O".For this, I build upon the "BLE_Custom" example and moved to a custom .ioc file/project later.But now I'm stuck. Is there any documentation of the generated code for the "Custom Template"? I found a few functions in the STM32WB HAL library, but non of the template-related stuff.Detailed Problems:1) I'm able to show services and characteristics to a device (phone/pc) read and write to it.Now, I would like to update a specific characteristic. Therefore I used "aci_gatt_update_char_value()". But it seems I'm, not allowed to change the value while the service is
The datasheet only shows the current of the STM32WB55 at 3.3V; what happens at 1.8V? In particular: how is the radio section affected by the voltage drop? Does the current drawn in TX and RX remain the same even at 1.8V? (Rx 4.5 mA / Tx at 0 dBm 5.2 mA) And how is it possible that even in reception it consumes so much? (Rx 4.5mA)Many thanks, Nino
STM32Cube/Example/BLE_AT_Client/readme.html requirement:This example requires to have STM32WB5M module flashed with latest BLE_AT_Server application from STM32CubeWB package.I downloaded stm32cubewb_v1-12-0 and patch-cubewb_v1-12-1 but these zips do not contain the binary specified.
Hello,I have an application with STM32WB55 that is working without a problem using UTIL_SEQ_Run(UTIL_SEQ_DEFAULT); and i am using app_ble_update_data function to update the packet data but i would like to start advertising without using UTIL_SEQ_Run(UTIL_SEQ_DEFAULT); so how to call the function that is responsible of starting CPU2 to start sending the packets without starting the sequencer? I have already tried hours trying to find out how to but the sequencer is really nested and each function calls a lot of others! Thanks a lot in advanced.
Hello! I'm trying to interface with a sensor that requires a repeated start condition.Datasheet: https://www.mouser.com/datasheet/2/348/ROHM_S_A0005047448_1-2562246.pdfI have other sensors on my I2C bus that I can communicate with. I also get '1' on HAL_I2C_IsDeviceReady(&hi2c1, 0x5B, 3, 5);I tried using HAL_I2C_Mem_Read, as it's my understanding that this function does a repeated start, but it doesn't seem to work with the sensor (this function works with 3 other sensors on my bus).I'm assuming the implementation of HAL_I2C_Mem_Read doesn't meet my requirements.The sensor I'm interfacing requires: [ST][SLAVE ADDR][W/0][ACK][READ REG][ACK][ST][SLAVE ADDR][R/1][ACK][DATA][NACK][SP]What am I getting wrong here?Using STM32WB, with CubeIDE.Thank you!!! :)
I have a custom board running the i cube lrwan (class A). I m going to deploy it in the field, so I dont want any messages coming on the UART. Is there a way to disable it ?When I add too many print statements for debugging, the LoRa Initialisations seems to freeze and hang up.Thanks
WATCH ON-DEMAND | STM32 Summit 2026
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.