Skip to main content
Hamdi Oussema
Associate
June 28, 2021
Question

I Nucleo lrwan problem

I'm currently using I Nucleo lrwan1 shield and STM32L073 to create a Lora end node. I downloaded the latest I cube lrwan (v2.0.0) and there is no configuration to the I Nucleo lrwan1. So I can't make it work.

So, is there anyone who has the same problem or can anyone guide me to make it work.

I also posted the problem on the TTN forum and they recommended me to ask the st community about this problem

here is the link : https://www.thethingsnetwork.org/forum/t/i-cube-lrwan-problem/48864/3

This topic has been closed for replies.

23 replies

ST Technical Moderator
June 28, 2021

Hello @Community member​ ,

I advise you to refer to this FAQ: LoRa communication within STM32, which concerns the LoRa communication and contains several helpful links to get started withLORA.

Have a look also at this link, it may be helpful.

Please, keep us informed about your progress on this issue.

-When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.-

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Hamdi Oussema
Associate
June 28, 2021

okay, thanks

Tesla DeLorean
Guru
June 28, 2021
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Hamdi Oussema
Associate
June 28, 2021

the first one : I-NUCLEO-LRWAN1

Tesla DeLorean
Guru
June 28, 2021

Not sure ST provides firmware for the USI model. It is possible to replace the USI firmware (protected against readout) with code built off the ST / Semtech stack, but certainly in the 1.x.x days this required a custom HW Configuration file dealing with the pins, and also dealing with the RF switching. USI once upon a time had a list of diffs to modify the code, and I'd previously built code for it, and my local FAE did too.

It is a compact platform, but I liked the Murata module a lot more, it had the SX1276 and a larger L072 for firmware

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
ST Technical Moderator
July 2, 2021

Hello,

I will try to contact expert internally to review this post.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Andrew Neil
Super User
July 13, 2021

thanks - ST expert has responded in this thread:

https://community.st.com/s/question/0D53W00000vP1XtSAK/icubelrwan-v200-with-nucleol073rz-board-and-inucleolrwan1-shield

It is confirmed that the AT_Master project in I-CUBE-LRWAN v2.0.0 (March 2021) does not work out-of-the-box.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
ST Technical Moderator
July 13, 2021

You are welcome.

Thank you for your contribution and thank you for your patience while we work on this.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Andrew Neil
Super User
July 13, 2021

@Community member​ "there is no configuration to the I Nucleo lrwan1"

Not quite sure what you mean by that?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Hamdi Oussema
Associate
July 13, 2021

@Andrew Neil​ as you can see here : https://github.com/USIWP1Module/USI_I-NUCLEO-LRWAN1 there are some configurations to be done depending on the I cube lrwan version.

Andrew Neil
Super User
July 14, 2021

Hmm ... I thought I'd replied to that yesterday?

That page refers to a very old version of I-CUBE-LRWAN - I just followed the instructions in the P-NUCLEO-LRWAN2 User Manual.

But it has been noted that these need updating for v2.0.0 of the I-CUBE-LRWAN:

https://community.st.com/s/question/0D53W00000wVhzTSAS/icubelrwan-the-things-stack-v3-replaces-the-things-network-v2

>:(

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
JCOUP
Visitor II
July 21, 2021

Where are you now? Could you recap the exact HW configuration you are using ? Are you in End-node configuration or in AT_Master configuration ? I'm trying to understand you problem to help you ? Do you drive the USI modem directly thanks to the AT-cmd or by th eway of the AT_Master. Regarding the documentation , you will find some relevant info in the UM 2073 ... regards

Tesla DeLorean
Guru
July 21, 2021

The complaint as I read it is that the NUCLEO-L073RZ examples for the NUCLEO+USI combo, as furnished by ST in the LRWAN2 kits, don't work properly out-of-the-box.

That the default UART settings/plumbing are wrong for the AT interface to the USI (I-NUCLEO-LRWAN1)

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Andrew Neil
Super User
July 22, 2021

@Community member​  - correct: the NUCLEO-L073RZ examples for the NUCLEO+USI combo, as furnished by ST in the LRWAN2 kits, do not work properly out-of-the-box.

"the default UART settings/plumbing are wrong for the AT interface to the USI (I-NUCLEO-LRWAN1)"

Indeed; plus:

  • (a) missing #include(s) of sys_conf.h
  • having fixed the UART selection, the code crashes (Hard Fault?)
  • Project defines duplicate settings in lorawanconf.h & sys_conf.h - leading to 57 warnings

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
JCOUP
Visitor II
July 21, 2021

OK, effectively we encountered some blocking points with this package. You will find here below all the needed fixes to be applied . Major fixe is regarding the fixe applied in lora_driver.c ... Regards

  • Main problem encountered was du to a less memory array allocation. Was already present in the previous version of the package (1.3.1) but without board effect !!! (could be possible following the final mapping organization provided by the linked).

in lora_driver.c in line 81 --> replace 16 by 32 size --> static uint8_t PtrTempValueFromDevice[32] ; /*to get back the device address in */

in sys_app.c --> just reorganize two statements UTIL_TIMER_Init() and Modem_IO_Init() in the SystemApp_Init(void) function
 
 
 */
 
void SystemApp_Init(void)
 
{
 
 /* USER CODE BEGIN SystemApp_Init_1 */
 
 /* USER CODE END SystemApp_Init_1 */
  
 /*Initialises timer and RTC*/
 
 /*UTIL_TIMER_Init();*/
 
 Gpio_PreInit();
  
 /* Configure the debug mode*/
 
#if 1 
 
 DBG_Init();
 
#endif
 
 /*Initialize the terminal */
 
 /*UTIL_ADV_TRACE_Init();*/
  
 Modem_IO_Init();
 
 /*Initialises timer and RTC*/
 
 UTIL_TIMER_Init();
 
 
 
 /*Set verbose LEVEL*/
 
 /*UTIL_ADV_TRACE_SetVerboseLevel(VERBOSE_LEVEL);*/
 
 /*Initialize the temperature and Battery measurement services */
 
 SYS_InitMeasurement();
  
 /*Initialize the Sensors */
 
 EnvSensors_Init();
  
 /*Init low power manager*/
 
 UTIL_LPM_Init();
 
 /* Disable Stand-by mode */
 
 UTIL_LPM_SetOffMode((1 << CFG_LPM_APPLI_Id), UTIL_LPM_DISABLE);
  
#if defined (LOW_POWER_DISABLE) && (LOW_POWER_DISABLE == 1)
 
 /* Disable Stop Mode */
 
 UTIL_LPM_SetStopMode((1 << CFG_LPM_APPLI_Id), UTIL_LPM_DISABLE);
 
#elif !defined (LOW_POWER_DISABLE)
 
#error LOW_POWER_DISABLE not defined
 
#endif /* LOW_POWER_DISABLE */
 
 /* USER CODE BEGIN SystemApp_Init_2 */
  
 /* USER CODE END SystemApp_Init_2 */
 
}
 
in sys_app.c --> remove from MasterApp_Init(void) the Modem_IO_Init()
 
in sys_app.c --> remove Gpio_PreInit(void) the two follwoing statements
 
line 310 --> /* __HAL_RCC_GPIOA_CLK_DISABLE();*/
 
line 312 --? /* __HAL_RCC_GPIOC_CLK_DISABLE();*/

  • in uart.c --> add the sys_conf.h --> to define the USE_USART2 symbol

here is the trace ( Rx pin) transmitted by the modem at reset .. Then after join accepted modem return 254 for battery level and return code OK for the sending frame . On Tx we see the AT+SEND cmd

This problem will be reported on L073 and L053 and will be present in the future next package release ...

JCOUP