Skip to main content
DS.4
Senior
Jul 28, 2025 5:15 PM UTC
Question

How to get XX_SCAN_REQUEST_XX event

ST ,

I am working on getting the scan request event ob the full stack.

After looking at these posts : 

https://community.st.com/t5/stm32-mcus-wireless/ble-how-can-i-get-a-scan-request-event/td-p/221485
https://community.st.com/t5/stm32-mcus-wireless/ble-how-can-i-get-a-scan-request-event/td-p/221485

It looks bleak.

 

Option 1: AN5270

The enable event :  ACI_HAL_SET_EVENT_MASK

The event message:  ACI HAL events
Both seems not to be enabled ( no "Y" on any of LO, BO , BF etc... ) . What does it mean ? Will they work on full stack ?

 

Option2 : AN6142/AN5270

The enable event :  HCI_LE_SET_EVENT ( I guess puting : • 0x0000000000040000: LE scan request received event  will do the trick?)  

The event message:: HCI_LE_SCAN_REQUEST_RECEIVED_EVENT  is enabled only for LO ? will it work on full stack bin?

 

DS4_0-1753722639206.png

 







This topic has been closed for replies.

4 replies

DS.4
DS.4Author
Senior
Jul 29, 2025 7:30 AM UTC

Update 

I found another unanswered thread : https://community.st.com/t5/stm32-mcus-wireless/aci-hal-set-event-mask-and-aci-hal-scan-req-report-vsevt-code/td-p/812836.

That got me to the WIKI : 

hci_le_scan_request_received_eventIndicate that a SCAN_REQ PDU or an AUX_SCAN_REQ PDU has been received by the advertiserBLE_p2pClient_Ext

Not quite sure,

Q:


1. But does it mean event available on Client side only? 

From AN5270 it looks like this event is for Server side ( what I am interested in :( 
HCI_LE_SCAN_REQUEST_RECEIVED_EVENT
Description
This event indicates that a SCAN_REQ PDU or an AUX_SCAN_REQ PDU has been received by the advertiser.
The request contains a device address from a scanner allowed by the advertising filter policy. The advertising set
is identified by Advertising_Handle. See Bluetooth spec. v.5.2 [Vol 4, Part E, 7.7.65.19].

2. What does _Ext? must be scanning/advertising in extended only ? 

DS.4
DS.4Author
Senior
Jul 29, 2025 1:40 PM UTC

Update: 

Like in this thread: 
https://community.st.com/t5/interface-and-connectivity-ics/how-to-receive-call-to-either-hci-le-scan-request-received-event/td-p/709317

ACI_HAL_SET_EVENT_MASK : does not work in ble full stack. I get an error that command does not exist.

HCI_LE_SET_EVENT : This command does not fail , default does not have 0x40000 enabled (scan_req_report) , so I added it.  but its not catching the event.
(Q:  should it fail if I configure an event that does not exist in stack ????? )

HCI_SET_EVENT : that has already the LE_META events enabled as default, and don't think anything else there can help.

 STM32WB repo : no luck couldn't find a single project using the events :
HCI_LE_SCAN_REQUEST_RECEIVED_SUBEVT_CODE 

ACI_HAL_SCAN_REQ_REPORT_VSEVT_CODE  

 

DS.4
DS.4Author
Senior
Jul 29, 2025 1:43 PM UTC

This thread , says aci_hal_set_mask()  works.


https://community.st.com/t5/interface-and-connectivity-ics/why-scan-req-event-is-not-sent/td-p/401895

.Any clue what stack is he using for: "I am using BlueNRG-2 chip with DTM firmware. It is connected to host processor STM32 by SPI."  ????


DS4_0-1753797600440.png

 

 

STTwo-32
ST Technical Moderator
Sep 17, 2025 7:50 AM UTC

Hello @DS.4 

If the correspondent commends is not supported on the mentioned BLE stacks, you have to use the stm32wb5x_BLE_Stack_full_extended_fw.bin. To know the stack you should use, you have to follow this table:

STTwo32_0-1758095438589.png

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.