Skip to main content
Associate
Jun 5, 2024 3:11 PM UTC
Question

Error : Unable to get core ID

Hi everyone,

I'm using a Nucleo WL55JC1 trying to run the Lorawan AT_slave application. When trying to run the project in STM32CubeIDE, I get the error "no device found on target". Did the process of the solution on this post : https://community.st.com/t5/stm32cubeide-mcus/error-in-stm32-cube-ide-on-nucleo-f746zg-target-no-device-found/td-p/54578

The Cube Programmer is able to connect correctly to the device, and to write the programm successfully, but when trying to run, I get "Error : Unable to get Core ID", and the device disconnects.

The Nucleo board is connected through USB to my Windows computer. I didn't modify anything in the LoRawan_AT_slave project code.

Does anyone have an idea about how to solve the problem ?

Thanks in advance!

This topic has been closed for replies.

4 replies

STTwo-32
ST Technical Moderator
Jun 5, 2024 3:49 PM UTC

Hello @mrgcap and welcome to the ST Community :smiling_face_with_smiling_eyes:.

Could you try using a USB Data cable and not a charging one. Also, try different USB ports on your PC.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
mrgcapAuthor
Associate
Jun 6, 2024 8:03 AM UTC

Hi,thank you for your reply !

I tried with two different cables and two different USB ports on my PC, but always get the same error. If the cable or the port was the problem, could I have been able to flash the program on the Nucleo ?

Also, I tried with two other brand new Nucleo boards, same model, and the same error appears on these two boards.

Do you have any other idea about what I could try ?

Thank you !

 

Uwe Bonnes
Chief
Jun 6, 2024 9:02 AM UTC

Probably you are running some deep sleep mode without setting the bits in DBGMCU to keep the debugger connection active during sleep. Expect substantial more sleep current need with the debugger connection active .

STTwo-32
ST Technical Moderator
Jul 15, 2024 1:41 PM UTC

Hello @mrgcap 

Could you please try to mass-erase your project and download it again using Cube Programmer to retry. Also, refer to this article for more details.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.