Skip to main content
Associate
Sep 8, 2025 2:23 AM UTC
Question

Can't get access to my NUCLEO-WB55RG board

I'm working on NUCLEO-WB55RG board, and I cannot access to my NUCLEO-WB55RG board.

1. I first tried DFU Mode with the setting below, but my computer couldn't find it.

mkk2_0-1757297160829.png

2. after that, I connected my board through ST-LINK with the setting below and used STM32CubeProgrammer for connection, But No STM32 target found! error occured. I've tried all the reset settings and Mode settings but same error occurs.

mkk2_2-1757297403612.png

stlink.jpg

3. So I gave up on checking the inside of the board. And I started IDE. I downloaded some examples and I run it. And now I see the error :
Failed to execute MI command:
target remote localhost:61234
Error message from debugger back end: localhost:
61234: Connection timed out.
4. So I tried to follow link below
(https://community.st.com/t5/stm32-mcus/how-to-solve-debugger-connection-issues/ta-p/49693)
but I cannot see debug option on changing the pin

mkk2_3-1757297826673.png


And I also cannot access to my board with CubeProgrammer,
And I also cannot get any different result by changing Debugger settings to Under Reset.

I'm really frustrated right now. Please help.

This topic has been closed for replies.

2 replies

mkk2Author
Associate
Sep 8, 2025 8:24 AM UTC

I Found out that I can only acces to my MCU with "HotPlug" Mode.

https://community.st.com/t5/stm32-mcus-wireless/can-t-program-connect-stm32wl55cc-unless-hot-plug-why/td-p/132939
according to the link above, ESD diode on NRST maybe on the wrong side
But I don't have any hardware techniques, is there any solutions that I can solve the problem?
Anybody Please answer ...

STTwo-32
ST Technical Moderator
Sep 29, 2025 12:51 PM UTC

Hello @mkk2 

This is not a behavior that should be seen on a ST design. Could please give more details about when this happend and what you tried exactly to connect it.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.