Skip to main content
Associate II
May 6, 2025 1:18 PM UTC
Solved

No device found on target. After some succesfull uploads

Hi,

I am working with a custom board with the STM32L431CCU6 mcu. The bord consist of the mcu and 2 i2c units and one SPI.

assjo_1-1746535632587.png

The board also has pin headers for BOOT0, SWDIO and SWCLK.

assjo_2-1746537392875.png

Sory for paint...

 

I am using the CubeIDE and a ST-LINK V2for programming the board and have successfully programed Blink on it. This was not problem free however since my coputer sometimes did not recognised the ST-LINK and sometimes failed to upload. Unfortuanatli I do not remember those errors in details.

After succesfully uploading a program for i2c communication I could not program the board any more. The error i receive from the IDE is:

STMicroelectronics ST-LINK GDB server. Version 7.9.0
Copyright (c) 2024, STMicroelectronics. All rights reserved.

Starting server with the following options:
 Persistent Mode : Disabled
 Logging Level : 1
 Listen Port Number : 61234
 Status Refresh Delay : 15s
 Verbose Mode : Disabled
 SWD Debug : Enabled
 InitWhile : Enabled

Target no device found

Error in initializing ST-LINK device.
Reason: No device found on target.

 

After a while of plugging the link in and out and trying to press boot and desperatly trying whatever I could, I tried a second board. This was a new board with a new ship but same problem. I tried using the ST-LINK of a NUCLEO board, same problem. Different computer, same problem. Cube programmer, same problem(? different errormessage: Error: Unable to get core ID,  Error: No STM32 target found!) I am all out of ideas and no other post seems to solve my problem. Any ideas?

 

 

This topic has been closed for replies.
Andrew Neil
Andrew NeilBest answer
Super User
May 6, 2025 1:26 PM UTC

First, is it a genuine ST-Link?

https://community.st.com/t5/stm32-mcus/how-to-recognize-a-genuine-st-link-v2-versus-a-cloned-one/ta-p/49471 

 

Note that breadboards are notoriously prone to unreliable connections - which can certainly mess-up your debugger connection.

Rather than route NRST via a breadboard, let the ST-Link control it and use connect under hardware reset.

 


@assjo wrote:

my coputer sometimes did not recognised the ST-LINK 


You mean the ST-Link didn't even appear in Device Manager (or equivalent).

That suggests a USB connection problem between the computer & the ST-Link.

 

On resolving debugger connection issues:

https://community.st.com/t5/stm32-mcus/how-to-solve-connection-errors-when-connecting-and-programming/tac-p/786977

https://community.st.com/t5/stm32-mcus/how-to-solve-debugger-connection-issues/ta-p/49693

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.

2 replies

Andrew Neil
Andrew NeilBest answer
Super User
May 6, 2025 1:26 PM UTC

First, is it a genuine ST-Link?

https://community.st.com/t5/stm32-mcus/how-to-recognize-a-genuine-st-link-v2-versus-a-cloned-one/ta-p/49471 

 

Note that breadboards are notoriously prone to unreliable connections - which can certainly mess-up your debugger connection.

Rather than route NRST via a breadboard, let the ST-Link control it and use connect under hardware reset.

 


@assjo wrote:

my coputer sometimes did not recognised the ST-LINK 


You mean the ST-Link didn't even appear in Device Manager (or equivalent).

That suggests a USB connection problem between the computer & the ST-Link.

 

On resolving debugger connection issues:

https://community.st.com/t5/stm32-mcus/how-to-solve-connection-errors-when-connecting-and-programming/tac-p/786977

https://community.st.com/t5/stm32-mcus/how-to-solve-debugger-connection-issues/ta-p/49693

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
assjoAuthor
Associate II
May 6, 2025 2:58 PM UTC

Thanks! This was the solution!

Firstly I connected the NRST directly to the ST-LINK, but then a new error occured. Unable to erase memory. Someone recomended changing all the cables incase any was broken or damaged and since then programming has worked without any problem.

(The ST-Link did appere in the device manager but the IDE could not see it or someting like that.)