Skip to main content
Associate
March 5, 2025
Question

Low power STOP1 mode current consumption high

Hello,

I am using STM32G4 to develop a project where I am running FreeRTOS.

Recently I was working on debugging the issues for low power mode.

I can confirm all the peripherals clocks are disabled before entering the STOP1 mode, but the power consumption is still very high (~35mA). 

My function to prepare for STOP1 mode is here:

void EnterStop1Mode(void)
{
    /* Ensure all tasks are idle before entering Stop mode */
    taskENTER_CRITICAL();  

    //HAL_PWREx_EnableLowPowerRunMode();

    /* Disable SysTick Completely */
    SysTick->CTRL &= ~SysTick_CTRL_ENABLE_Msk;  
    HAL_SuspendTick();

    /* Disable Peripheral Clocks to Reduce Power */
    HighPowerSwitch(SWITCH_OFF);
    HAL_ADC_MspDeInit(&hadc1);
    HAL_SPI_MspDeInit(&hspi1);
    HAL_SPI_MspDeInit(&hspi2);
    HAL_TIM_PWM_MspDeInit(&htim1);
    HAL_TIM_PWM_MspDeInit(&htim2);
    HAL_TIM_PWM_MspDeInit(&htim15);
    HAL_TIM_Encoder_MspDeInit(&htim3);
    HAL_TIM_Encoder_MspDeInit(&htim4);
    HAL_UART_MspDeInit(&huart1);
    HAL_I2C_MspDeInit(&hi2c2);
    HAL_DAC_MspDeInit(&hdac1);

    /* Disable Debug Mode to Allow Full Power Down */
    //HAL_DBGMCU_DisableDBGStopMode();
    PreStop_SystemClock_Config();

    HAL_PWREx_EnableLowPowerRunMode(); // Enable low-power regulator

    /* Enter Stop 1 Mode */
    HAL_PWREx_EnterSTOP1Mode(PWR_STOPENTRY_WFI);

    /* --- Wake-Up Occurred --- */

    /* Restore System Clock */
    SystemClock_Config();

    /* Re-enable SysTick */
    SysTick->CTRL |= SysTick_CTRL_ENABLE_Msk;
    HAL_ResumeTick();

    /* Restore GPIOs */
    MX_GPIO_Init();

    /* Resume FreeRTOS Task Scheduling */
    taskEXIT_CRITICAL();
}

I tried with the code like below:

int main(void)
{
    HAL_Init();
    SystemClock_Config();
    MX_GPIO_Init();
   
    HAL_Delay(1000);

    /* Enter Stop 1 Mode */
    HAL_PWREx_EnterSTOP1Mode(PWR_STOPENTRY_WFI);

    while (1);
}
just to test if it might be because of any peripherals not properly disabled. However running this code gives the me same result. 
 
Do you see anything I made is fundamentally incorrect? I tried to find a standard procedure for entering the low power mode, but couldn't find any. Would you suggest some different approaches I could maybe check it out? 

One thing worth to mention is, when I had a fresh PCB without any program, the power consumption is close to zero. Thus, I can be sure, I don't have anywhere in hardware it is leaking the current.
 
Thanks for your support!
 
 
This topic has been closed for replies.

4 replies

ST Employee
March 11, 2025

Hello @weji_taku, welcome to ST Community, 

First, set all unused GPIOs to analog mode to minimize power consumption : check Tips for using STM32 low-power modes - STMicroelectronics Community

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Andrew Neil
Super User
March 22, 2025

Please see How to insert source code.

 


@weji_taku wrote:

I can confirm all the peripherals clocks are disabled before entering the STOP1 mode, but the power consumption is still very high (~35mA). 


Is the debugger physically disconnected?

Have you power-cycled the target since disconnecting the debugger?

See:

https://community.st.com/t5/stm32-mcus-wireless/how-to-reduce-the-power-consumption-of-stm32wb55-stop2-mode/m-p/785696/highlight/true#M23997

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
weji_takuAuthor
Associate
March 24, 2025

Hi Andrew,

Thank you for your reply!

I finally identified the issues were because of some encoder circuits, which are consuming quite some current.

However, I have problem to wake it up now. I configured the wake up source to be EXTI. I could confirm that EXTI pin works before the sleep (HW is 100% working), but it cannot wake up. I wonder if there are some standard procedures about this topic? Just so I could walk it through to see what I might be missing?

Thanks :)

 

Andrew Neil
Super User
March 24, 2025

@weji_taku wrote:

I finally identified the issues were because of some encoder circuits, which are consuming quite some current.


Excellent so please mark that as the solution:

https://community.st.com/t5/community-guidelines/help-others-to-solve-their-issues/ta-p/575256

 


@weji_taku wrote:

However, I have problem to wake it up now. I configured the wake up source to be EXTI. I could confirm that EXTI pin works before the sleep (HW is 100% working), but it cannot wake up. I wonder if there are some standard procedures about this topic? Just so I could walk it through to see what I might be missing?


That's a separate question - please start a new thread for that.

Please post a link here for people to find it.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.