Skip to main content
Associate
March 20, 2025
Solved

How to reduce the power consumption of STM32WB55 stop2 mode?

  • March 20, 2025
  • 4 replies
  • 951 views

Hello,

We have a project that uses STM32WB55 as the main controller.
This project has certain requirements for power consumption and wants to enter sleep mode through stop2 mode.

But I tested the power consumption current of stop2 mode on the STM32WB55 DK board (Nucleo-WB55) and it was 107uA.  We have configured RTC and external interrupts to wake up stop2 mode, and we want its power consumption current in stop2 mode to be less than 5uA.

May I ask if the power consumption current can reach 5uA when enabling RTC Alarm A and external interrupt to enter stop2 mode?

I used the routine on the stm32wb55 official website to test the stop2 mode: STM32Cube_FW_WB_V1.22.0\Projects\P-NUCLEO-WB55.Nucleo\Examples_LL\PWR\PWR_EnterStopMode

I added serial port printing and configuration before entering stop2 mode to this routine.

Now I have configured the MSI clock to 100Khz.

void EnterStop2Mode(void)
{
	LL_GPIO_InitTypeDef gpio_initstruct = {LL_GPIO_PIN_ALL, LL_GPIO_MODE_ANALOG, 
										 LL_GPIO_SPEED_FREQ_HIGH, LL_GPIO_OUTPUT_PUSHPULL, 
										 LL_GPIO_PULL_NO, LL_GPIO_AF_0};

	/* Set all GPIO in analog state to reduce power consumption, */
	/* Note: Debug using ST-Link is not possible during the execution of this */
	/* example because communication between ST-link and the device */
	/* under test is done through UART. All GPIO pins are disabled (set */
	/* to analog input mode) including UART I/O pins. */
	LL_AHB2_GRP1_EnableClock(LL_AHB2_GRP1_PERIPH_GPIOA |
							LL_AHB2_GRP1_PERIPH_GPIOB |
							LL_AHB2_GRP1_PERIPH_GPIOC |
							LL_AHB2_GRP1_PERIPH_GPIOD |
							LL_AHB2_GRP1_PERIPH_GPIOE |
							LL_AHB2_GRP1_PERIPH_GPIOH);

	LL_GPIO_Init(GPIOA, &gpio_initstruct);
	LL_GPIO_Init(GPIOB, &gpio_initstruct);
	LL_GPIO_Init(GPIOC, &gpio_initstruct);
	LL_GPIO_Init(GPIOD, &gpio_initstruct);
	LL_GPIO_Init(GPIOE, &gpio_initstruct);
	LL_GPIO_Init(GPIOH, &gpio_initstruct);

	LL_AHB2_GRP1_DisableClock(LL_AHB2_GRP1_PERIPH_GPIOA |
							LL_AHB2_GRP1_PERIPH_GPIOB |
							LL_AHB2_GRP1_PERIPH_GPIOC |
							LL_AHB2_GRP1_PERIPH_GPIOD |
							LL_AHB2_GRP1_PERIPH_GPIOE |
							LL_AHB2_GRP1_PERIPH_GPIOH);

	HAL_SuspendTick();
	HAL_UART_DeInit(&huart1);
	HAL_UART_MspDeInit(&huart1);

	LL_PWR_SetRegulVoltageScaling(LL_PWR_REGU_VOLTAGE_SCALE2);

	LL_RCC_MSI_Enable();

	while( !LL_RCC_MSI_IsReady() )
	{
	}

	LL_RCC_SetSysClkSource( LL_RCC_SYS_CLKSOURCE_MSI );
	LL_RCC_SetSMPSClockSource( LL_RCC_SMPS_CLKSOURCE_MSI );

	while( LL_RCC_GetSysClkSource() != LL_RCC_SYS_CLKSOURCE_STATUS_MSI )
	{
	}
	/* 1 - Set Frequency to 100KHz to activate Low Power Run Mode: 100KHz */
	/* Range Selection already enabled. Need to change Range only */
	LL_RCC_MSI_SetRange(LL_RCC_MSIRANGE_0);
	// /* Update CMSIS variable */
	LL_SetSystemCoreClock(100 * 1000);
	LL_RCC_SetClkAfterWakeFromStop( LL_RCC_STOP_WAKEUPCLOCK_MSI );

	/** Request to enter Stop 2 mode */
	/* Set Stop 2 mode when CPU enters deepsleep */
	LL_PWR_SetPowerMode(LL_PWR_MODE_STOP2);
	LL_C2_PWR_SetPowerMode(LL_PWR_MODE_STOP2);
	LL_LPM_EnableDeepSleep();

	/* Request Wait For Interrupt */
	__WFI();
}

 

How to configure it to reduce power consumption?

 

Thanks!

This topic has been closed for replies.
Best answer by alexliao

This issue has been resolved.

The code configuration is correct.

After downloading the program, I unplugged the power from the board and then plugged it back in to enter stop2 mode, with a power consumption of 2.5uA.

Thank you!

4 replies

Andrew Neil
Super User
March 20, 2025

@alexliao wrote:

I tested the power consumption current of stop2 mode on the STM32WB55 DK board


Are you sure that you've disconnected all other resources on the board, and are measuring only the target microcontroller's consumption?

In particular, check for leakage through connections to on-board ST-Link, etc.

You will need to examine the schematics carefully - the written documentation can miss things ...

 


@alexliao wrote:

May I ask if the power consumption current can reach 5uA when enabling RTC Alarm A and external interrupt to enter stop2 mode?


What does the datasheet tell you? It should have figures to at least give you a ballpark estimate ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
alexliaoAuthor
Associate
March 20, 2025

Hi @Andrew Neil 

I am using the Nucleo-WB55 development board. According to the user manual, I disconnected J5 and jump cap J2, and connected the ammeter to VDD on J2. At this time, the power consumption in stop2 mode is 107uA.

According to the datasheet, the power consumption current when turning on RTC in Stop2 mode is only 2uA..

I have tested standby mode, and the power consumption of this mode is 1uA.

The power consumption of stop2 mode has not decreased yet...

alexliaoAuthorBest answer
Associate
March 21, 2025

This issue has been resolved.

The code configuration is correct.

After downloading the program, I unplugged the power from the board and then plugged it back in to enter stop2 mode, with a power consumption of 2.5uA.

Thank you!

Andrew Neil
Super User
March 22, 2025

@alexliao wrote:

I unplugged the power from the board and then plugged it back in to enter stop2 mode, with a power consumption of 2.5uA.


ISTR that the "allow debug during sleep" setting is only cleared by a power-cycle - not even a hard reset.

Maybe that's what was going on here?

 

PS:

Found it:

https://community.st.com/t5/stm32cubeide-mcus/dbgmcu-cr-dbg-stop-setting-ignored/m-p/616354/highlight/true#M22468

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.